<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Powertrain and Electrification Analog DriversのトピックRe: FRDM-HB2001-EVM Compatibility with Arduino Boards</title>
    <link>https://community.nxp.com/t5/Powertrain-and-Electrification/FRDM-HB2001-EVM-Compatibility-with-Arduino-Boards/m-p/626484#M146</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hong Wei,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can connect the FRDM-HB2001-EVM to the Arduino UNO board without any problems, but only SPI mode will be possible, you will not be able to use IN1 and IN2 inputs (parallel mode).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for the Arduino Mega board, there should be soon available the DEVKIT-TRANSLATE which will allow you to use also IN1 and IN2 inputs (parallel mode) and FB output if you need to measure an output current.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 Mar 2017 13:01:07 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2017-03-30T13:01:07Z</dc:date>
    <item>
      <title>FRDM-HB2001-EVM Compatibility with Arduino Boards</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/FRDM-HB2001-EVM-Compatibility-with-Arduino-Boards/m-p/626483#M145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Hi all.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;I would like to ask if the MC33HB2001's Evaluation Board, FRDM-HB2001-EVM, can be used with Arduino boards such as the Arduino Mega 2560, or the Arduino UNO.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;It seems like the FRDM-HB2001-EVM has pins specifically to fit FRDM-KL25Z only. However, according to the FRDM-HB2001-EVM user's guide, it was stated that this Evaluation Board is "compatible with any Arduino Platform Boards. However, if a board other than the FRDM-KL25Z is used, MCU code must be written to work with the board."&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Does this mean that it can be used with the Arduino Mega 2560 or UNO?&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Thank you very much for your assistance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Mar 2017 07:31:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/FRDM-HB2001-EVM-Compatibility-with-Arduino-Boards/m-p/626483#M145</guid>
      <dc:creator>hongweikoh</dc:creator>
      <dc:date>2017-03-28T07:31:32Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-HB2001-EVM Compatibility with Arduino Boards</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/FRDM-HB2001-EVM-Compatibility-with-Arduino-Boards/m-p/626484#M146</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hong Wei,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can connect the FRDM-HB2001-EVM to the Arduino UNO board without any problems, but only SPI mode will be possible, you will not be able to use IN1 and IN2 inputs (parallel mode).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for the Arduino Mega board, there should be soon available the DEVKIT-TRANSLATE which will allow you to use also IN1 and IN2 inputs (parallel mode) and FB output if you need to measure an output current.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Mar 2017 13:01:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/FRDM-HB2001-EVM-Compatibility-with-Arduino-Boards/m-p/626484#M146</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2017-03-30T13:01:07Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-HB2001-EVM Compatibility with Arduino Boards</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/FRDM-HB2001-EVM-Compatibility-with-Arduino-Boards/m-p/626485#M147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tomas,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you so much for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to clarify something with you. By saying that I cannot use IN1 &amp;amp; IN2 inputs (parallel mode), do you mean I cannot simply connect two PWM pins from the UNO to IN1 &amp;amp; IN2 to control the FRDM-HB2001-EVM?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you once again!&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Apr 2017 08:44:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/FRDM-HB2001-EVM-Compatibility-with-Arduino-Boards/m-p/626485#M147</guid>
      <dc:creator>hongweikoh</dc:creator>
      <dc:date>2017-04-06T08:44:38Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-HB2001-EVM Compatibility with Arduino Boards</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/FRDM-HB2001-EVM-Compatibility-with-Arduino-Boards/m-p/626486#M148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tomas,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to ask, since the data sheet of the EVM states that it can be operated in two modes, H bridge mode and a Half Bridge mode, is there something that must be done for the board to enter these individual mode? Is it through the SPI software?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Apr 2017 08:47:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/FRDM-HB2001-EVM-Compatibility-with-Arduino-Boards/m-p/626486#M148</guid>
      <dc:creator>hongweikoh</dc:creator>
      <dc:date>2017-04-07T08:47:54Z</dc:date>
    </item>
  </channel>
</rss>