<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Powertrain and Electrification Analog DriversのトピックRe: HB2000 status value error</title>
    <link>https://community.nxp.com/t5/Powertrain-and-Electrification/HB2000-status-value-error/m-p/992977#M128</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;OUT1 &amp;amp; OUT2 are connected by wire, not by motor&lt;/P&gt;&lt;P&gt;Fault status mask is default setting.&lt;/P&gt;&lt;P&gt;The same register is while the motor is running, 0x2001 occurs frequently in the reverse direction,&amp;nbsp;&lt;/P&gt;&lt;P&gt;and 0x2194 occurs frequently inthe forward direction.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Mar 2020 07:49:16 GMT</pubDate>
    <dc:creator>hyjung</dc:creator>
    <dc:date>2020-03-20T07:49:16Z</dc:date>
    <item>
      <title>HB2000 status value error</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/HB2000-status-value-error/m-p/992975#M126</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question to ask about the MC33HB2000 about fault detection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. test setup&lt;/P&gt;&lt;P&gt;&amp;nbsp;-.&amp;nbsp;Used as H-bridge mode &amp;amp; Parallel mode with Vpwr 12V.&lt;/P&gt;&lt;P&gt;&amp;nbsp;-.&amp;nbsp;Set the initial SPI default value and run after Out 1 &amp;amp; out 2 short.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; 2. Read motor driver status value&lt;BR /&gt;&amp;nbsp; -. case 1) 0x2001&lt;BR /&gt;&amp;nbsp; -. case 2) 0x2194&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question)&lt;/P&gt;&lt;P&gt;As a result of repeatedly checking the motor status value under the same conditions,&lt;/P&gt;&lt;P&gt;different fault value appears, and we inquire about the reason.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Mar 2020 01:27:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/HB2000-status-value-error/m-p/992975#M126</guid>
      <dc:creator>hyjung</dc:creator>
      <dc:date>2020-03-20T01:27:03Z</dc:date>
    </item>
    <item>
      <title>Re: HB2000 status value error</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/HB2000-status-value-error/m-p/992976#M127</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;How to understand about OUT1&amp;amp;OUT2 short? they are short together?&lt;/P&gt;&lt;P&gt;What's the register setting of Fault status mask register?&lt;/P&gt;&lt;P&gt;Or what about work normally then short OUT1/OUT2 to read fault register normal or not?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Mar 2020 02:39:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/HB2000-status-value-error/m-p/992976#M127</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2020-03-20T02:39:08Z</dc:date>
    </item>
    <item>
      <title>Re: HB2000 status value error</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/HB2000-status-value-error/m-p/992977#M128</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;OUT1 &amp;amp; OUT2 are connected by wire, not by motor&lt;/P&gt;&lt;P&gt;Fault status mask is default setting.&lt;/P&gt;&lt;P&gt;The same register is while the motor is running, 0x2001 occurs frequently in the reverse direction,&amp;nbsp;&lt;/P&gt;&lt;P&gt;and 0x2194 occurs frequently inthe forward direction.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Mar 2020 07:49:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/HB2000-status-value-error/m-p/992977#M128</guid>
      <dc:creator>hyjung</dc:creator>
      <dc:date>2020-03-20T07:49:16Z</dc:date>
    </item>
    <item>
      <title>Re: HB2000 status value error</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/HB2000-status-value-error/m-p/992978#M129</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I attached the short circuit application note for more explain here.&lt;/P&gt;&lt;P&gt;If short OUT1 and OUT2 the over current will happened,at last over temperature also happen to trigger.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Mar 2020 13:19:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/HB2000-status-value-error/m-p/992978#M129</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2020-03-20T13:19:21Z</dc:date>
    </item>
    <item>
      <title>Re: HB2000 status value error</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/HB2000-status-value-error/m-p/992979#M130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When OUT1 and OUT2 are set to short and operate at normal temperature, OT occurs immediately, and the Tj of the device does not exceed OT.&lt;BR /&gt;Does it mean that OT shutdown does not correlate with Tj temperature?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 22 Mar 2020 19:11:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/HB2000-status-value-error/m-p/992979#M130</guid>
      <dc:creator>hyjung</dc:creator>
      <dc:date>2020-03-22T19:11:56Z</dc:date>
    </item>
    <item>
      <title>Re: HB2000 status value error</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/HB2000-status-value-error/m-p/992980#M131</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If so please suggest customer to do same test in NXP evb KIT to eliminate hardware issue.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Mar 2020 03:40:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/HB2000-status-value-error/m-p/992980#M131</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2020-03-23T03:40:36Z</dc:date>
    </item>
  </channel>
</rss>