<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Using Our CommunityのトピックNXP MCAL Package</title>
    <link>https://community.nxp.com/t5/Using-Our-Community/NXP-MCAL-Package/m-p/2115434#M869</link>
    <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;For S32K3xx series NXP controller - We are planning to buy the NXP MCAL Package for Autosar Project.&lt;/P&gt;&lt;P&gt;The BSW Modules Configuration is done via Vector Davinci Configurator Tool.&lt;/P&gt;&lt;P&gt;1. Can NXP Mcal package be integrated into Davinci configurator directly using the Third-Party setup which vector supports?? and MCAL modules can be configured and generated?&lt;/P&gt;&lt;P&gt;2. Does Eb Tresos Tool is used for MCAL configuration .. Is it a separate License we need to buy for EB Tresos for configuration or is it part of NXP Package.?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your support&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Vinay&lt;/P&gt;</description>
    <pubDate>Thu, 12 Jun 2025 13:17:41 GMT</pubDate>
    <dc:creator>Vinaymsn</dc:creator>
    <dc:date>2025-06-12T13:17:41Z</dc:date>
    <item>
      <title>NXP MCAL Package</title>
      <link>https://community.nxp.com/t5/Using-Our-Community/NXP-MCAL-Package/m-p/2115434#M869</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;For S32K3xx series NXP controller - We are planning to buy the NXP MCAL Package for Autosar Project.&lt;/P&gt;&lt;P&gt;The BSW Modules Configuration is done via Vector Davinci Configurator Tool.&lt;/P&gt;&lt;P&gt;1. Can NXP Mcal package be integrated into Davinci configurator directly using the Third-Party setup which vector supports?? and MCAL modules can be configured and generated?&lt;/P&gt;&lt;P&gt;2. Does Eb Tresos Tool is used for MCAL configuration .. Is it a separate License we need to buy for EB Tresos for configuration or is it part of NXP Package.?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your support&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Vinay&lt;/P&gt;</description>
      <pubDate>Thu, 12 Jun 2025 13:17:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Using-Our-Community/NXP-MCAL-Package/m-p/2115434#M869</guid>
      <dc:creator>Vinaymsn</dc:creator>
      <dc:date>2025-06-12T13:17:41Z</dc:date>
    </item>
    <item>
      <title>Re: NXP MCAL Package</title>
      <link>https://community.nxp.com/t5/Using-Our-Community/NXP-MCAL-Package/m-p/2121666#M870</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/251521"&gt;@Vinaymsn&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I apologize for the late reply, there was an issue with the tracker tool, and the ticket never got assigned. However, I can see this is the same question you posted to the support case internally, so in order to avoid any confusion, I will keep supporting you through your case.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Mon, 23 Jun 2025 21:23:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Using-Our-Community/NXP-MCAL-Package/m-p/2121666#M870</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2025-06-23T21:23:51Z</dc:date>
    </item>
  </channel>
</rss>