<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Connecting two flash in parallel using 32 bit data bus in Using Our Community</title>
    <link>https://community.nxp.com/t5/Using-Our-Community/Connecting-two-flash-in-parallel-using-32-bit-data-bus/m-p/405828#M218</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have one design constraint to use two flash connected in parallel: First flash uses (D0-D15) and second flash uses D16 - D31. Using same physically address for both flash with available 28 bit address bus using A1 - A19. For example, When we write double word into flash, it is as good as writing first word into first flash and second word into second flash. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We need to know how to send commands to both flash at same time for operation like READ or WRITE. Both flash shares same CE, OE &amp;amp; WE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Manjunath&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Aug 2015 11:13:58 GMT</pubDate>
    <dc:creator>manjunathgangad</dc:creator>
    <dc:date>2015-08-28T11:13:58Z</dc:date>
    <item>
      <title>Connecting two flash in parallel using 32 bit data bus</title>
      <link>https://community.nxp.com/t5/Using-Our-Community/Connecting-two-flash-in-parallel-using-32-bit-data-bus/m-p/405828#M218</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have one design constraint to use two flash connected in parallel: First flash uses (D0-D15) and second flash uses D16 - D31. Using same physically address for both flash with available 28 bit address bus using A1 - A19. For example, When we write double word into flash, it is as good as writing first word into first flash and second word into second flash. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We need to know how to send commands to both flash at same time for operation like READ or WRITE. Both flash shares same CE, OE &amp;amp; WE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Manjunath&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Aug 2015 11:13:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Using-Our-Community/Connecting-two-flash-in-parallel-using-32-bit-data-bus/m-p/405828#M218</guid>
      <dc:creator>manjunathgangad</dc:creator>
      <dc:date>2015-08-28T11:13:58Z</dc:date>
    </item>
  </channel>
</rss>