<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RW612 BLE peripheral maximum connections to centrals in Zephyr Project</title>
    <link>https://community.nxp.com/t5/Zephyr-Project/RW612-BLE-peripheral-maximum-connections-to-centrals/m-p/2420493#M757</link>
    <description>&lt;P&gt;You may check the datasheet for different topology.There are one antenna topology and two antenna topology using internal SPDT&lt;/P&gt;</description>
    <pubDate>Mon, 12 Oct 2026 21:54:50 GMT</pubDate>
    <dc:creator>db16122</dc:creator>
    <dc:date>2026-10-12T21:54:50Z</dc:date>
    <item>
      <title>RW612 BLE peripheral maximum connections to centrals</title>
      <link>https://community.nxp.com/t5/Zephyr-Project/RW612-BLE-peripheral-maximum-connections-to-centrals/m-p/2420339#M756</link>
      <description>&lt;P&gt;The NXP zsdk information specifies that RW612 supports scantternet topology, which allows for a peripheral to be connected to multiple centrals &lt;A href="https://github.com/nxp-zephyr/nxp-zsdk/blob/main/doc/wireless/release-notes/topics/bluetooth_radio_features.md" target="_blank"&gt;nxp-zsdk/doc/wireless/release-notes/topics/bluetooth_radio_features.md at main · nxp-zephyr/nxp-zsdk · GitHub&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;How many connections are supported from a peripheral device to different BLE centrals?&lt;BR /&gt;&lt;BR /&gt;Are there any constraints across these connections? Shall they use same PHY, connection parameters or other traits ?&lt;BR /&gt;&lt;BR /&gt;Best regards Tonny Bing&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 12 Oct 2026 08:43:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Zephyr-Project/RW612-BLE-peripheral-maximum-connections-to-centrals/m-p/2420339#M756</guid>
      <dc:creator>tobg</dc:creator>
      <dc:date>2026-10-12T08:43:34Z</dc:date>
    </item>
    <item>
      <title>Re: RW612 BLE peripheral maximum connections to centrals</title>
      <link>https://community.nxp.com/t5/Zephyr-Project/RW612-BLE-peripheral-maximum-connections-to-centrals/m-p/2420493#M757</link>
      <description>&lt;P&gt;You may check the datasheet for different topology.There are one antenna topology and two antenna topology using internal SPDT&lt;/P&gt;</description>
      <pubDate>Mon, 12 Oct 2026 21:54:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Zephyr-Project/RW612-BLE-peripheral-maximum-connections-to-centrals/m-p/2420493#M757</guid>
      <dc:creator>db16122</dc:creator>
      <dc:date>2026-10-12T21:54:50Z</dc:date>
    </item>
    <item>
      <title>Re: RW612 BLE peripheral maximum connections to centrals</title>
      <link>https://community.nxp.com/t5/Zephyr-Project/RW612-BLE-peripheral-maximum-connections-to-centrals/m-p/2420809#M758</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For our examples, we&amp;nbsp; have the&lt;/P&gt;
&lt;LI-CODE lang="c"&gt;CONFIG_BT_MAX_CONN=16&lt;/LI-CODE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;This match the "Maximum 16 Bluetooth LE connections" from the Relese Notes.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Tue, 13 Oct 2026 18:31:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Zephyr-Project/RW612-BLE-peripheral-maximum-connections-to-centrals/m-p/2420809#M758</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2026-10-13T18:31:01Z</dc:date>
    </item>
  </channel>
</rss>