<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Zephyr ProjectのトピックEdgelock RW612 Zephyr</title>
    <link>https://community.nxp.com/t5/Zephyr-Project/Edgelock-RW612-Zephyr/m-p/2378833#M695</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I would like to store cetificates and private key in the edge lock secure enclave of the RW612.&lt;BR /&gt;My application is developed using zephyr and I need to be able to provision those certificates and read them at run time. Is this supported ? Could you provide documents / guides on how to do that.&lt;BR /&gt;&lt;BR /&gt;I am currently using upstream Zephyr 4.2.0&lt;BR /&gt;&lt;BR /&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Tue, 09 Jun 2026 08:59:30 GMT</pubDate>
    <dc:creator>benjaminaxiles</dc:creator>
    <dc:date>2026-06-09T08:59:30Z</dc:date>
    <item>
      <title>Edgelock RW612 Zephyr</title>
      <link>https://community.nxp.com/t5/Zephyr-Project/Edgelock-RW612-Zephyr/m-p/2378833#M695</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I would like to store cetificates and private key in the edge lock secure enclave of the RW612.&lt;BR /&gt;My application is developed using zephyr and I need to be able to provision those certificates and read them at run time. Is this supported ? Could you provide documents / guides on how to do that.&lt;BR /&gt;&lt;BR /&gt;I am currently using upstream Zephyr 4.2.0&lt;BR /&gt;&lt;BR /&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 09 Jun 2026 08:59:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Zephyr-Project/Edgelock-RW612-Zephyr/m-p/2378833#M695</guid>
      <dc:creator>benjaminaxiles</dc:creator>
      <dc:date>2026-06-09T08:59:30Z</dc:date>
    </item>
    <item>
      <title>Re: Edgelock RW612 Zephyr</title>
      <link>https://community.nxp.com/t5/Zephyr-Project/Edgelock-RW612-Zephyr/m-p/2379710#M696</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/249745"&gt;@benjaminaxiles&lt;/a&gt;, hope you are doing well.&lt;/P&gt;
&lt;P&gt;Would you please provide more details on your expected application functionality to provision the certificates/private key? Are you expecting the provisioning to be done with an specific transport?&lt;/P&gt;
&lt;P&gt;In the meantime, I suggest referring to the examples "zephyr/samples/tfm_integration/psa_crypto" and "modules/lib/nxp_iot_agent/zephyr/samples/el2go_agent", as these implement different approaches to key storage and provisioning, in particular, the "el2go_agent" example is meant to demonstrate how to use the Edgelock 2GO service to provision keys and certificates.&lt;/P&gt;
&lt;P&gt;As a side note, I would suggest migrating to latest Zephyr downstream/upstream versions, as the support for RW612's security features has been modified since version 4.2.0.&lt;/P&gt;
&lt;P&gt;Please let me know if this information is helpful.&lt;/P&gt;</description>
      <pubDate>Wed, 10 Jun 2026 21:21:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Zephyr-Project/Edgelock-RW612-Zephyr/m-p/2379710#M696</guid>
      <dc:creator>RomanVR</dc:creator>
      <dc:date>2026-06-10T21:21:48Z</dc:date>
    </item>
  </channel>
</rss>