<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Zephyr Project中的主题 Re: Zephyr BLE examples for RW610</title>
    <link>https://community.nxp.com/t5/Zephyr-Project/Zephyr-BLE-examples-for-RW610/m-p/2195512#M520</link>
    <description>&lt;P&gt;If custom a board, nxp need to review the design and make sure the custom board meet our request.&lt;/P&gt;</description>
    <pubDate>Thu, 30 Oct 2025 06:14:18 GMT</pubDate>
    <dc:creator>shaun_wu</dc:creator>
    <dc:date>2025-10-30T06:14:18Z</dc:date>
    <item>
      <title>Zephyr BLE examples for RW610</title>
      <link>https://community.nxp.com/t5/Zephyr-Project/Zephyr-BLE-examples-for-RW610/m-p/2195308#M518</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on bringing up a custom board based on RW610. So far i have tested I2C, SPI and UART on the board. The project is based on Zephyr and the next step is to test out BLE.&lt;/P&gt;&lt;P&gt;Firstly, there is no option to import an example for the RW610 because there is no dedicated dev board for the chip. I tried using the FRDM-RW610 board for a reference, configured the pins according to my custom board by passing a supplementary overlay file, and also configured the peripherals as necessary. I tried multiple ways to enable BLE but none of them are working.&lt;/P&gt;&lt;P&gt;The example 'peripheral_ht' works straightaway on the FRDM-RW612 as it should, but the same example doesnt work for the RW610 even after the configurations.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have referred to &lt;A href="https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Zephyr-amp-RW610/m-p/1969253" target="_self"&gt;this question&lt;/A&gt; for reference.&lt;/P&gt;&lt;P&gt;On serial debug, i am getting the following error:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;ASSERTION FAIL [err == 0] @ WEST_TOPDIR/zephyr/subsys/bluetooth/host/hci_core.c:504
        Controller unresponsive, command opcode 0xfc61 timeout with err -11
[00:00:16.717,989] &amp;lt;err&amp;gt; os: r0/a1:  0x00000003  r1/a2:  0x00000000  r2/a3:  0x00000002
[00:00:16.717,992] &amp;lt;err&amp;gt; os: r3/a4:  0x00000003 r12/ip:  0x00000010 r14/lr:  0x10045e9f
[00:00:16.717,994] &amp;lt;err&amp;gt; os:  xpsr:  0x01000000
[00:00:16.717,997] &amp;lt;err&amp;gt; os: Faulting instruction address (r15/pc): 0x10045eae
[00:00:16.718,004] &amp;lt;err&amp;gt; os: &amp;gt;&amp;gt;&amp;gt; ZEPHYR FATAL ERROR 3: Kernel oops on CPU 0
[00:00:16.718,010] &amp;lt;err&amp;gt; os: Current thread: 0x100b48a8 (unknown)
[00:00:16.777,075] &amp;lt;err&amp;gt; os: Halting system&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 30 Oct 2025 00:08:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Zephyr-Project/Zephyr-BLE-examples-for-RW610/m-p/2195308#M518</guid>
      <dc:creator>snjy</dc:creator>
      <dc:date>2025-10-30T00:08:33Z</dc:date>
    </item>
    <item>
      <title>Re: Zephyr BLE examples for RW610</title>
      <link>https://community.nxp.com/t5/Zephyr-Project/Zephyr-BLE-examples-for-RW610/m-p/2195508#M519</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/255823"&gt;@snjy&lt;/a&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;there is no dedicated dev board for the chip.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;You are custom a board with rw610? we provide frdm board and evk for development and our partener have rw61x based modules.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Shaun&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 30 Oct 2025 06:11:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Zephyr-Project/Zephyr-BLE-examples-for-RW610/m-p/2195508#M519</guid>
      <dc:creator>shaun_wu</dc:creator>
      <dc:date>2025-10-30T06:11:54Z</dc:date>
    </item>
    <item>
      <title>Re: Zephyr BLE examples for RW610</title>
      <link>https://community.nxp.com/t5/Zephyr-Project/Zephyr-BLE-examples-for-RW610/m-p/2195512#M520</link>
      <description>&lt;P&gt;If custom a board, nxp need to review the design and make sure the custom board meet our request.&lt;/P&gt;</description>
      <pubDate>Thu, 30 Oct 2025 06:14:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Zephyr-Project/Zephyr-BLE-examples-for-RW610/m-p/2195512#M520</guid>
      <dc:creator>shaun_wu</dc:creator>
      <dc:date>2025-10-30T06:14:18Z</dc:date>
    </item>
  </channel>
</rss>