<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX93evk zephyr RS485 in Zephyr Project</title>
    <link>https://community.nxp.com/t5/Zephyr-Project/IMX93evk-zephyr-RS485/m-p/2181107#M495</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have been working on this issue for 2 days now and I am not progressing anymore. I am trying to use OSDP in Zephyr through the control_panel example. I have provided my files in the zip I attached below.&amp;nbsp;&lt;/P&gt;&lt;P&gt;My wiring is as follows:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="zefox_0-1759829994100.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/359728i9A722B0349B9C870/image-size/medium?v=v2&amp;amp;px=400" role="button" title="zefox_0-1759829994100.png" alt="zefox_0-1759829994100.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I have checked that the GPIO17 is indeed multiplexed correctly. This is correct.&lt;BR /&gt;I have tried using pull-down resistors (10K) on the DE&amp;amp;/RE pin. Didn't do anything.&lt;BR /&gt;I have tried sending test data directly using the serial driver in Zephyr. Didn't work.&lt;/P&gt;&lt;P&gt;I can tell it is sending correctly because my reader is correctly receiving a message. But the DE pin always stays high. This means it won't receive anything. Which is exactly what I am observing.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have had this issue with the STmicroelectronics UART driver as well where the hardware-controlled DE pin had the same issue.&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do i fix this issue&lt;/P&gt;</description>
    <pubDate>Tue, 07 Oct 2025 09:40:44 GMT</pubDate>
    <dc:creator>zefox</dc:creator>
    <dc:date>2025-10-07T09:40:44Z</dc:date>
    <item>
      <title>IMX93evk zephyr RS485</title>
      <link>https://community.nxp.com/t5/Zephyr-Project/IMX93evk-zephyr-RS485/m-p/2181107#M495</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have been working on this issue for 2 days now and I am not progressing anymore. I am trying to use OSDP in Zephyr through the control_panel example. I have provided my files in the zip I attached below.&amp;nbsp;&lt;/P&gt;&lt;P&gt;My wiring is as follows:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="zefox_0-1759829994100.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/359728i9A722B0349B9C870/image-size/medium?v=v2&amp;amp;px=400" role="button" title="zefox_0-1759829994100.png" alt="zefox_0-1759829994100.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I have checked that the GPIO17 is indeed multiplexed correctly. This is correct.&lt;BR /&gt;I have tried using pull-down resistors (10K) on the DE&amp;amp;/RE pin. Didn't do anything.&lt;BR /&gt;I have tried sending test data directly using the serial driver in Zephyr. Didn't work.&lt;/P&gt;&lt;P&gt;I can tell it is sending correctly because my reader is correctly receiving a message. But the DE pin always stays high. This means it won't receive anything. Which is exactly what I am observing.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have had this issue with the STmicroelectronics UART driver as well where the hardware-controlled DE pin had the same issue.&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do i fix this issue&lt;/P&gt;</description>
      <pubDate>Tue, 07 Oct 2025 09:40:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Zephyr-Project/IMX93evk-zephyr-RS485/m-p/2181107#M495</guid>
      <dc:creator>zefox</dc:creator>
      <dc:date>2025-10-07T09:40:44Z</dc:date>
    </item>
    <item>
      <title>Re: IMX93evk zephyr RS485</title>
      <link>https://community.nxp.com/t5/Zephyr-Project/IMX93evk-zephyr-RS485/m-p/2181390#M496</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252157"&gt;@zefox&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Unfortunately, this channel does not provide support to Zephyr.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Salas.&lt;/P&gt;</description>
      <pubDate>Tue, 07 Oct 2025 17:39:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Zephyr-Project/IMX93evk-zephyr-RS485/m-p/2181390#M496</guid>
      <dc:creator>Manuel_Salas</dc:creator>
      <dc:date>2025-10-07T17:39:09Z</dc:date>
    </item>
  </channel>
</rss>