<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Zephyr Projectのトピックdrivers: enet: eth_nxp_enet_mac: Could not alloc RX pkt</title>
    <link>https://community.nxp.com/t5/Zephyr-Project/drivers-enet-eth-nxp-enet-mac-Could-not-alloc-RX-pkt/m-p/2128081#M398</link>
    <description>&lt;P&gt;I am seeing this "Could not alloc RX pkt" error message with NXP MCXN947 - http_server example.&lt;/P&gt;&lt;P&gt;At the beginning, it all seems okay however after 10 minutes the network statistics freezes and after 5 - 10 minutes I see this error.&lt;/P&gt;&lt;P&gt;When this error appears everything freezes.&lt;/P&gt;&lt;P&gt;This is environment:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;OS: Windows&lt;BR /&gt;Zephyr: 4.1.99&lt;BR /&gt;Board: NXP FRDM MCXN947&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;To reproduce the issue:&lt;/P&gt;&lt;P&gt;Take the sample http_server code and add the following line to the prj.conf&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;CONFIG_ETH_NXP_ENET_QOS_TX_BUFFER_DESCRIPTORS=16&lt;BR /&gt;CONFIG_ETH_NXP_ENET_QOS_RX_BUFFER_DESCRIPTORS=16&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Is this something to do with Zephyr?&lt;/P&gt;</description>
    <pubDate>Thu, 03 Jul 2025 12:14:37 GMT</pubDate>
    <dc:creator>elby</dc:creator>
    <dc:date>2025-07-03T12:14:37Z</dc:date>
    <item>
      <title>drivers: enet: eth_nxp_enet_mac: Could not alloc RX pkt</title>
      <link>https://community.nxp.com/t5/Zephyr-Project/drivers-enet-eth-nxp-enet-mac-Could-not-alloc-RX-pkt/m-p/2128081#M398</link>
      <description>&lt;P&gt;I am seeing this "Could not alloc RX pkt" error message with NXP MCXN947 - http_server example.&lt;/P&gt;&lt;P&gt;At the beginning, it all seems okay however after 10 minutes the network statistics freezes and after 5 - 10 minutes I see this error.&lt;/P&gt;&lt;P&gt;When this error appears everything freezes.&lt;/P&gt;&lt;P&gt;This is environment:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;OS: Windows&lt;BR /&gt;Zephyr: 4.1.99&lt;BR /&gt;Board: NXP FRDM MCXN947&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;To reproduce the issue:&lt;/P&gt;&lt;P&gt;Take the sample http_server code and add the following line to the prj.conf&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;CONFIG_ETH_NXP_ENET_QOS_TX_BUFFER_DESCRIPTORS=16&lt;BR /&gt;CONFIG_ETH_NXP_ENET_QOS_RX_BUFFER_DESCRIPTORS=16&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Is this something to do with Zephyr?&lt;/P&gt;</description>
      <pubDate>Thu, 03 Jul 2025 12:14:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Zephyr-Project/drivers-enet-eth-nxp-enet-mac-Could-not-alloc-RX-pkt/m-p/2128081#M398</guid>
      <dc:creator>elby</dc:creator>
      <dc:date>2025-07-03T12:14:37Z</dc:date>
    </item>
    <item>
      <title>Re: drivers: enet: eth_nxp_enet_mac: Could not alloc RX pkt</title>
      <link>https://community.nxp.com/t5/Zephyr-Project/drivers-enet-eth-nxp-enet-mac-Could-not-alloc-RX-pkt/m-p/2129046#M410</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/250355"&gt;@elby&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I see a similar issue in&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;EM&gt;Zephyr project&lt;/EM&gt;:&lt;/P&gt;
&lt;P&gt;&lt;A style="background-color: #ffffff; outline: 0px;" href="https://github.com/zephyrproject-rtos/zephyr/issues/85172" target="_blank"&gt;ETH NXP MCXN: eth_nxp_enet_qos buffer problem · Issue #85172 · zephyrproject-rtos/zephyr&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I think you can discuss it here, where experts on the subject can help you.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Mon, 07 Jul 2025 06:30:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Zephyr-Project/drivers-enet-eth-nxp-enet-mac-Could-not-alloc-RX-pkt/m-p/2129046#M410</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2025-07-07T06:30:40Z</dc:date>
    </item>
  </channel>
</rss>