<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Zephyr ProjectのトピックRe: RPMsg support for m33 core on i.mx93</title>
    <link>https://community.nxp.com/t5/Zephyr-Project/RPMsg-support-for-m33-core-on-i-mx93/m-p/2035259#M266</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245680"&gt;@Louis-HQ&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope you are doing very well.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;At this date (January of 2025), Zephyr is just as it is, the shared examples for cortex M and Cortex A on SDK.&lt;/P&gt;
&lt;P&gt;We have not information about if RPMSG will be supported for Zephyr in Cortex M.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Salas.&lt;/P&gt;</description>
    <pubDate>Tue, 28 Jan 2025 18:52:57 GMT</pubDate>
    <dc:creator>Manuel_Salas</dc:creator>
    <dc:date>2025-01-28T18:52:57Z</dc:date>
    <item>
      <title>RPMsg support for m33 core on i.mx93</title>
      <link>https://community.nxp.com/t5/Zephyr-Project/RPMsg-support-for-m33-core-on-i-mx93/m-p/2035191#M265</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;As of now, I don't believe that the&amp;nbsp;i.mx93 zephyr port provides facilities to implement messaging between the m33 core running zephyr and the A55 cores running Linux using a framework such as RPMsg. The &lt;A title="imx93 m33 device tree" href="https://github.com/zephyrproject-rtos/zephyr/blob/main/dts/arm/nxp/nxp_imx93_m33.dtsi" target="_blank" rel="noopener"&gt;device tree&lt;/A&gt; exposes a DTCM which could be used as a internal shared memory, but no internal interrupt mechanism between the cores as far as I can see.&lt;/P&gt;&lt;P&gt;Is there something on the roadmap to improve support of zephyr development on the m33 core?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 28 Jan 2025 16:00:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Zephyr-Project/RPMsg-support-for-m33-core-on-i-mx93/m-p/2035191#M265</guid>
      <dc:creator>Louis-HQ</dc:creator>
      <dc:date>2025-01-28T16:00:45Z</dc:date>
    </item>
    <item>
      <title>Re: RPMsg support for m33 core on i.mx93</title>
      <link>https://community.nxp.com/t5/Zephyr-Project/RPMsg-support-for-m33-core-on-i-mx93/m-p/2035259#M266</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245680"&gt;@Louis-HQ&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope you are doing very well.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;At this date (January of 2025), Zephyr is just as it is, the shared examples for cortex M and Cortex A on SDK.&lt;/P&gt;
&lt;P&gt;We have not information about if RPMSG will be supported for Zephyr in Cortex M.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Salas.&lt;/P&gt;</description>
      <pubDate>Tue, 28 Jan 2025 18:52:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Zephyr-Project/RPMsg-support-for-m33-core-on-i-mx93/m-p/2035259#M266</guid>
      <dc:creator>Manuel_Salas</dc:creator>
      <dc:date>2025-01-28T18:52:57Z</dc:date>
    </item>
    <item>
      <title>Re: RPMsg support for m33 core on i.mx93</title>
      <link>https://community.nxp.com/t5/Zephyr-Project/RPMsg-support-for-m33-core-on-i-mx93/m-p/2064979#M281</link>
      <description>&lt;P&gt;RPMsg is supported for Linux to RTOS communication in NXP's Real-Time Edge software framework. RTOS support includes Zephyr (along with FreeRTOS and bare metal). You can find out more about this at &lt;A href="https://nxp.com/rtedge" target="_blank"&gt;https://nxp.com/rtedge&lt;/A&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 19 Mar 2025 21:00:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Zephyr-Project/RPMsg-support-for-m33-core-on-i-mx93/m-p/2064979#M281</guid>
      <dc:creator>brendonslade</dc:creator>
      <dc:date>2025-03-19T21:00:08Z</dc:date>
    </item>
  </channel>
</rss>