<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wi-Fi® + Bluetooth® + 802.15.4のトピックCMP9010 wifi module integration</title>
    <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/CMP9010-wifi-module-integration/m-p/1509066#M568</link>
    <description>&lt;P&gt;I have bought a &lt;SPAN class=""&gt;&lt;SPAN&gt;CMP9010-1-EVB&lt;/SPAN&gt;&lt;/SPAN&gt; from mouser. The board has an CEL CMP9010 module, which is based on iw416. CEL provides a brief description on hardware on their web site but no further documentation on software integration.&lt;/P&gt;&lt;P&gt;The module is not listed in latest SDK for my imxrt1020 evk board. There are three modules based on iw416. One from murata and others from azurewave.&lt;/P&gt;&lt;P&gt;I wonder what I could do to bring it up. Is it compatible with a module from azurewave or murata? Or I must wait for a new SDK release including this module? Or perhaps I can get help here.&lt;/P&gt;</description>
    <pubDate>Sun, 21 Aug 2022 21:02:59 GMT</pubDate>
    <dc:creator>gingerologist</dc:creator>
    <dc:date>2022-08-21T21:02:59Z</dc:date>
    <item>
      <title>CMP9010 wifi module integration</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/CMP9010-wifi-module-integration/m-p/1509066#M568</link>
      <description>&lt;P&gt;I have bought a &lt;SPAN class=""&gt;&lt;SPAN&gt;CMP9010-1-EVB&lt;/SPAN&gt;&lt;/SPAN&gt; from mouser. The board has an CEL CMP9010 module, which is based on iw416. CEL provides a brief description on hardware on their web site but no further documentation on software integration.&lt;/P&gt;&lt;P&gt;The module is not listed in latest SDK for my imxrt1020 evk board. There are three modules based on iw416. One from murata and others from azurewave.&lt;/P&gt;&lt;P&gt;I wonder what I could do to bring it up. Is it compatible with a module from azurewave or murata? Or I must wait for a new SDK release including this module? Or perhaps I can get help here.&lt;/P&gt;</description>
      <pubDate>Sun, 21 Aug 2022 21:02:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/CMP9010-wifi-module-integration/m-p/1509066#M568</guid>
      <dc:creator>gingerologist</dc:creator>
      <dc:date>2022-08-21T21:02:59Z</dc:date>
    </item>
    <item>
      <title>Re: CMP9010 wifi module integration</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/CMP9010-wifi-module-integration/m-p/1509285#M569</link>
      <description>&lt;P&gt;Dear&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205315"&gt;@gingerologist&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;NXP IW416 chipset is supported on most of the i.MX RT hosts, using latest SDK 2.12:&lt;/P&gt;&lt;P&gt;- i.MX RT 1020, 1064, 1160: wifi only supported&lt;/P&gt;&lt;P&gt;- i.MX RT 1050, 1060, 1170, 685, 595 both wifi and BT supported&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We could not test CEL CMP9010 module, but we assume it should work by selecting one of the WIFI_IW416_BOARD_*_USD flag in source/app_config.h.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/183357"&gt;@bruce_havemeier&lt;/a&gt;&amp;nbsp;could you help on that request ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Olivier&lt;/P&gt;</description>
      <pubDate>Mon, 22 Aug 2022 07:29:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/CMP9010-wifi-module-integration/m-p/1509285#M569</guid>
      <dc:creator>ocourson</dc:creator>
      <dc:date>2022-08-22T07:29:46Z</dc:date>
    </item>
    <item>
      <title>Re: CMP9010 wifi module integration</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/CMP9010-wifi-module-integration/m-p/1509465#M570</link>
      <description>&lt;P&gt;Matian and oliver...I sent Matian the CMP9010-1-EVB quick start guide in a private email.&amp;nbsp; Also, I have put him in touch with our lead software engineer.&lt;/P&gt;&lt;P&gt;-Bruce&lt;/P&gt;</description>
      <pubDate>Mon, 22 Aug 2022 10:39:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/CMP9010-wifi-module-integration/m-p/1509465#M570</guid>
      <dc:creator>bruce_havemeier</dc:creator>
      <dc:date>2022-08-22T10:39:14Z</dc:date>
    </item>
    <item>
      <title>Re: CMP9010 wifi module integration</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/CMP9010-wifi-module-integration/m-p/1509730#M571</link>
      <description>&lt;P&gt;Thank you for your reply and also thanks to Bruce Havemeier, I have received his email with some hardware documents.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Besides, I had some luck today. After carefully reading all related documents, I did the following steps:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. Connect micro USB power to CMP9010 EVB and set jumper J1 to REG ('down position' according to quick start guide provided by CEL).&lt;/P&gt;&lt;P&gt;2. set J2 on CMP9010 EVB to 1.8V ('down position' according to quick start guide provided by CEL)&lt;/P&gt;&lt;P&gt;3. in app_config.h, comment out definition of "WIFI_88W8801_BOARD_AW_NM191_USD", define "WIFI_IW416_BOARD_AW_AM510_USD" instead.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then at lease the "xxxx_wifi_setup" example works. I got the following output from serial console (/dev/ttyACM0 on my linux desktop).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;```&lt;/P&gt;&lt;P&gt;Wifi setup example&lt;BR /&gt;Initialize WLAN Driver&lt;BR /&gt;MAC Address: 00:22:A3:07:25:07&lt;BR /&gt;[net] Initialized TCP/IP networking stack&lt;BR /&gt;app_cb: WLAN: received event 10&lt;BR /&gt;app_cb: WLAN initialized&lt;BR /&gt;WLAN Driver Version : v1.3.r37.p3&lt;BR /&gt;WLAN Firmware Version : IW416-V0, RF878X, FP91, 16.91.21.p11.3, WPA2_CVE_FIX 1, PVE_FIX 1&lt;BR /&gt;Scan scheduled...&lt;BR /&gt;10 networks found:&lt;BR /&gt;18:31:BF:00:D1:1C "ASUS_5G"&lt;BR /&gt;channel: 149&lt;BR /&gt;rssi: -60 dBm&lt;BR /&gt;security: WPA2&lt;BR /&gt;WMM: YES&lt;BR /&gt;18:31:BF:00:D1:18 "ASUS"&lt;BR /&gt;channel: 2&lt;BR /&gt;rssi: -65 dBm&lt;BR /&gt;security: WPA2&lt;BR /&gt;WMM: YES&lt;BR /&gt;D8:8A:DC:D4:1B:D4 "HAPPINESS"&lt;BR /&gt;channel: 6&lt;BR /&gt;rssi: -56 dBm&lt;BR /&gt;security: WPA2&lt;BR /&gt;WMM: YES&lt;BR /&gt;D8:8A:DC:D4:87:D0 "HAPPINESS"&lt;BR /&gt;channel: 6&lt;BR /&gt;rssi: -81 dBm&lt;BR /&gt;security: WPA2&lt;BR /&gt;WMM: YES&lt;BR /&gt;D8:8A:DC:D4:87:D1 (hidden)&lt;BR /&gt;channel: 6&lt;BR /&gt;rssi: -82 dBm&lt;BR /&gt;security: WPA2&lt;BR /&gt;WMM: YES&lt;BR /&gt;D8:8A:DC:D4:1B:D5 (hidden)&lt;BR /&gt;channel: 6&lt;BR /&gt;rssi: -54 dBm&lt;BR /&gt;security: WPA2&lt;BR /&gt;WMM: YES&lt;BR /&gt;EC:26:CA:90:F6:BB "juwanke-test-a5a5a5a5"&lt;BR /&gt;channel: 11&lt;BR /&gt;rssi: -19 dBm&lt;BR /&gt;security: WPA/WPA2 Mixed&lt;BR /&gt;WMM: YES&lt;BR /&gt;D8:8A:DC:F4:1B:D8 (hidden)&lt;BR /&gt;channel: 149&lt;BR /&gt;rssi: -56 dBm&lt;BR /&gt;security: WPA2&lt;BR /&gt;WMM: YES&lt;BR /&gt;3E:06:A7:4C:A3:BA (hidden)&lt;BR /&gt;channel: 11&lt;BR /&gt;rssi: -91 dBm&lt;BR /&gt;security: WPA/WPA2 Mixed&lt;BR /&gt;WMM: YES&lt;BR /&gt;D8:8A:DC:D4:1B:D8 "HAPPINESS"&lt;BR /&gt;channel: 149&lt;BR /&gt;rssi: -57 dBm&lt;BR /&gt;security: WPA2&lt;BR /&gt;WMM: YES&lt;BR /&gt;Connecting to SSID .....app_cb: WLAN: received event 2&lt;BR /&gt;[!] WLAN: network not found&lt;BR /&gt;Connection Failed! Stopping!&lt;/P&gt;&lt;P&gt;```&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Aug 2022 22:00:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/CMP9010-wifi-module-integration/m-p/1509730#M571</guid>
      <dc:creator>gingerologist</dc:creator>
      <dc:date>2022-08-22T22:00:27Z</dc:date>
    </item>
  </channel>
</rss>