<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: wlan: mlan0 START SCAN in Wi-Fi® + Bluetooth® + 802.15.4</title>
    <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/wlan-mlan0-START-SCAN/m-p/1858965#M56</link>
    <description>I am also getting same problem could you please share correction which is required dram side.</description>
    <pubDate>Fri, 03 May 2024 13:55:00 GMT</pubDate>
    <dc:creator>masateesh</dc:creator>
    <dc:date>2024-05-03T13:55:00Z</dc:date>
    <item>
      <title>wlan: mlan0 START SCAN</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/wlan-mlan0-START-SCAN/m-p/1405654#M50</link>
      <description>&lt;P&gt;In rare cases, a custom board equipped with i.MX8MQ keeps failing to scan Wi-Fi.&lt;BR /&gt;If the scan is successful, the connection will be completed in about 10 seconds, but if an ABORT SCAN occurs, it will not return.&lt;BR /&gt;The wi-fi module we are using is 88W9098.&lt;/P&gt;&lt;P&gt;I have changed the moal log level to 2 and am analyzing it, but it doesn't seem to output any significant logs.&lt;BR /&gt;If anyone has solved a similar problem, please let me know how to solve it.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;[ 11.428717] mlan: loading out-of-tree module taints kernel.&lt;BR /&gt;[ 11.454906] wlan: Loading MWLAN driver&lt;BR /&gt;[ 11.455385] wlan_pcie 0000:01:00.0: enabling device (0000 -&amp;gt; 0002)&lt;BR /&gt;[ 11.455449] Attach moal handle ops, card interface type: 0x206&lt;BR /&gt;[ 11.456183] PCIE9098: init module param from usr cfg&lt;BR /&gt;[ 11.456231] card_type: PCIE9098, config block: 0&lt;BR /&gt;[ 11.456237] cfg80211_wext=0xf&lt;BR /&gt;[ 11.456241] wfd_name=p2p&lt;BR /&gt;[ 11.456245] max_vir_bss=1&lt;BR /&gt;[ 11.456249] cal_data_cfg=none&lt;BR /&gt;[ 11.456253] drv_mode = 7&lt;BR /&gt;[ 11.456256] ps_mode = 2&lt;BR /&gt;[ 11.456259] auto_ds = 2&lt;BR /&gt;[ 11.456263] fw_name=nxp/pcieuart9098_combo_v1.bin&lt;BR /&gt;[ 11.456270] host_mlme=enable&lt;BR /&gt;[ 11.456316] rx_work=1 cpu_num=4&lt;BR /&gt;[ 11.456331] Attach mlan adapter operations.card_type is 0x206.&lt;BR /&gt;[ 11.458146] Request firmware: nxp/pcieuart9098_combo_v1.bin&lt;BR /&gt;[ 12.026570] FW download over, size 618724 bytes&lt;BR /&gt;[ 12.552662] ddrc freq set to low bus mode&lt;BR /&gt;[ 12.890879] WLAN FW is active&lt;BR /&gt;[ 12.890904] on_time is 12888812952&lt;BR /&gt;[ 12.905158] fw_cap_info=0x81c3fa3, dev_cap_mask=0xffffffff&lt;BR /&gt;[ 12.905361] max_p2p_conn = 8, max_sta_conn = 64&lt;BR /&gt;[ 12.961013] ddrc freq set to high bus mode&lt;BR /&gt;[ 12.961124] wlan: version = PCIE9098--17.92.5.p3-MM5X17247.p5-GPL-(FP92)&lt;BR /&gt;[ 12.961726] wlan_pcie 0000:01:00.1: enabling device (0000 -&amp;gt; 0002)&lt;BR /&gt;[ 12.961795] Attach moal handle ops, card interface type: 0x206&lt;BR /&gt;[ 12.961889] PCIE9098: init module param from usr cfg&lt;BR /&gt;[ 12.961940] card_type: PCIE9098, config block: 1&lt;BR /&gt;[ 12.961947] cfg80211_wext=0xf&lt;BR /&gt;[ 12.961951] wfd_name=p2p&lt;BR /&gt;[ 12.961954] max_vir_bss=1&lt;BR /&gt;[ 12.961959] cal_data_cfg=none&lt;BR /&gt;[ 12.961962] drv_mode = 7&lt;BR /&gt;[ 12.961965] ps_mode = 2&lt;BR /&gt;[ 12.961968] auto_ds = 2&lt;BR /&gt;[ 12.961972] fw_name=nxp/pcieuart9098_combo_v1.bin&lt;BR /&gt;[ 12.961979] host_mlme=enable&lt;BR /&gt;[ 12.961994] rx_work=1 cpu_num=4&lt;BR /&gt;[ 12.962012] Attach mlan adapter operations.card_type is 0x206.&lt;BR /&gt;[ 12.966172] Request firmware: nxp/pcieuart9098_combo_v1.bin&lt;BR /&gt;[ 12.967101] WLAN FW already running! Skip FW download&lt;BR /&gt;[ 12.967112] WLAN FW is active&lt;BR /&gt;[ 12.967119] on_time is 12965036475&lt;BR /&gt;[ 12.969398] fw_cap_info=0x81c3fa3, dev_cap_mask=0xffffffff&lt;BR /&gt;[ 12.969427] max_p2p_conn = 8, max_sta_conn = 64&lt;BR /&gt;[ 12.988979] wlan: version = PCIE9098--17.92.5.p3-MM5X17247.p5-GPL-(FP92)&lt;BR /&gt;[ 12.989366] wlan: Driver loaded successfully&lt;BR /&gt;[ 14.187052] wlan: mlan0 START SCAN&lt;BR /&gt;[ 15.268701] ddrc freq set to low bus mode&lt;BR /&gt;[ 24.188103] &lt;STRONG&gt;wlan: ABORT SCAN start&lt;/STRONG&gt;&lt;BR /&gt;[ 24.188330] &lt;STRONG&gt;IOCTL failed: 000000006991828c id=0x10000, sub_id=0x10003 action=1, status_code=0x80000007&lt;/STRONG&gt;&lt;BR /&gt;[ 29.205726] wlan: mlan0 START SCAN&lt;BR /&gt;[ 33.511905] ddrc freq set to high bus mode&lt;BR /&gt;[ 34.596334] ddrc freq set to low bus mode&lt;BR /&gt;[ 39.207750] &lt;STRONG&gt;wlan: ABORT SCAN start&lt;/STRONG&gt;&lt;BR /&gt;[ 39.207972] &lt;STRONG&gt;IOCTL failed: 00000000de34e17e id=0x10000, sub_id=0x10003 action=1, status_code=0x80000007&lt;/STRONG&gt;&lt;BR /&gt;[ 43.751761] ddrc freq set to high bus mode&lt;BR /&gt;[ 44.222069] wlan: mlan0 START SCAN&lt;BR /&gt;[ 44.836336] ddrc freq set to low bus mode&lt;BR /&gt;[ 48.872768] ddrc freq set to high bus mode&lt;BR /&gt;[ 49.961326] ddrc freq set to low bus mode&lt;BR /&gt;[ 54.223771] &lt;STRONG&gt;wlan: ABORT SCAN start&lt;/STRONG&gt;&lt;BR /&gt;[ 54.224010] &lt;STRONG&gt;IOCTL failed: 00000000dd8cf28c id=0x10000, sub_id=0x10003 action=1, status_code=0x80000007&lt;/STRONG&gt;&lt;BR /&gt;[ 64.231817] ddrc freq set to high bus mode&lt;BR /&gt;[ 65.316338] ddrc freq set to low bus mode&lt;BR /&gt;[ 67.393538] ddrc freq set to high bus mode&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 27 Jan 2022 02:30:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/wlan-mlan0-START-SCAN/m-p/1405654#M50</guid>
      <dc:creator>KentarouFujita</dc:creator>
      <dc:date>2022-01-27T02:30:32Z</dc:date>
    </item>
    <item>
      <title>Re: wlan: mlan0 START SCAN</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/wlan-mlan0-START-SCAN/m-p/1407319#M51</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Is the issue happening in the same custom board ? Could you please share the configuration settings you have ? According to the log you shared, you are using the latest version of &lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=In-Depth_Tab" target="_self"&gt;this&lt;/A&gt; release, could you please help me confirm if you are and also are you using the default driver or are you using another driver ?&amp;nbsp; Is there some pattern identified when the scan fails ? &lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Estephania&lt;/P&gt;</description>
      <pubDate>Mon, 31 Jan 2022 22:19:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/wlan-mlan0-START-SCAN/m-p/1407319#M51</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2022-01-31T22:19:11Z</dc:date>
    </item>
    <item>
      <title>Re: wlan: mlan0 START SCAN</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/wlan-mlan0-START-SCAN/m-p/1407799#M52</link>
      <description>&lt;P&gt;Hi Estephania!&lt;/P&gt;&lt;P&gt;&amp;gt;Is the problem happening on the same custom board?&lt;BR /&gt;Yes, the problem is happening on the same custom board.&lt;/P&gt;&lt;P&gt;&amp;gt;Please let me know your configuration settings.&lt;BR /&gt;I am attaching my defconfig and dts.&lt;BR /&gt;The defconfig is almost unchanged from BSP (imx8mqevk).&lt;/P&gt;&lt;P&gt;&amp;gt;According to your log, you are using the latest version of this release, please confirm and tell me if you are using the default driver or some other driver.&lt;BR /&gt;I am not using the default driver.&lt;BR /&gt;The moal and pcieuart9098_combo_v1.bin are using Linux 5.10.72_2.2.0, as I initially suspected a driver problem.&lt;BR /&gt;However, the same phenomenon occurred with Linux 5.10.35_2.0.0.&lt;/P&gt;&lt;P&gt;&amp;gt;Is there any pattern when the scan fails?&lt;BR /&gt;There is no particular pattern when the scan fails.&lt;BR /&gt;When I start up moal and wpa_supplicant after the kernel starts, ABORT SCAN occurs evenly.&lt;/P&gt;</description>
      <pubDate>Wed, 02 Feb 2022 00:21:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/wlan-mlan0-START-SCAN/m-p/1407799#M52</guid>
      <dc:creator>KentarouFujita</dc:creator>
      <dc:date>2022-02-02T00:21:36Z</dc:date>
    </item>
    <item>
      <title>Re: wlan: mlan0 START SCAN</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/wlan-mlan0-START-SCAN/m-p/1408424#M53</link>
      <description>&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&amp;gt;moal and pcieuart9098_combo_v1.bin, I first suspected a driver problem and used Linux 5.10.72_2.2.0.&lt;BR /&gt;Sorry, this is a mistake. When I got the first log, the mall and firmware version defaulted to 5.10.35_2.0.0.&lt;BR /&gt;It is still at 5.10.35_2.0.0.&lt;/P&gt;&lt;P&gt;I referred to UM11490 to get the moal and firmware logs.&lt;BR /&gt;I set the debug flag (drvbdg) for moal to 0x60000207.&lt;/P&gt;&lt;P&gt;The dmesg does not seem to have changed from the first log I posted.&lt;BR /&gt;In the firmware dump, there was a log in file_drv_info that I found interesting.&lt;BR /&gt;The value of num_cmd_assoc_failure is set to 1.&lt;BR /&gt;UM11490 does not have a detailed description of the dump file, so I don't know what this represents.&lt;BR /&gt;Does "num_cmd_assoc_failure = 1" have anything to do with ABORT SCAN?&lt;/P&gt;&lt;P&gt;I'm looking for clues to solve the problem, whatever it may be.&lt;BR /&gt;Any information is welcome.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 03 Feb 2022 06:32:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/wlan-mlan0-START-SCAN/m-p/1408424#M53</guid>
      <dc:creator>KentarouFujita</dc:creator>
      <dc:date>2022-02-03T06:32:37Z</dc:date>
    </item>
    <item>
      <title>Re: wlan: mlan0 START SCAN</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/wlan-mlan0-START-SCAN/m-p/1410573#M54</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I have been checking this and I have not been able to reproduce it with my setup, we might need more details on this setup that you have. I already sent you a message directly, could you please help me check it ?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Feb 2022 00:02:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/wlan-mlan0-START-SCAN/m-p/1410573#M54</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2022-02-09T00:02:46Z</dc:date>
    </item>
    <item>
      <title>Re: wlan: mlan0 START SCAN</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/wlan-mlan0-START-SCAN/m-p/1425909#M55</link>
      <description>&lt;P&gt;This case was due to memory corruption caused by an inadequate DRAM configuration.&lt;/P&gt;&lt;P&gt;The problem has now been resolved.&lt;BR /&gt;This ticket has served its purpose and is closed.&lt;/P&gt;</description>
      <pubDate>Thu, 10 Mar 2022 07:26:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/wlan-mlan0-START-SCAN/m-p/1425909#M55</guid>
      <dc:creator>KentarouFujita</dc:creator>
      <dc:date>2022-03-10T07:26:45Z</dc:date>
    </item>
    <item>
      <title>Re: wlan: mlan0 START SCAN</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/wlan-mlan0-START-SCAN/m-p/1858965#M56</link>
      <description>I am also getting same problem could you please share correction which is required dram side.</description>
      <pubDate>Fri, 03 May 2024 13:55:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/wlan-mlan0-START-SCAN/m-p/1858965#M56</guid>
      <dc:creator>masateesh</dc:creator>
      <dc:date>2024-05-03T13:55:00Z</dc:date>
    </item>
    <item>
      <title>Re: wlan: mlan0 START SCAN</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/wlan-mlan0-START-SCAN/m-p/1858968#M57</link>
      <description>I am also facing above issue.&lt;BR /&gt;&lt;BR /&gt;here is my log I have observed some times wifi driver ioctl failed. I am using sdiouartiw416_combo_v0.bin loading driver sudo modprobe moal mod_para=nxp/wifi_mod_para.conf.&lt;BR /&gt;&lt;BR /&gt;[ 2249.074648] wlan: wfd0 START SCAN&lt;BR /&gt;[ 2660.394617] wlan: SCAN COMPLETED: scanned AP count=30&lt;BR /&gt;[ 2254.854750] wlan: mlan0 START SCAN&lt;BR /&gt;[ 2259.914505] wlan: SCAN COMPLETED: scanned AP count=35&lt;BR /&gt;[ 2312.324716] wlan: SCAN COMPLETED: scanned AP count=31&lt;BR /&gt;[ 2312.684583] wlan: wfd0 START SCAN&lt;BR /&gt;[ 2666.224503] wlan: SCAN COMPLETED: scanned AP count=39&lt;BR /&gt;[ 2666.972040] wlan: wfd0 START SCANN&lt;BR /&gt;[ 2672.064528] wlan: SCAN COMPLETED: scanned AP count=37&lt;BR /&gt;[ 2407.364646] wlan: SCAN COMPLETED: scanned AP count=32&lt;BR /&gt;[ 2407.928449] wlan: wfd0 START SCAN&lt;BR /&gt;[ 2412.994503] wlan: SCAN COMPLETED: scanned AP count=32&lt;BR /&gt;[ 2413.405633] wlan: mlan0 START SCAN&lt;BR /&gt;[ 2418.534565] wlan: SCAN COMPLETED: scanned AP count=35&lt;BR /&gt;[ 2528.394626] wlan: SCAN COMPLETED: scanned AP count=31&lt;BR /&gt;[ 2529.165897] wlan: wfd0 START SCAN&lt;BR /&gt;[ 2534.234496] wlan: SCAN COMPLETED: scanned AP count=33&lt;BR /&gt;[ 2534.965963] wlan: mlan0 START SCAN&lt;BR /&gt;[ 2540.084709] wlan: SCAN COMPLETED: scanned AP count=34&lt;BR /&gt;[ 2544.424473] wlan: SCAN COMPLETED: scanned AP count=16&lt;BR /&gt;[ 2545.027157] wlan: mlan0 START SCAN&lt;BR /&gt;[ 2550.104524] wlan: SCAN COMPLETED: scanned AP count=31&lt;BR /&gt;[ 2554.164474] wlan: SCAN COMPLETED: scanned AP count=22&lt;BR /&gt;[ 2554.565009] wlan: mlan0 START SCAN&lt;BR /&gt;[ 2559.624488] wlan: SCAN COMPLETED: scanned AP count=30&lt;BR /&gt;[ 2559.900300] wlan: wfd0 START SCAN&lt;BR /&gt;[ 2564.954503] wlan: SCAN COMPLETED: scanned AP count=34&lt;BR /&gt;[ 2565.644052] wlan: wfd0 START SCAN&lt;BR /&gt;[ 2570.904533] wlan: SCAN COMPLETED: scanned AP count=37&lt;BR /&gt;[ 2571.604640] wlan: wfd0 START SCAN&lt;BR /&gt;[ 2576.634507] wlan: SCAN COMPLETED: scanned AP count=36&lt;BR /&gt;[ 2576.674711] wlan: sched scan start&lt;BR /&gt;[ 2580.994510] wlan: SCAN COMPLETED: scanned AP count=22&lt;BR /&gt;[ 2581.824932] wlan: wfd0 START SCAN&lt;BR /&gt;[ 2586.974511] wlan: SCAN COMPLETED: scanned AP count=34&lt;BR /&gt;[ 2591.424516] wlan: SCAN COMPLETED: scanned AP count=23&lt;BR /&gt;[ 2591.498128] wlan: sched scan stop&lt;BR /&gt;[ 2592.215838] wlan: mlan0 START SCAN&lt;BR /&gt;[ 2597.324500] wlan: SCAN COMPLETED: scanned AP count=33&lt;BR /&gt;[ 2601.864495] wlan: SCAN COMPLETED: scanned AP count=26&lt;BR /&gt;[ 2602.588863] wlan: mlan0 START SCAN&lt;BR /&gt;[ 2607.664489] wlan: SCAN COMPLETED: scanned AP count=31&lt;BR /&gt;[ 2607.704607] CMD_RESP: cmd 0x6b error, result=0x1&lt;BR /&gt;[ 2607.707795] IOCTL failed: 10f51139 id=0x10000, sub_id=0x1000b action=1, status_code=0x3&lt;BR /&gt;[ 2608.116416] wlan: wfd0 START SCAN&lt;BR /&gt;[ 2613.264499] wlan: SCAN COMPLETED: scanned AP count=34&lt;BR /&gt;[ 2617.744473] wlan: SCAN COMPLETED: scanned AP count=19&lt;BR /&gt;[ 2618.354975] wlan: mlan0 START SCAN&lt;BR /&gt;[ 2623.424485] wlan: SCAN COMPLETED: scanned AP count=29&lt;BR /&gt;[ 2624.064420] wlan: wfd0 START SCAN&lt;BR /&gt;[ 2629.154523] wlan: SCAN COMPLETED: scanned AP count=33&lt;BR /&gt;</description>
      <pubDate>Fri, 03 May 2024 14:00:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/wlan-mlan0-START-SCAN/m-p/1858968#M57</guid>
      <dc:creator>masateesh</dc:creator>
      <dc:date>2024-05-03T14:00:38Z</dc:date>
    </item>
    <item>
      <title>Re: wlan: mlan0 START SCAN</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/wlan-mlan0-START-SCAN/m-p/1858970#M58</link>
      <description>&lt;P&gt;Which dram used? what configuration Is required. Could you share solution?&lt;/P&gt;</description>
      <pubDate>Fri, 03 May 2024 14:09:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/wlan-mlan0-START-SCAN/m-p/1858970#M58</guid>
      <dc:creator>masateesh</dc:creator>
      <dc:date>2024-05-03T14:09:36Z</dc:date>
    </item>
  </channel>
</rss>