<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Wi-Fi command response timeout in Wi-Fi® + Bluetooth® + 802.15.4</title>
    <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Wi-Fi-command-response-timeout/m-p/2393039#M4909</link>
    <description>&lt;P&gt;I started with wifi_setup SDK example, but it is very heavily modified now. I'm using a custom board.&lt;/P&gt;&lt;P&gt;We noticed this issue happens when there is heavy Rx (maybe Tx works too) traffic to the wireless card (60 MegaBytes/second or more), and at the same time the firmware sends a command to the wireless card to query the average RSSI and SNR. Our code did that once per second, and the issue was triggered within a minute, usually less.&lt;/P&gt;&lt;P&gt;If I disable the command transmission, the issue is not triggered.&lt;/P&gt;&lt;P&gt;I hope this info helps you in reproducing the issue (the key moments are heavy Rx traffic and command transmission at the same time).&lt;/P&gt;</description>
    <pubDate>Thu, 09 Jul 2026 11:59:15 GMT</pubDate>
    <dc:creator>azarubkin</dc:creator>
    <dc:date>2026-07-09T11:59:15Z</dc:date>
    <item>
      <title>Wi-Fi command response timeout</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Wi-Fi-command-response-timeout/m-p/2380584#M4863</link>
      <description>&lt;P&gt;I'm working on a project using i.MXRT1062 crossover MCU and Murata 2EL M.2 wireless card based on NXP IW612 chipset. The project uses MCUXpresso SDK and FreeRTOS. The current SDK version is 25.12.&lt;/P&gt;&lt;P&gt;During the firmware operation, sometimes I get the following output in the debug console:&lt;BR /&gt;&lt;BR /&gt;`[wifi] Warn: Command response timed out. command 0x0, len 1514, seqno 0x16`&lt;/P&gt;&lt;P&gt;or&lt;/P&gt;&lt;P&gt;`[wifi] Warn: Command response timed out. command 0x0, len 66, seqno 0x16`&lt;/P&gt;&lt;P&gt;or&lt;/P&gt;&lt;P&gt;`[wifi] Warn: Command response timed out. command 0x0, len 190, seqno 0x16`&lt;/P&gt;&lt;P&gt;or&lt;/P&gt;&lt;P&gt;`[wifi] Warn: Command response timed out. command 0x0, len 60, seqno 0x16`&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I don't know what do these lines mean, probably some problem with wireless module. After that a task list is printed, panic is triggered and the firmware stalls. I think the problem happens after ~30 minutes during more or less heavy traffic through the wireless connection.&lt;/P&gt;&lt;P&gt;A corresponding place in the SDK files is located at `middleware/wifi_nxp/wifidriver/wifi.c` in `wifi_wait_for_cmdresp` function. This is further confirmed that there's a pause of roughly 20 seconds between the previous debug console print and this line.&lt;/P&gt;&lt;P&gt;How can I troubleshoot the problem? I can work with you to provide further debugging information or test SDK fixes.&lt;/P&gt;</description>
      <pubDate>Fri, 12 Jun 2026 07:06:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Wi-Fi-command-response-timeout/m-p/2380584#M4863</guid>
      <dc:creator>azarubkin</dc:creator>
      <dc:date>2026-06-12T07:06:09Z</dc:date>
    </item>
    <item>
      <title>Re: Wi-Fi command response timeout</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Wi-Fi-command-response-timeout/m-p/2380948#M4865</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P class=""&gt;I understand you are using a custom application, but which SDK example did you use as a starting point? If you can reproduce the same behavior using an unmodified SDK example, it would significantly help isolate the issue.&lt;/P&gt;
&lt;P class=""&gt;Seems the driver was waiting for a command response, and did not receive it before the timeout expired.&lt;/P&gt;
&lt;P class=""&gt;Please enable the following debug macros in wifi_config.h:&lt;/P&gt;
&lt;P class=""&gt;CONFIG_WIFI_CMD_RESP_DEBUG &lt;BR /&gt;CONFIG_WIFI_EVENTS_DEBUG &lt;BR /&gt;CONFIG_WIFI_IO_INFO_DUMP &lt;BR /&gt;CONFIG_WIFI_EXTRA_DEBUG&lt;/P&gt;
&lt;P class=""&gt;Once the macros are enabled; rebuild the example and test it again. Please share the output.&lt;/P&gt;
&lt;P class=""&gt;I would be a good idea to test it with the latest SDK and see if the problems still occurs.&lt;/P&gt;</description>
      <pubDate>Fri, 12 Jun 2026 20:21:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Wi-Fi-command-response-timeout/m-p/2380948#M4865</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2026-06-12T20:21:03Z</dc:date>
    </item>
    <item>
      <title>Re: Wi-Fi command response timeout</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Wi-Fi-command-response-timeout/m-p/2385266#M4885</link>
      <description>&lt;P&gt;This is the debug output when the firmware hangs up. Please let me know if you need any previous log lines.&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;23/06/2026 12:27:48.808 [RX] - [wifi] Warn: Command response timed out. command 0x0, len 890, seqno 0x16&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;SDIO multiple port group registers value:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;**** Dump @ 20218FC0 Len: 196 ****&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;00 00 00 00 ff 00 00 00 c3 00 00 00 00 00 00 00 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;00 00 00 00 00 00 f0 7f 00 01 00 01 00 01 00 01 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;00 01 00 01 00 01 00 01 00 01 00 01 00 01 00 01 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;00 01 00 01 00 01 00 01 00 01 00 01 00 01 00 01 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;00 01 00 01 00 01 00 01 00 01 00 03 00 01 00 01 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;00 01 00 01 00 01 00 01 00 01 00 00 00 00 00 00 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;87 0c 00 00 00 00 00 00 00 00 00 00 1c c2 06 c0 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;f4 de 09 c0 00 1e ff ff 00 0a 36 01 00 00 96 00 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;ff ff ff ff 00 00 00 00 00 00 00 00 ff ff ff ff &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;00 00 00 00 00 00 00 00 10 cc f0 ff ff ff ff ff &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;00 00 ff ff ff ff ff ff f4 74 04 c0 80 98 04 c0 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;00 00 00 00 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;******** End Dump *******&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;Name State Priority Stack Num&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;==================================================&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;main_task X 3 581 6&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;print_dhcp R 0 683 17&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;IDLE R 0 92 2&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;tcp/ip B 3 400 1&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;Tmr Svc B 4 196 3&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;supplicant_main_tas B 2 1456 14&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;nfc_cfg B 0 715 7&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;dhcpd_task B 3 406 15&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;HTTP server B 1 888 18&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;wifi_scan_task B 1 255 11&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;wlcmgr_task B 3 244 13&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;wifi_drv_task B 3 228 10&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;lwip_rx B 3 431 8&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;wifi_core_task B 3 276 12&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;[wifi] Start to process hanging&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;[wifi] initiating wifi-deauth&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;[FW Download] S&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;23/06/2026 12:27:48.824 [RX] - tart to download firmware from 0x602319fc: 1618224&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;23/06/2026 12:27:54.807 [RX] - [wifi_io] Error: SDIO - FW Ready Registers not set&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;[wifi] Error: sd_wifi_reinit failed. status code -1&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;ASSERT: wlan_process_hang: 550&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;Assert failed: Panic!&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;ASSERT ERROR " 0 ": file "C:/tmp/mcuxsdk/mcuxsdk/middleware/wifi_nxp/wifidriver/incl/mlan_api.h" Line "65" function name "panic"&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Jun 2026 18:58:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Wi-Fi-command-response-timeout/m-p/2385266#M4885</guid>
      <dc:creator>azarubkin</dc:creator>
      <dc:date>2026-06-23T18:58:03Z</dc:date>
    </item>
    <item>
      <title>Re: Wi-Fi command response timeout</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Wi-Fi-command-response-timeout/m-p/2390232#M4900</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/198556"&gt;@DanielRuvalcaba&lt;/a&gt;&amp;nbsp;, is there any update on this issue? This also happens on SDK 26.03, do you need more debug info from me?&lt;/P&gt;</description>
      <pubDate>Fri, 03 Jul 2026 09:11:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Wi-Fi-command-response-timeout/m-p/2390232#M4900</guid>
      <dc:creator>azarubkin</dc:creator>
      <dc:date>2026-07-03T09:11:19Z</dc:date>
    </item>
    <item>
      <title>Re: Wi-Fi command response timeout</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Wi-Fi-command-response-timeout/m-p/2391789#M4904</link>
      <description>&lt;DIV&gt;
&lt;P&gt;What SDK example are you using?&lt;/P&gt;
&lt;P&gt;Could you please share the steps required to reproduce the behavior?&lt;/P&gt;
&lt;P&gt;Are you using a custom board or an NXP reference board?&lt;/P&gt;
&lt;P&gt;Is there any specific action or condition that consistently triggers the issue?&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Daniel.&lt;/P&gt;
&lt;/DIV&gt;</description>
      <pubDate>Tue, 07 Jul 2026 17:52:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Wi-Fi-command-response-timeout/m-p/2391789#M4904</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2026-07-07T17:52:19Z</dc:date>
    </item>
    <item>
      <title>Re: Wi-Fi command response timeout</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Wi-Fi-command-response-timeout/m-p/2393039#M4909</link>
      <description>&lt;P&gt;I started with wifi_setup SDK example, but it is very heavily modified now. I'm using a custom board.&lt;/P&gt;&lt;P&gt;We noticed this issue happens when there is heavy Rx (maybe Tx works too) traffic to the wireless card (60 MegaBytes/second or more), and at the same time the firmware sends a command to the wireless card to query the average RSSI and SNR. Our code did that once per second, and the issue was triggered within a minute, usually less.&lt;/P&gt;&lt;P&gt;If I disable the command transmission, the issue is not triggered.&lt;/P&gt;&lt;P&gt;I hope this info helps you in reproducing the issue (the key moments are heavy Rx traffic and command transmission at the same time).&lt;/P&gt;</description>
      <pubDate>Thu, 09 Jul 2026 11:59:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Wi-Fi-command-response-timeout/m-p/2393039#M4909</guid>
      <dc:creator>azarubkin</dc:creator>
      <dc:date>2026-07-09T11:59:15Z</dc:date>
    </item>
  </channel>
</rss>