<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FRDM-RW612 - Getting USB device error in Wi-Fi® + Bluetooth® + 802.15.4</title>
    <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Getting-USB-device-error/m-p/2196111#M4420</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256293"&gt;@pratikpanchal44&lt;/a&gt;,&amp;nbsp;hope you are doing well.&lt;/P&gt;
&lt;P&gt;Could you please confirm which modifications (if any) were done to the project? Is your device being detected by the host (FRDM-RW612)?&lt;/P&gt;
&lt;P&gt;Additionally, please notice that this example only supports three types of devices:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Single mouse or single keyboard devices.&lt;/LI&gt;
&lt;LI&gt;Composite device containing one mouse and one keyboard.&lt;/LI&gt;
&lt;LI&gt;HUBs connected with one mouse and one keyboard.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Any further development to add more supported devices will have to be done on the customer side, however if any further support is needed, feel free to reach us.&lt;/P&gt;</description>
    <pubDate>Thu, 30 Oct 2025 21:07:35 GMT</pubDate>
    <dc:creator>RomanVR</dc:creator>
    <dc:date>2025-10-30T21:07:35Z</dc:date>
    <item>
      <title>FRDM-RW612 - Getting USB device error</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Getting-USB-device-error/m-p/2195125#M4406</link>
      <description>&lt;P&gt;I am using FRDM-RW612 for my project. I have connected barcode scanner module on USB device to my FRDM board. Barcode scanner has USB HID support.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now, I am getting an error continuously as per below, once I scan any barcode.&lt;/P&gt;&lt;P&gt;=====================================&lt;/P&gt;&lt;DIV&gt;runwaitState 10,deviceState 1, usb status 0USB_HostKeyboardProcessBuffer means data recvd&lt;/DIV&gt;&lt;DIV&gt;===================================&lt;/DIV&gt;&lt;P&gt;Currently, I am using the SDK version &lt;U&gt;&lt;STRONG&gt;SDK_25.06.00_FRDM-RW612&lt;/STRONG&gt;&lt;/U&gt;.&lt;/P&gt;&lt;P&gt;Please advise.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 29 Oct 2025 12:57:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Getting-USB-device-error/m-p/2195125#M4406</guid>
      <dc:creator>pratikpanchal44</dc:creator>
      <dc:date>2025-10-29T12:57:33Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612 - Getting USB device error</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Getting-USB-device-error/m-p/2195302#M4411</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256293"&gt;@pratikpanchal44&lt;/a&gt;&amp;nbsp;, hope you are doing well.&lt;/P&gt;
&lt;P&gt;Could you please specify which USB HID example are you using and the modifications done to it?&lt;/P&gt;
&lt;P&gt;Also please confirm if the example runs properly as is.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Wed, 29 Oct 2025 23:15:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Getting-USB-device-error/m-p/2195302#M4411</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2025-10-29T23:15:25Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612 - Getting USB device error</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Getting-USB-device-error/m-p/2195479#M4414</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/184557"&gt;@Ricardo_Zamora&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We have used the keyboard-mouse USB HID example in our device.&lt;/P&gt;</description>
      <pubDate>Thu, 30 Oct 2025 05:09:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Getting-USB-device-error/m-p/2195479#M4414</guid>
      <dc:creator>pratikpanchal44</dc:creator>
      <dc:date>2025-10-30T05:09:17Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612 - Getting USB device error</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Getting-USB-device-error/m-p/2196111#M4420</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256293"&gt;@pratikpanchal44&lt;/a&gt;,&amp;nbsp;hope you are doing well.&lt;/P&gt;
&lt;P&gt;Could you please confirm which modifications (if any) were done to the project? Is your device being detected by the host (FRDM-RW612)?&lt;/P&gt;
&lt;P&gt;Additionally, please notice that this example only supports three types of devices:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Single mouse or single keyboard devices.&lt;/LI&gt;
&lt;LI&gt;Composite device containing one mouse and one keyboard.&lt;/LI&gt;
&lt;LI&gt;HUBs connected with one mouse and one keyboard.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Any further development to add more supported devices will have to be done on the customer side, however if any further support is needed, feel free to reach us.&lt;/P&gt;</description>
      <pubDate>Thu, 30 Oct 2025 21:07:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Getting-USB-device-error/m-p/2196111#M4420</guid>
      <dc:creator>RomanVR</dc:creator>
      <dc:date>2025-10-30T21:07:35Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612 - Getting USB device error</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Getting-USB-device-error/m-p/2200034#M4459</link>
      <description>&lt;P&gt;Hello Team,&lt;/P&gt;&lt;P&gt;Thanks for the solution.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Currently, the system is working fine, and we found a problem on the device side.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 06 Nov 2025 11:24:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Getting-USB-device-error/m-p/2200034#M4459</guid>
      <dc:creator>pratikpanchal44</dc:creator>
      <dc:date>2025-11-06T11:24:32Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612 - Getting USB device error</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Getting-USB-device-error/m-p/2200241#M4460</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256293"&gt;@pratikpanchal44&lt;/a&gt;.&lt;/P&gt;
&lt;P&gt;Thanks for letting us know that the issue has been solved.&lt;/P&gt;</description>
      <pubDate>Thu, 06 Nov 2025 17:58:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Getting-USB-device-error/m-p/2200241#M4460</guid>
      <dc:creator>RomanVR</dc:creator>
      <dc:date>2025-11-06T17:58:38Z</dc:date>
    </item>
  </channel>
</rss>