<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RW610 WiFi Direct Implementation in Wi-Fi® + Bluetooth® + 802.15.4</title>
    <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/RW610-WiFi-Direct-Implementation/m-p/2188463#M4353</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/32234"&gt;@Designer11&lt;/a&gt;, hope you are doing well.&lt;/P&gt;
&lt;P&gt;I will check this internally and I will inform you once I get a response from the internal team.&lt;/P&gt;
&lt;P&gt;Thank you for your patience.&lt;/P&gt;</description>
    <pubDate>Fri, 17 Oct 2025 18:07:09 GMT</pubDate>
    <dc:creator>RomanVR</dc:creator>
    <dc:date>2025-10-17T18:07:09Z</dc:date>
    <item>
      <title>RW610 WiFi Direct Implementation</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/RW610-WiFi-Direct-Implementation/m-p/2186844#M4342</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;I'm looking to use the RW610 chipset for an upcoming project and was wondering whether its hardware can support Wi-Fi Direct. In addition, does anyone know where i can obtain&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class=""&gt;application note or any documentation that explains the implementation and operation of Wi-Fi Direct for the RW610 chipset module.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thank you so much in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Oct 2025 18:18:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/RW610-WiFi-Direct-Implementation/m-p/2186844#M4342</guid>
      <dc:creator>Designer11</dc:creator>
      <dc:date>2025-10-15T18:18:34Z</dc:date>
    </item>
    <item>
      <title>Re: RW610 WiFi Direct Implementation</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/RW610-WiFi-Direct-Implementation/m-p/2188463#M4353</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/32234"&gt;@Designer11&lt;/a&gt;, hope you are doing well.&lt;/P&gt;
&lt;P&gt;I will check this internally and I will inform you once I get a response from the internal team.&lt;/P&gt;
&lt;P&gt;Thank you for your patience.&lt;/P&gt;</description>
      <pubDate>Fri, 17 Oct 2025 18:07:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/RW610-WiFi-Direct-Implementation/m-p/2188463#M4353</guid>
      <dc:creator>RomanVR</dc:creator>
      <dc:date>2025-10-17T18:07:09Z</dc:date>
    </item>
    <item>
      <title>Re: RW610 WiFi Direct Implementation</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/RW610-WiFi-Direct-Implementation/m-p/2193771#M4387</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/32234"&gt;@Designer11&lt;/a&gt;,&amp;nbsp;hope you are doing well and sorry for the late reply.&lt;/P&gt;
&lt;P&gt;The Wi-Fi example "wpa_supplicant" within SDK version 25.09, is compatible with Wi-Fi Direct/P2P feature, however to enable the feature it is required to define the macro: CONFIG_WPA_SUPP_P2P inside the "wifi_config.h"&amp;nbsp; file.&lt;/P&gt;
&lt;P&gt;For more information about WFD interface please refer to &lt;A href="https://mcuxpresso.nxp.com/mcuxsdk/latest/html/_static/wireless/UM11442-NXP-Wi-Fi-and-Bluetooth-Demo-Applications-for-i.MX-RT-platforms-User-Guide.pdf" target="_blank"&gt;UM11442&lt;/A&gt; on section 3.8.1.5.&lt;/P&gt;
&lt;P&gt;Please let me know if this information is helpful.&lt;/P&gt;</description>
      <pubDate>Mon, 27 Oct 2025 21:24:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/RW610-WiFi-Direct-Implementation/m-p/2193771#M4387</guid>
      <dc:creator>RomanVR</dc:creator>
      <dc:date>2025-10-27T21:24:19Z</dc:date>
    </item>
  </channel>
</rss>