<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wi-Fi® + Bluetooth® + 802.15.4のトピックRe: SDIO Initialization Stuck on Custom Board with IW610 Module</title>
    <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SDIO-Initialization-Stuck-on-Custom-Board-with-IW610-Module/m-p/2175068#M4283</link>
    <description>&lt;P&gt;For your clarification, the full part number of the Wi-Fi/BLE module is &lt;STRONG&gt;u-blox MAYA-W476&lt;/STRONG&gt;, which is based on the &lt;STRONG&gt;NXP IW610&lt;/STRONG&gt; chipset.&lt;/P&gt;&lt;P&gt;If driver support is available, kindly guide me on the software changes required to enable support.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Amarnath.&lt;/P&gt;</description>
    <pubDate>Wed, 24 Sep 2025 13:37:45 GMT</pubDate>
    <dc:creator>Amarnath_473</dc:creator>
    <dc:date>2025-09-24T13:37:45Z</dc:date>
    <item>
      <title>SDIO Initialization Stuck on Custom Board with IW610 Module</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SDIO-Initialization-Stuck-on-Custom-Board-with-IW610-Module/m-p/2174397#M4273</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am working on the &lt;STRONG&gt;MIMXRT1176&lt;/STRONG&gt; with a custom board and using MCUXpresso &lt;STRONG&gt;SDK v25.09&lt;/STRONG&gt; for a Bluetooth/Wi-Fi module based on the &lt;STRONG&gt;IW610&lt;/STRONG&gt; chip family.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Hardware Connections:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;SDIO interface&lt;/STRONG&gt;: SD_DATA0-3, SD_CMD, SD_CLK connected.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;UART&lt;/STRONG&gt;: Tx, Rx, and GND connected.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;GPIO&lt;/STRONG&gt;: WL_RST, SDIO_RST connected.&lt;/P&gt;&lt;P&gt;The module is powered via an external USB-C cable.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Software:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I am using the SDK example &lt;STRONG&gt;Wireless_uart&lt;/STRONG&gt; for BLE.&lt;/P&gt;&lt;P&gt;I updated the macro in preprocessor section to:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;WIFI_IW610_BOARD_MURATA_2LL_M2&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;When attempting to initialize the SDIO interface, the program gets &lt;STRONG&gt;stuck in a loop&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;I have attached a screenshot of the code section where it hangs.&lt;/P&gt;&lt;P&gt;Could anyone suggest what could be causing this issue or provide guidance on proper SDIO initialization for the IW610 module on a custom board?&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;BR /&gt;Amar.&lt;/P&gt;</description>
      <pubDate>Tue, 23 Sep 2025 14:44:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SDIO-Initialization-Stuck-on-Custom-Board-with-IW610-Module/m-p/2174397#M4273</guid>
      <dc:creator>Amarnath_473</dc:creator>
      <dc:date>2025-09-23T14:44:55Z</dc:date>
    </item>
    <item>
      <title>Re: SDIO Initialization Stuck on Custom Board with IW610 Module</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SDIO-Initialization-Stuck-on-Custom-Board-with-IW610-Module/m-p/2174481#M4275</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well. By any chance, have you tried with our &lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/i-mx-evaluation-and-development-boards/i-mx-rt1170-evaluation-kit:MIMXRT1170-EVKB" target="_blank"&gt;MIMXRT1170-EVKB&lt;/A&gt;? Are you seeing the same behavior?&lt;/P&gt;
&lt;P&gt;Could you please confirm that you are using the 2LL Murata module?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Tue, 23 Sep 2025 18:01:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SDIO-Initialization-Stuck-on-Custom-Board-with-IW610-Module/m-p/2174481#M4275</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2025-09-23T18:01:33Z</dc:date>
    </item>
    <item>
      <title>Re: SDIO Initialization Stuck on Custom Board with IW610 Module</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SDIO-Initialization-Stuck-on-Custom-Board-with-IW610-Module/m-p/2174748#M4279</link>
      <description>&lt;P&gt;Hi&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/184557" target="_blank"&gt;@Ricardo_Zamora&lt;/A&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;1. I do not have the&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;MIMXRT1170-EVKB&lt;/STRONG&gt;, which is why I am working with a custom board.&lt;/P&gt;&lt;P&gt;2.&amp;nbsp;I am currently using the&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;u-blox MAYA-W4&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;module, which is based on the&lt;STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;IW610&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;chip family, for Wi-Fi/BLE.&lt;/P&gt;&lt;P&gt;Could you please let me know that driver/firmware support is available for&amp;nbsp;&lt;STRONG&gt;u-blox MAYA-W4?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Amar.&lt;/P&gt;</description>
      <pubDate>Wed, 24 Sep 2025 05:39:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SDIO-Initialization-Stuck-on-Custom-Board-with-IW610-Module/m-p/2174748#M4279</guid>
      <dc:creator>Amarnath_473</dc:creator>
      <dc:date>2025-09-24T05:39:03Z</dc:date>
    </item>
    <item>
      <title>Re: SDIO Initialization Stuck on Custom Board with IW610 Module</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SDIO-Initialization-Stuck-on-Custom-Board-with-IW610-Module/m-p/2175068#M4283</link>
      <description>&lt;P&gt;For your clarification, the full part number of the Wi-Fi/BLE module is &lt;STRONG&gt;u-blox MAYA-W476&lt;/STRONG&gt;, which is based on the &lt;STRONG&gt;NXP IW610&lt;/STRONG&gt; chipset.&lt;/P&gt;&lt;P&gt;If driver support is available, kindly guide me on the software changes required to enable support.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Amarnath.&lt;/P&gt;</description>
      <pubDate>Wed, 24 Sep 2025 13:37:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SDIO-Initialization-Stuck-on-Custom-Board-with-IW610-Module/m-p/2175068#M4283</guid>
      <dc:creator>Amarnath_473</dc:creator>
      <dc:date>2025-09-24T13:37:45Z</dc:date>
    </item>
    <item>
      <title>Re: SDIO Initialization Stuck on Custom Board with IW610 Module</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SDIO-Initialization-Stuck-on-Custom-Board-with-IW610-Module/m-p/2176640#M4296</link>
      <description>&lt;P&gt;hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/184557"&gt;@Ricardo_Zamora&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;I have an update regarding my progress. &lt;STRONG&gt;The SDIO initialization is now working successfully&lt;/STRONG&gt;, and I am attempting to download the firmware to the MAYA W476 module. However, I am encountering an issue in the function &lt;STRONG&gt;static fwdnld_intf_ret_t sdio_interface_send()&lt;/STRONG&gt; within &lt;STRONG&gt;fwdnld_sdio.c&lt;/STRONG&gt;. During execution, the length value is &lt;STRONG&gt;16 for 2–3 iterations&lt;/STRONG&gt;, after which an error occurs. I have attached an image for reference showing the exact point where it stops.&lt;/P&gt;&lt;P&gt;Additionally, I would like clarification: since both the &lt;STRONG&gt;Murata Type 2LL module&lt;/STRONG&gt; and the &lt;STRONG&gt;MAYA-W4&lt;/STRONG&gt; are based on the &lt;STRONG&gt;IW610 chipset&lt;/STRONG&gt;, can the same &lt;STRONG&gt;firmware provided for the Murata 2LL be used for the MAYA-W4 as well?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Amar.&lt;/P&gt;</description>
      <pubDate>Fri, 26 Sep 2025 13:04:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SDIO-Initialization-Stuck-on-Custom-Board-with-IW610-Module/m-p/2176640#M4296</guid>
      <dc:creator>Amarnath_473</dc:creator>
      <dc:date>2025-09-26T13:04:23Z</dc:date>
    </item>
    <item>
      <title>Re: SDIO Initialization Stuck on Custom Board with IW610 Module</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SDIO-Initialization-Stuck-on-Custom-Board-with-IW610-Module/m-p/2177139#M4299</link>
      <description>&lt;P&gt;Hello Amar,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;By any chance, have you tested any other Wi-Fi example?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Mon, 29 Sep 2025 03:42:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SDIO-Initialization-Stuck-on-Custom-Board-with-IW610-Module/m-p/2177139#M4299</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2025-09-29T03:42:05Z</dc:date>
    </item>
    <item>
      <title>Re: SDIO Initialization Stuck on Custom Board with IW610 Module</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SDIO-Initialization-Stuck-on-Custom-Board-with-IW610-Module/m-p/2177486#M4304</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/184557"&gt;@Ricardo_Zamora&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tested using the other example codes and encountered the same issue. While command transfers are responding correctly — confirmed using the following function, which returns a length of 16 or 17: in&amp;nbsp;Wi-Fi client example.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;t_u16 wlan_card_read_f1_base_regs(void)&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;{&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;t_u16 reg;&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;uint32_t resp = 0;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;(void)sdio_drv_creg_read(READ_BASE_0_REG, 1, &amp;amp;resp);&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;reg = (t_u16)(resp &amp;amp; 0xFFU);&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;(void)sdio_drv_creg_read(READ_BASE_1_REG, 1, &amp;amp;resp);&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;reg |= (t_u16)((resp &amp;amp; 0xFFU) &amp;lt;&amp;lt; 8);&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;return reg;&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;}&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;However, when attempting to send firmware data, the transfer fails within the&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;SDMMCHOST_TransferFunction&lt;/STRONG&gt;. The function detects a data transfer failure by using flags in&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;else condition&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;and sets&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;error = kStatus_Fail&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;I have attached an image of the function for your reference. Could you please provide guidance on how to resolve this data transfer issue?&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Can we use same firmware which is provided for MURATA TYPE 2LL module to the MAYA W4 module because both are based on IW610 chipset family?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; regards,&lt;BR /&gt;Tarak.&lt;/P&gt;</description>
      <pubDate>Mon, 29 Sep 2025 13:39:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SDIO-Initialization-Stuck-on-Custom-Board-with-IW610-Module/m-p/2177486#M4304</guid>
      <dc:creator>Amarnath_473</dc:creator>
      <dc:date>2025-09-29T13:39:28Z</dc:date>
    </item>
  </channel>
</rss>