<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wi-Fi® + Bluetooth® + 802.15.4中的主题 Re: RW612 and Thread FTD</title>
    <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/RW612-and-Thread-FTD/m-p/2114646#M3970</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Most of the code works now except the Openthread running as FTD which is most important.&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Would you have an idea when the ieee802.15.4 node will be in the device tree and enabled in Zephyr so that a Openthread FTD can operate? I added the question last month to Zephyr Discord, but there was no response.&lt;/P&gt;&lt;P&gt;&lt;A href="https://discord.com/channels/720317445772017664/1032993479061667900" target="_blank"&gt;https://discord.com/channels/720317445772017664/1032993479061667900&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The company project is blocked unfortunately. If I knew how to do this, I would implement it.&amp;nbsp; I am perplexed since this seems so fundamental to the purpose of this part.&lt;BR /&gt;&lt;BR /&gt;Is there someone or group I can work with to get the ieee802.15.4 node into the device tree and into Zephyr for this RW612 part?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 11 Jun 2025 17:29:16 GMT</pubDate>
    <dc:creator>joanou</dc:creator>
    <dc:date>2025-06-11T17:29:16Z</dc:date>
    <item>
      <title>RW612 and Thread FTD</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/RW612-and-Thread-FTD/m-p/2091182#M3904</link>
      <description>&lt;P&gt;Main question - Can I use the RW612 as a Full Thread Device (FTD) sensor node and act as a router eligible end device (REED)?&lt;/P&gt;&lt;P&gt;If so, is this recommended and is there a working example for VSCode? Also, no need for Matter in my application. I need low latency.&lt;BR /&gt;&lt;BR /&gt;I found the firmware binary:&amp;nbsp;rw61x_sb_ble_15d4_combo_a2.bin.&amp;nbsp; Any plans to release the source code that that it can be tuned and optimized? Same question for&amp;nbsp;rw61x_sb_wifi_a2.bin.&lt;BR /&gt;&lt;BR /&gt;Finally, can WiFi and Thread be supported in the same application, even if only one can be used at a time?&lt;BR /&gt;&lt;BR /&gt;Thanks&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 04 May 2025 19:30:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/RW612-and-Thread-FTD/m-p/2091182#M3904</guid>
      <dc:creator>joanou</dc:creator>
      <dc:date>2025-05-04T19:30:02Z</dc:date>
    </item>
    <item>
      <title>Re: RW612 and Thread FTD</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/RW612-and-Thread-FTD/m-p/2091542#M3905</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well. Here you can find the OpenThread examples available for RW612: &lt;A href="https://github.com/NXP/ot-nxp/blob/release/v1.4.0/src/rw/rw612/README.md" target="_blank"&gt;NXP/ot-nxp · GitHub&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Also, I would recommend checking this User Manual: &lt;A href="https://www.nxp.com/docs/en/user-manual/UM11861.pdf" target="_blank"&gt;NXP 802.15.4 Demo Applications for RW612&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope this helps!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Mon, 05 May 2025 15:56:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/RW612-and-Thread-FTD/m-p/2091542#M3905</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2025-05-05T15:56:47Z</dc:date>
    </item>
    <item>
      <title>Re: RW612 and Thread FTD</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/RW612-and-Thread-FTD/m-p/2092957#M3908</link>
      <description>&lt;P&gt;Hello Ricardo,&lt;/P&gt;&lt;P&gt;Thanks for the links.&amp;nbsp; I am looking to use Zephyr, VSCode MCUXpresso with the included device tree for the FRDM-RW612.&amp;nbsp; Would there be a sample for openthread CLI?&amp;nbsp; If not, any plans... I am stuck otherwise with my current code base?&lt;/P&gt;&lt;P&gt;The error is:&lt;/P&gt;&lt;P&gt;In file included from C:/Zephyr/zephyr_v4_1_0/zephyr/include/zephyr/toolchain/gcc.h:98,&lt;BR /&gt;from C:/Zephyr/zephyr_v4_1_0/zephyr/include/zephyr/toolchain.h:52,&lt;BR /&gt;from C:/Zephyr/zephyr_v4_1_0/zephyr/include/zephyr/sys/__assert.h:11,&lt;BR /&gt;from C:/Zephyr/zephyr_v4_1_0/zephyr/include/zephyr/sys/iterable_sections.h:10,&lt;BR /&gt;from C:/Zephyr/zephyr_v4_1_0/zephyr/include/zephyr/logging/log_instance.h:10,&lt;BR /&gt;from C:/Zephyr/zephyr_v4_1_0/zephyr/include/zephyr/logging/log.h:10,&lt;BR /&gt;from C:/Zephyr/zephyr_v4_1_0/zephyr/modules/openthread/platform/radio.c:17:&lt;BR /&gt;C:/Zephyr/zephyr_v4_1_0/zephyr/include/zephyr/device.h:96:41: error: '__device_dts_ord_DT_CHOSEN_zephyr_ieee802154_ORD' undeclared here (not in a function)&lt;BR /&gt;96 | #define DEVICE_NAME_GET(dev_id) _CONCAT(__device_, dev_id)&lt;BR /&gt;| ^~~~~~~~~&lt;/P&gt;&lt;P&gt;The code lines in zephyr\modules\openthread\platform\radio.c are:&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;static&lt;/SPAN&gt; &lt;SPAN&gt;const&lt;/SPAN&gt; &lt;SPAN&gt;struct&lt;/SPAN&gt; &lt;SPAN&gt;device&lt;/SPAN&gt; &lt;SPAN&gt;*const&lt;/SPAN&gt; &lt;SPAN&gt;radio_dev&lt;/SPAN&gt; &lt;SPAN&gt;=&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;&lt;SPAN&gt;DEVICE_DT_GET&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;DT_CHOSEN&lt;/SPAN&gt;&lt;SPAN&gt;(zephyr_ieee802154));&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;static&lt;/SPAN&gt; &lt;SPAN&gt;struct&lt;/SPAN&gt; &lt;SPAN&gt;ieee802154_radio_api&lt;/SPAN&gt; &lt;SPAN&gt;*&lt;/SPAN&gt;&lt;SPAN&gt;radio_api&lt;/SPAN&gt;&lt;SPAN&gt;;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&lt;BR /&gt;I had tried adding this to the device tree, but more is needed.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;amp;nbu_802154_channel {&lt;BR /&gt;status = "okay";&lt;BR /&gt;};&lt;BR /&gt;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;chosen {&lt;BR /&gt;zephyr,ieee802154 = &amp;lt;&amp;amp;nbu_802154_channel&amp;gt;;&lt;BR /&gt;};&lt;BR /&gt;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;These were added to prj.conf&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;CONFIG_CRYPTO=y&lt;BR /&gt;CONFIG_MBEDTLS=y&lt;BR /&gt;CONFIG_NETWORKING=y&lt;BR /&gt;CONFIG_SHELL=y&lt;BR /&gt;CONFIG_UART_CONSOLE=y&lt;BR /&gt;CONFIG_NET_L2_IEEE802154=y&lt;BR /&gt;CONFIG_NET_L2_OPENTHREAD=y&lt;BR /&gt;CONFIG_OPENTHREAD_FTD=y&lt;BR /&gt;CONFIG_OPENTHREAD_MTD=n&lt;BR /&gt;CONFIG_OPENTHREAD_COPROCESSOR_RCP=n&lt;BR /&gt;CONFIG_OPENTHREAD_COPROCESSOR_NCP=n&lt;BR /&gt;CONFIG_OPENTHREAD_THREAD_VERSION_1_4=y&lt;BR /&gt;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Wed, 07 May 2025 16:38:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/RW612-and-Thread-FTD/m-p/2092957#M3908</guid>
      <dc:creator>joanou</dc:creator>
      <dc:date>2025-05-07T16:38:23Z</dc:date>
    </item>
    <item>
      <title>Re: RW612 and Thread FTD</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/RW612-and-Thread-FTD/m-p/2093110#M3910</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I apologize, but currently there is no support for this MCU.&lt;/P&gt;
&lt;P&gt;I would recommend checking official channels from OT and Zephyr to check availability and support.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Wed, 07 May 2025 20:10:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/RW612-and-Thread-FTD/m-p/2093110#M3910</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2025-05-07T20:10:14Z</dc:date>
    </item>
    <item>
      <title>Re: RW612 and Thread FTD</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/RW612-and-Thread-FTD/m-p/2093124#M3911</link>
      <description>&lt;P&gt;Thanks for this information.&amp;nbsp; So Zephyr (or OT) community is the appropriate organization to implement OT FTD?&amp;nbsp; Anyone else?&amp;nbsp; I would have thought NXP would drive this. I will review the FreeRTOS implementation.&lt;/P&gt;&lt;P&gt;Following up from earlier, will source code for&amp;nbsp;rw61x_sb_ble_15d4_combo_a2.bin be available anytime soon?&amp;nbsp; This could help interface and optimize the implementation for the application?&lt;/P&gt;&lt;P&gt;Regards, Steve&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 07 May 2025 21:05:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/RW612-and-Thread-FTD/m-p/2093124#M3911</guid>
      <dc:creator>joanou</dc:creator>
      <dc:date>2025-05-07T21:05:14Z</dc:date>
    </item>
    <item>
      <title>Re: RW612 and Thread FTD</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/RW612-and-Thread-FTD/m-p/2094759#M3913</link>
      <description>&lt;P&gt;Hello Steve,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;NXP works on these repositories, so the support is updated there.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For other wireless protocols, the FW for the radio is used and integrated on the application. We do not offer the source code for these binaries.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Fri, 09 May 2025 17:24:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/RW612-and-Thread-FTD/m-p/2094759#M3913</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2025-05-09T17:24:25Z</dc:date>
    </item>
    <item>
      <title>Re: RW612 and Thread FTD</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/RW612-and-Thread-FTD/m-p/2114646#M3970</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Most of the code works now except the Openthread running as FTD which is most important.&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Would you have an idea when the ieee802.15.4 node will be in the device tree and enabled in Zephyr so that a Openthread FTD can operate? I added the question last month to Zephyr Discord, but there was no response.&lt;/P&gt;&lt;P&gt;&lt;A href="https://discord.com/channels/720317445772017664/1032993479061667900" target="_blank"&gt;https://discord.com/channels/720317445772017664/1032993479061667900&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The company project is blocked unfortunately. If I knew how to do this, I would implement it.&amp;nbsp; I am perplexed since this seems so fundamental to the purpose of this part.&lt;BR /&gt;&lt;BR /&gt;Is there someone or group I can work with to get the ieee802.15.4 node into the device tree and into Zephyr for this RW612 part?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 11 Jun 2025 17:29:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/RW612-and-Thread-FTD/m-p/2114646#M3970</guid>
      <dc:creator>joanou</dc:creator>
      <dc:date>2025-06-11T17:29:16Z</dc:date>
    </item>
  </channel>
</rss>