<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Toolchain problem with SDK example in Wi-Fi® + Bluetooth® + 802.15.4</title>
    <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Toolchain-problem-with-SDK-example/m-p/2043208#M3799</link>
    <description>&lt;P&gt;Hi, thanks for answering,&amp;nbsp;&lt;/P&gt;&lt;P&gt;The procedure I did is from the IDE, import SDK Example, then select my board and the NCP, device example. And then just build. When I build I got include and path errors. I try to add the paths manually to the project's properties and then I got the errors mentioned.&amp;nbsp;&lt;/P&gt;&lt;P&gt;About the versions I'm using:&amp;nbsp;&lt;/P&gt;&lt;P&gt;- MCUXpressoIDE&amp;nbsp;v24.12.148&lt;/P&gt;&lt;P&gt;_ SDK Version 24.12.00&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Maybe it's an error of the example?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Thu, 13 Feb 2025 08:05:05 GMT</pubDate>
    <dc:creator>VonMartins</dc:creator>
    <dc:date>2025-02-13T08:05:05Z</dc:date>
    <item>
      <title>Toolchain problem with SDK example</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Toolchain-problem-with-SDK-example/m-p/2041728#M3797</link>
      <description>&lt;P&gt;Hi, I'm having a toolchain compatibility problem. I want to load the ncp_device example to a rw612 from the SDK but when compiling I get errors indicating that the toolchain is not correct. The documentation for the example says to use ARMGCC 12.3.1. I am using arm-none-eabi-gcc, which should be the same, with version 13.2. I don't know why I get so many errors like this:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&amp;nbsp;... \arm-gnu-toolchain-12.3.rel1-mingw-w64-i686-arm-none-eabi\arm-none-eabi\include/stdio.h:180:18: error: unknown type name '__gnuc_va_list'; did you mean '__va_list'?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;... \arm-gnu-toolchain-12.3.rel1-mingw-w64-i686-arm-none-eabi\arm-none-eabi\include/sys/_timeval.h:42:25: error: conflicting types for 'time_t'; have '__int_least64_t' {aka 'long long int'}&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;\arm-gnu-toolchain-12.3.rel1-mingw-w64-i686-arm-none-eabi\arm-none-eabi\include/sys/types.h:107:25: error: conflicting types for 'clock_t'; have 'long unsigned int'&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What toolchain should I use and how can I change it in the configuration? Where can I manage toolchains in the MCUXpressoIDE?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Tue, 11 Feb 2025 11:25:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Toolchain-problem-with-SDK-example/m-p/2041728#M3797</guid>
      <dc:creator>VonMartins</dc:creator>
      <dc:date>2025-02-11T11:25:50Z</dc:date>
    </item>
    <item>
      <title>Re: Toolchain problem with SDK example</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Toolchain-problem-with-SDK-example/m-p/2042753#M3798</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well. Could you please clarify the procedure you are following?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;What SDK version are you using? What IDE version do you have?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Wed, 12 Feb 2025 16:50:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Toolchain-problem-with-SDK-example/m-p/2042753#M3798</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2025-02-12T16:50:45Z</dc:date>
    </item>
    <item>
      <title>Re: Toolchain problem with SDK example</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Toolchain-problem-with-SDK-example/m-p/2043208#M3799</link>
      <description>&lt;P&gt;Hi, thanks for answering,&amp;nbsp;&lt;/P&gt;&lt;P&gt;The procedure I did is from the IDE, import SDK Example, then select my board and the NCP, device example. And then just build. When I build I got include and path errors. I try to add the paths manually to the project's properties and then I got the errors mentioned.&amp;nbsp;&lt;/P&gt;&lt;P&gt;About the versions I'm using:&amp;nbsp;&lt;/P&gt;&lt;P&gt;- MCUXpressoIDE&amp;nbsp;v24.12.148&lt;/P&gt;&lt;P&gt;_ SDK Version 24.12.00&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Maybe it's an error of the example?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 13 Feb 2025 08:05:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Toolchain-problem-with-SDK-example/m-p/2043208#M3799</guid>
      <dc:creator>VonMartins</dc:creator>
      <dc:date>2025-02-13T08:05:05Z</dc:date>
    </item>
    <item>
      <title>Re: Toolchain problem with SDK example</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Toolchain-problem-with-SDK-example/m-p/2043922#M3800</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you please use VSCode for the compilation of this example?&lt;/P&gt;
&lt;P&gt;I just tested with latest SDK version, and it is working:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Ricardo_Zamora_0-1739482800193.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/323900i1473FA175BA8F8EE/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Ricardo_Zamora_0-1739482800193.png" alt="Ricardo_Zamora_0-1739482800193.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Ricardo_Zamora_0-1739482800193.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Thu, 13 Feb 2025 21:40:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Toolchain-problem-with-SDK-example/m-p/2043922#M3800</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2025-02-13T21:40:15Z</dc:date>
    </item>
  </channel>
</rss>