<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FRDM-RW612: Error while programming flash: Verify failed in Wi-Fi® + Bluetooth® + 802.15.4</title>
    <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Error-while-programming-flash-Verify-failed/m-p/2037101#M3618</link>
    <description>&lt;P&gt;Hi There,&lt;/P&gt;&lt;P&gt;Flashing failed for &lt;STRONG&gt;FRDM-RW612&lt;/STRONG&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried erasing the board. It works fine but is not able to program the board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;below is the MCUXpresso Console log&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Executing flash operation 'Program' (Program executable into flash Debug/frdmrw612_hello_world.axf) - Mon Feb 03 13:55:49 IST 2025
Checking MCU info...
Scanning for targets...
Executing flash action...
SEGGER J-Link Commander V8.12a (Compiled Jan  9 2025 14:43:13)
DLL version V8.12a, compiled Jan  9 2025 14:42:08
J-Link Command File read successfully.
Processing script file...
J-Link&amp;gt;ExitOnError 1
J-Link Commander will now exit on Error
J-Link&amp;gt;r
J-Link connection not established yet but required for command.
Connecting to J-Link via USB...O.K.
Firmware: J-Link MCU-Link V1 compiled Oct  9 2024 11:01:41
Hardware version: V1.00
J-Link uptime (since boot): 0d 01h 24m 30s
S/N: 1067701573
USB speed mode: High speed (480 MBit/s)
VTref=3.300V
Target connection not established yet but required for command.
Device "RW612" selected.
Connecting to target via SWD
InitTarget() start
SWD selected. Executing JTAG -&amp;gt; SWD switching sequence.
DAP initialized successfully.
DMAP_REG_ID: DM-AP IDCODE detected: 0x002A0000
DHCSR: 0x05100000
InitTarget() end - Took 2.36ms
Found SW-DP with ID 0x6BA02477
DPIDR: 0x6BA02477
CoreSight SoC-400 or earlier
Scanning AP map to find all available APs
AP[1]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x84770001, ADDR: 0x00000000)
Iterating through AP map to find AHB-AP to use
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FF000
CPUID register: 0x410FD214. Implementer code: 0x41 (ARM)
Feature set: Mainline
Cache: No cache
Found Cortex-M33 r0p4, Little endian.
FPUnit: 8 code (BP) slots and 0 literal slots
Security extension: implemented
Secure debug: enabled
CoreSight components:
ROMTbl[0] @ E00FF000
[0][0]: E000E000 CID B105900D PID 000BBD21 DEVARCH 47702A04 DEVTYPE 00 Cortex-M33
[0][1]: E0001000 CID B105900D PID 000BBD21 DEVARCH 47701A02 DEVTYPE 00 DWT
[0][2]: E0002000 CID B105900D PID 000BBD21 DEVARCH 47701A03 DEVTYPE 00 FPB
[0][3]: E0000000 CID B105900D PID 000BBD21 DEVARCH 47701A01 DEVTYPE 43 ITM
[0][5]: E0041000 CID B105900D PID 002BBD21 DEVARCH 47724A13 DEVTYPE 13 ETM
[0][6]: E0042000 CID B105900D PID 000BBD21 DEVARCH 47701A14 DEVTYPE 14 CSS600-CTI
Memory zones:
"Default" Description: Default access mode
Cortex-M33 identified.
Reset delay: 0 ms
ResetTarget() start
Reset via SYSRESETREQ and reset pin + halt after bootloader
ROM entered ISP command handling loop. Re-enable the debug access.
MSPLIM cleared
ResetTarget() end - Took 113ms
Device specific reset executed.
J-Link&amp;gt;h
PC = 1302B460, CycleCnt = 00000000
R0 = 00000000, R1 = 5AC33CA5, R2 = 00000001, R3 = 5AC33CA5
R4 = 3012F5FC, R5 = 50002E24, R6 = 55AACC33, R7 = 33CCAA55
R8 = 5AA55AA5, R9 = FCF0030F, R10= C33CA55A, R11= 55AACC33
R12= 3012F5FC
SP(R13)= 30125A38, MSP= 30125A38, PSP= 00000000, R14(LR) = 1302B421
XPSR = 01000000: APSR = nzcvq, EPSR = 01000000, IPSR = 000 (NoException)
CFBP = 00000001, CONTROL = 00, FAULTMASK = 00, BASEPRI = 00, PRIMASK = 01
MSPLIM = 00000000
PSPLIM = 00000000
Security extension regs:
MSP_S = 30125A38, MSP_NS = 00000000
MSPLIM_S = 00000000, MSPLIM_NS = 00000000
PSP_S = 00000000, PSP_NS = FFFFFFFC
PSPLIM_S = 00000000, PSPLIM_NS = 00000000
CONTROL_S  = 00, FAULTMASK_S  = 00, BASEPRI_S  = 00, PRIMASK_S  = 01
CONTROL_NS = 00, FAULTMASK_NS = 00, BASEPRI_NS = 00, PRIMASK_NS = 00
FPS0 = 00000000, FPS1 = 00000000, FPS2 = 00000000, FPS3 = 00000000
FPS4 = 00000000, FPS5 = 00000000, FPS6 = 00000000, FPS7 = 00000000
FPS8 = 00000000, FPS9 = 00000000, FPS10= 00000000, FPS11= 00000000
FPS12= 00000000, FPS13= 00000000, FPS14= 00000000, FPS15= 00000000
FPS16= 00000000, FPS17= 00000000, FPS18= 00000000, FPS19= 00000000
FPS20= 00000000, FPS21= 00000000, FPS22= 00000000, FPS23= 00000000
FPS24= 00000000, FPS25= 00000000, FPS26= 00000000, FPS27= 00000000
FPS28= 00000000, FPS29= 00000000, FPS30= 00000000, FPS31= 00000000
FPSCR= 00000000
J-Link&amp;gt;loadfile "/home/bhavya/Documents/MCUXpresso_24.12.148/workspace/frdmrw612_hello_world/Debug/frdmrw612_hello_world.hex" 0x8000000
'loadfile': Performing implicit reset &amp;amp; halt of MCU.
ResetTarget() start
Reset via SYSRESETREQ and reset pin + halt after bootloader
ROM entered ISP command handling loop. Re-enable the debug access.
MSPLIM cleared
ResetTarget() end - Took 113ms
Device specific reset executed.
Downloading file [/home/bhavya/Documents/MCUXpresso_24.12.148/workspace/frdmrw612_hello_world/Debug/frdmrw612_hello_world.hex]...
J-Link: Flash download: Bank 0 @ 0x08000000: 1 range affected (65536 bytes)
J-Link: Flash download: Total: 0.647s (Prepare: 0.181s, Compare: 0.113s, Erase: 0.005s, Program: 0.164s, Verify: 0.107s, Restore: 0.076s)
J-Link: Flash download: Program speed: 390 KB/s
****** Error: Verification failed @ address 0x08000000
Error while programming flash: Verify failed.
Script processing completed.
Unable to perform operation!
Command failed with exit code 1&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Installed SDK:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot from 2025-02-03 14-02-34.png" style="width: 934px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/322189iB2F795BF7F78B002/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot from 2025-02-03 14-02-34.png" alt="Screenshot from 2025-02-03 14-02-34.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Screenshot from 2025-02-03 14-02-34.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Bhavya&lt;/P&gt;</description>
    <pubDate>Mon, 03 Feb 2025 08:34:58 GMT</pubDate>
    <dc:creator>bmathukiya</dc:creator>
    <dc:date>2025-02-03T08:34:58Z</dc:date>
    <item>
      <title>FRDM-RW612: Error while programming flash: Verify failed</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Error-while-programming-flash-Verify-failed/m-p/2037101#M3618</link>
      <description>&lt;P&gt;Hi There,&lt;/P&gt;&lt;P&gt;Flashing failed for &lt;STRONG&gt;FRDM-RW612&lt;/STRONG&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried erasing the board. It works fine but is not able to program the board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;below is the MCUXpresso Console log&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Executing flash operation 'Program' (Program executable into flash Debug/frdmrw612_hello_world.axf) - Mon Feb 03 13:55:49 IST 2025
Checking MCU info...
Scanning for targets...
Executing flash action...
SEGGER J-Link Commander V8.12a (Compiled Jan  9 2025 14:43:13)
DLL version V8.12a, compiled Jan  9 2025 14:42:08
J-Link Command File read successfully.
Processing script file...
J-Link&amp;gt;ExitOnError 1
J-Link Commander will now exit on Error
J-Link&amp;gt;r
J-Link connection not established yet but required for command.
Connecting to J-Link via USB...O.K.
Firmware: J-Link MCU-Link V1 compiled Oct  9 2024 11:01:41
Hardware version: V1.00
J-Link uptime (since boot): 0d 01h 24m 30s
S/N: 1067701573
USB speed mode: High speed (480 MBit/s)
VTref=3.300V
Target connection not established yet but required for command.
Device "RW612" selected.
Connecting to target via SWD
InitTarget() start
SWD selected. Executing JTAG -&amp;gt; SWD switching sequence.
DAP initialized successfully.
DMAP_REG_ID: DM-AP IDCODE detected: 0x002A0000
DHCSR: 0x05100000
InitTarget() end - Took 2.36ms
Found SW-DP with ID 0x6BA02477
DPIDR: 0x6BA02477
CoreSight SoC-400 or earlier
Scanning AP map to find all available APs
AP[1]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x84770001, ADDR: 0x00000000)
Iterating through AP map to find AHB-AP to use
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FF000
CPUID register: 0x410FD214. Implementer code: 0x41 (ARM)
Feature set: Mainline
Cache: No cache
Found Cortex-M33 r0p4, Little endian.
FPUnit: 8 code (BP) slots and 0 literal slots
Security extension: implemented
Secure debug: enabled
CoreSight components:
ROMTbl[0] @ E00FF000
[0][0]: E000E000 CID B105900D PID 000BBD21 DEVARCH 47702A04 DEVTYPE 00 Cortex-M33
[0][1]: E0001000 CID B105900D PID 000BBD21 DEVARCH 47701A02 DEVTYPE 00 DWT
[0][2]: E0002000 CID B105900D PID 000BBD21 DEVARCH 47701A03 DEVTYPE 00 FPB
[0][3]: E0000000 CID B105900D PID 000BBD21 DEVARCH 47701A01 DEVTYPE 43 ITM
[0][5]: E0041000 CID B105900D PID 002BBD21 DEVARCH 47724A13 DEVTYPE 13 ETM
[0][6]: E0042000 CID B105900D PID 000BBD21 DEVARCH 47701A14 DEVTYPE 14 CSS600-CTI
Memory zones:
"Default" Description: Default access mode
Cortex-M33 identified.
Reset delay: 0 ms
ResetTarget() start
Reset via SYSRESETREQ and reset pin + halt after bootloader
ROM entered ISP command handling loop. Re-enable the debug access.
MSPLIM cleared
ResetTarget() end - Took 113ms
Device specific reset executed.
J-Link&amp;gt;h
PC = 1302B460, CycleCnt = 00000000
R0 = 00000000, R1 = 5AC33CA5, R2 = 00000001, R3 = 5AC33CA5
R4 = 3012F5FC, R5 = 50002E24, R6 = 55AACC33, R7 = 33CCAA55
R8 = 5AA55AA5, R9 = FCF0030F, R10= C33CA55A, R11= 55AACC33
R12= 3012F5FC
SP(R13)= 30125A38, MSP= 30125A38, PSP= 00000000, R14(LR) = 1302B421
XPSR = 01000000: APSR = nzcvq, EPSR = 01000000, IPSR = 000 (NoException)
CFBP = 00000001, CONTROL = 00, FAULTMASK = 00, BASEPRI = 00, PRIMASK = 01
MSPLIM = 00000000
PSPLIM = 00000000
Security extension regs:
MSP_S = 30125A38, MSP_NS = 00000000
MSPLIM_S = 00000000, MSPLIM_NS = 00000000
PSP_S = 00000000, PSP_NS = FFFFFFFC
PSPLIM_S = 00000000, PSPLIM_NS = 00000000
CONTROL_S  = 00, FAULTMASK_S  = 00, BASEPRI_S  = 00, PRIMASK_S  = 01
CONTROL_NS = 00, FAULTMASK_NS = 00, BASEPRI_NS = 00, PRIMASK_NS = 00
FPS0 = 00000000, FPS1 = 00000000, FPS2 = 00000000, FPS3 = 00000000
FPS4 = 00000000, FPS5 = 00000000, FPS6 = 00000000, FPS7 = 00000000
FPS8 = 00000000, FPS9 = 00000000, FPS10= 00000000, FPS11= 00000000
FPS12= 00000000, FPS13= 00000000, FPS14= 00000000, FPS15= 00000000
FPS16= 00000000, FPS17= 00000000, FPS18= 00000000, FPS19= 00000000
FPS20= 00000000, FPS21= 00000000, FPS22= 00000000, FPS23= 00000000
FPS24= 00000000, FPS25= 00000000, FPS26= 00000000, FPS27= 00000000
FPS28= 00000000, FPS29= 00000000, FPS30= 00000000, FPS31= 00000000
FPSCR= 00000000
J-Link&amp;gt;loadfile "/home/bhavya/Documents/MCUXpresso_24.12.148/workspace/frdmrw612_hello_world/Debug/frdmrw612_hello_world.hex" 0x8000000
'loadfile': Performing implicit reset &amp;amp; halt of MCU.
ResetTarget() start
Reset via SYSRESETREQ and reset pin + halt after bootloader
ROM entered ISP command handling loop. Re-enable the debug access.
MSPLIM cleared
ResetTarget() end - Took 113ms
Device specific reset executed.
Downloading file [/home/bhavya/Documents/MCUXpresso_24.12.148/workspace/frdmrw612_hello_world/Debug/frdmrw612_hello_world.hex]...
J-Link: Flash download: Bank 0 @ 0x08000000: 1 range affected (65536 bytes)
J-Link: Flash download: Total: 0.647s (Prepare: 0.181s, Compare: 0.113s, Erase: 0.005s, Program: 0.164s, Verify: 0.107s, Restore: 0.076s)
J-Link: Flash download: Program speed: 390 KB/s
****** Error: Verification failed @ address 0x08000000
Error while programming flash: Verify failed.
Script processing completed.
Unable to perform operation!
Command failed with exit code 1&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Installed SDK:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot from 2025-02-03 14-02-34.png" style="width: 934px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/322189iB2F795BF7F78B002/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot from 2025-02-03 14-02-34.png" alt="Screenshot from 2025-02-03 14-02-34.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Screenshot from 2025-02-03 14-02-34.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Bhavya&lt;/P&gt;</description>
      <pubDate>Mon, 03 Feb 2025 08:34:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Error-while-programming-flash-Verify-failed/m-p/2037101#M3618</guid>
      <dc:creator>bmathukiya</dc:creator>
      <dc:date>2025-02-03T08:34:58Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612: Error while programming flash: Verify failed</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Error-while-programming-flash-Verify-failed/m-p/2039463#M3645</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Were you able to flash the board before? And if so, which was the last SDK example that was running on the board?&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Can you help me by following the steps to the &lt;A href="https://community.nxp.com/t5/FRDM-Training-Hub/FRDM-RW612-Getting-Started-Wi-Fi-CLI-on-VS-Code/ta-p/1995032" target="_blank"&gt;FRDM-RW612 Getting Started. Wi-Fi CLI on VS Code&lt;/A&gt; and let me know if the issue persists?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ana Sofia&lt;/P&gt;</description>
      <pubDate>Thu, 06 Feb 2025 17:40:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Error-while-programming-flash-Verify-failed/m-p/2039463#M3645</guid>
      <dc:creator>sofiaurueta</dc:creator>
      <dc:date>2025-02-06T17:40:54Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612: Error while programming flash: Verify failed</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Error-while-programming-flash-Verify-failed/m-p/2040605#M3651</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/242964"&gt;@sofiaurueta&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, I was able to flash the board previously. I had flashed&amp;nbsp;&lt;STRONG&gt;light-switch-combo-app&lt;/STRONG&gt; &lt;A href="https://github.com/NXP/matter/blob/v1.4.0.0/examples/light-switch-combo-app/nxp/rt/rw61x/README.md" target="_blank" rel="noopener"&gt;https://github.com/NXP/matter/blob/v1.4.0.0/examples/light-switch-combo-app/nxp/rt/rw61x/README.md&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After that, I was trying to reflash the board and this issue arose.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to follow the steps you shared in&amp;nbsp;&lt;A href="https://community.nxp.com/t5/FRDM-Training-Hub/FRDM-RW612-Getting-Started-Wi-Fi-CLI-on-VS-Code/ta-p/1995032" target="_blank" rel="noopener"&gt;FRDM-RW612 Getting Started. Wi-Fi CLI on VS Code&lt;/A&gt;&amp;nbsp;but&amp;nbsp;&lt;STRONG&gt;&lt;A href="http://%20https//mcuxpresso.nxp.com/en/select" target="_self" rel="nofollow noopener noreferrer"&gt;FRDM-RW612 SDK&lt;/A&gt;&lt;/STRONG&gt;&amp;nbsp;but the link seems broken.&amp;nbsp;&lt;/P&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot from 2025-02-10 10-54-19.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/323098i19FD642D2D2591FD/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot from 2025-02-10 10-54-19.png" alt="Screenshot from 2025-02-10 10-54-19.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Screenshot from 2025-02-10 10-54-19.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I must say NXP's documentation seems untested. I have also faced various issues in following the quick start for&amp;nbsp;&lt;A href="https://docs.nxp.com/bundle/UG10178/page/topics/introduction.html?_gl=1*1rchgw5*_ga*MjQ0NjIxMTA3LjE3Mzc2OTkyMDc.*_ga_WM5LE0KMSH*MTczNzcyMjQwNi40LjEuMTczNzcyMjc0NC4wLjAuMA.." target="_self"&gt;UG10178: Quick Start to the Matter Demo NXP CHIP Tool app, FRDM-RW612 and FRDM-MCU W71&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Bhavya&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 10 Feb 2025 05:26:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Error-while-programming-flash-Verify-failed/m-p/2040605#M3651</guid>
      <dc:creator>bmathukiya</dc:creator>
      <dc:date>2025-02-10T05:26:36Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612: Error while programming flash: Verify failed</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Error-while-programming-flash-Verify-failed/m-p/2041389#M3662</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/242964"&gt;@sofiaurueta&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tried to follow the steps to flash the WiFi CLI app using VS code. But getting the same error.&lt;/P&gt;&lt;P&gt;I am attaching the screenshot for your reference.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot from 2025-02-10 12-35-20.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/323297i4F1533386FAA7300/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot from 2025-02-10 12-35-20.png" alt="Screenshot from 2025-02-10 12-35-20.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Screenshot from 2025-02-10 12-35-20.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Can you please look into this.&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Bhavya&lt;/P&gt;</description>
      <pubDate>Tue, 11 Feb 2025 04:26:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Error-while-programming-flash-Verify-failed/m-p/2041389#M3662</guid>
      <dc:creator>bmathukiya</dc:creator>
      <dc:date>2025-02-11T04:26:21Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612: Error while programming flash: Verify failed</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Error-while-programming-flash-Verify-failed/m-p/2041951#M3668</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Bhavya,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Could you please clarify if you selected the FRDM (and not the RD) when building the matter application?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;If you selected the RD, (or did not select any option), the binary for the RD was generated. So, please follow this guide:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/Unlock-FRDM-RW612-flash/ta-p/2015561" target="_blank"&gt;Unlock FRDM-RW612 flash - NXP Community&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Ricardo&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 11 Feb 2025 17:40:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Error-while-programming-flash-Verify-failed/m-p/2041951#M3668</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2025-02-11T17:40:30Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612: Error while programming flash: Verify failed</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Error-while-programming-flash-Verify-failed/m-p/2042434#M3672</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/184557"&gt;@Ricardo_Zamora&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, I have selected the FRDM only. I have flashed the&amp;nbsp;&lt;STRONG&gt;light-switch-combo-app&amp;nbsp;&lt;/STRONG&gt;matter firmware and can test it. But after that, I cannot flash another firmware; the previous firmware is also not booting up.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have also tried the long manual activity mentioned in the&amp;nbsp;&lt;A href="https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/Unlock-FRDM-RW612-flash/ta-p/2015561" target="_blank" rel="noopener"&gt;Unlock FRDM-RW612 flash - NXP Community&lt;/A&gt;&amp;nbsp;link but the issue is still the same.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Bhavya&lt;/P&gt;</description>
      <pubDate>Wed, 12 Feb 2025 08:49:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Error-while-programming-flash-Verify-failed/m-p/2042434#M3672</guid>
      <dc:creator>bmathukiya</dc:creator>
      <dc:date>2025-02-12T08:49:54Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612: Error while programming flash: Verify failed</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Error-while-programming-flash-Verify-failed/m-p/2045684#M3691</link>
      <description>&lt;P&gt;Hello &lt;SPAN&gt;Bhavya,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you try to do a mass-erase as shown in this guide: &lt;A href="https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs-Knowledge/RT-board-recovery-for-debugger-connect-issues/ta-p/1635260" target="_blank" rel="noopener"&gt;RT board recovery for debugger connect issues&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ana Sofia&lt;/P&gt;</description>
      <pubDate>Mon, 17 Feb 2025 17:17:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Error-while-programming-flash-Verify-failed/m-p/2045684#M3691</guid>
      <dc:creator>sofiaurueta</dc:creator>
      <dc:date>2025-02-17T17:17:00Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612: Error while programming flash: Verify failed</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Error-while-programming-flash-Verify-failed/m-p/2047317#M3704</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/242964"&gt;@sofiaurueta&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have already done the mass erase at a very first instant and also mentioned the same in this ticket's 1st reply. Mass erase works fine.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="mass erase.PNG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/324767iF249C65F69DF5AD8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="mass erase.PNG" alt="mass erase.PNG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;mass erase.PNG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;The guide&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs-Knowledge/RT-board-recovery-for-debugger-connect-issues/ta-p/1635260" target="_blank" rel="noopener"&gt;RT board recovery for debugger connect issues&lt;/A&gt; which you are pointing is for&amp;nbsp;&lt;SPAN&gt;MIMXRT1060-EVK and I have &lt;STRONG&gt;FRDM-RW612&lt;/STRONG&gt;. Can you please guide the steps for FRDM-RW612&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Bhavya&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 19 Feb 2025 12:54:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Error-while-programming-flash-Verify-failed/m-p/2047317#M3704</guid>
      <dc:creator>bmathukiya</dc:creator>
      <dc:date>2025-02-19T12:54:29Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612: Error while programming flash: Verify failed</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Error-while-programming-flash-Verify-failed/m-p/2047325#M3705</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/242964"&gt;@sofiaurueta&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have also tried to test the external flash using SPT tool but it is also failed. Below is the snapshot for the same.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="SPT.PNG" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/324772i55A06AEA4DEBA5FF/image-size/large?v=v2&amp;amp;px=999" role="button" title="SPT.PNG" alt="SPT.PNG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;SPT.PNG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Bhavya&lt;/P&gt;</description>
      <pubDate>Wed, 19 Feb 2025 13:00:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Error-while-programming-flash-Verify-failed/m-p/2047325#M3705</guid>
      <dc:creator>bmathukiya</dc:creator>
      <dc:date>2025-02-19T13:00:49Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-RW612: Error while programming flash: Verify failed</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Error-while-programming-flash-Verify-failed/m-p/2047589#M3706</link>
      <description>&lt;P&gt;Hello Bhavya,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you follow the steps to the &lt;A href="https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/Unlock-FRDM-RW612-flash/ta-p/2015561" target="_blank"&gt;Unlock FRDM-RW612 flash&lt;/A&gt; guide once again?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Before running the last blhost steps "Now run the following (YOUR BINARY should be the path and file in which the binary is located):"&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please do the following:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Open a Terminal (such as TeraTerm or PuTTY) and share with me the output of the example. I would like to see that the example to unlock the flash is running correctly.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ana Sofia&lt;/P&gt;</description>
      <pubDate>Wed, 19 Feb 2025 20:47:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/FRDM-RW612-Error-while-programming-flash-Verify-failed/m-p/2047589#M3706</guid>
      <dc:creator>sofiaurueta</dc:creator>
      <dc:date>2025-02-19T20:47:44Z</dc:date>
    </item>
  </channel>
</rss>