<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 88W8801(LILY W131) WiFI SDIO chip -  not responding after FW download in Wi-Fi® + Bluetooth® + 802.15.4</title>
    <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8801-LILY-W131-WiFI-SDIO-chip-not-responding-after-FW/m-p/1985026#M3505</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I just did a test using an iMX8MP running Linux 5.15.71 and a 2DS wireless module and seems to be working on my side.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;root@imx8mpevk:~# uname -r
5.15.71+g50912be38601
root@imx8mpevk:~# modprobe moal mod_para=nxp/wifi_mod_para.conf
[   29.718678] mlan: loading out-of-tree module taints kernel.
[   29.743284] wlan: Loading MWLAN driver
[   29.747330] wlan: Register to Bus Driver...
[   29.758102] vendor=0x02DF device=0x9139 class=0 function=1
[   29.763683] Attach moal handle ops, card interface type: 0x10a
[   29.770597] SD8801: init module param from usr cfg
[   29.775450] card_type: SD8801, config block: 0
[   29.779910] cfg80211_wext=0xf
[   29.782888] max_vir_bss=1
[   29.785511] cal_data_cfg=none
[   29.788488] ps_mode = 1
[   29.790945] auto_ds = 1
[   29.793396] host_mlme=enable
[   29.796305] fw_name=nxp/sd8801_uapsta.bin
[   29.800344] SDIO: max_segs=128 max_seg_size=65535
[   29.805061] rx_work=1 cpu_num=4
[   29.808227] Attach mlan adapter operations.card_type is 0x10a.
[   29.815228] wlan: Enable TX SG mode
[   29.818755] wlan: Enable RX SG mode
[   29.829669] Request firmware: nxp/sd8801_uapsta.bin
[   30.114525] Wlan: FW download over, firmwarelen=256744 downloaded 256744
[   30.317972] WLAN FW is active
[   30.320953] on_time is 30319390625
[   30.353278] fw_cap_info=0xba3, dev_cap_mask=0xffffffff
[   30.483665] Register NXP 802.11 Adapter mlan0
[   30.489778] Register NXP 802.11 Adapter uap0
[   30.499256] Register NXP 802.11 Adapter wfd0
[   30.505382] wlan: version = SD8801----14.92.36.p178-MM5X14366.p5-GPL-(FP92)
[   30.514305] wlan: Register to Bus Driver Done
[   30.518750] wlan: Driver loaded successfully
root@imx8mpevk:~# ifconfig mlan0 up&lt;/LI-CODE&gt;
&lt;P&gt;This is the configuration for 8801:&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;SD8801 = {
        cfg80211_wext=0xf
        max_vir_bss=1
        cal_data_cfg=none
        ps_mode=1
        auto_ds=1
        host_mlme=1
        fw_name=nxp/sd8801_uapsta.bin
}&lt;/LI-CODE&gt;
&lt;P&gt;Please let me know if you notice any difference.&lt;BR /&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel.&lt;/P&gt;</description>
    <pubDate>Wed, 30 Oct 2024 19:32:54 GMT</pubDate>
    <dc:creator>DanielRuvalcaba</dc:creator>
    <dc:date>2024-10-30T19:32:54Z</dc:date>
    <item>
      <title>88W8801(LILY W131) WiFI SDIO chip -  not responding after FW download</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8801-LILY-W131-WiFI-SDIO-chip-not-responding-after-FW/m-p/1983893#M3499</link>
      <description>&lt;P&gt;Hello, I am trying to run the 88W8801 on an Nvidia AGX Orin, but unfortunately, I'm experiencing issues with a lack of response after fw_download. Any idea why this might be happening?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;[  392.618241] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[  392.618541] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[  392.619180] cfg80211: loaded regulatory.db is malformed or signature is missing/invalid
[  392.629162] wlan: Loading MWLAN driver
[  392.631120] wlan: Register to Bus Driver...
[  392.632317] vendor=0x02DF device=0x9139 class=0 function=1
[  392.632408] Attach moal handle ops, card interface type: 0x10a
[  392.632582] SD8801: init module param from usr cfg
[  392.632605] card_type: SD8801, config block: 0
[  392.632608] cfg80211_wext=0xf
[  392.632611] cal_data_cfg=none
[  392.632612] ps_mode = 1
[  392.632614] fw_name=nxp/new.bin
[  392.632622] SDIO: max_segs=128 max_seg_size=65535
[  392.632625] rx_work=1 cpu_num=12
[  392.632640] Attach mlan adapter operations.card_type is 0x10a.
[  392.633036] wlan: Enable TX SG mode
[  392.633038] wlan: Enable RX SG mode
[  392.637804] Request firmware: nxp/new.bin
[  392.638422] WLAN FW already running! Skip FW download
[  392.638470] WLAN FW is active
[  392.638472] on_time is 392636776160
[  397.790492] Timeout cmd id (397.788783) = 0xa9, act = 0x0
...
...
...


[  397.795899] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
..
..
..
[  397.796170] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
[  397.796196] 0x00 
[  397.796228] 0x00 
[  397.796248] 0x00 
[  397.796280] 0x00 
[  397.796298] 0x00 
[  397.796316] 0x00 
[  397.796345] 0x00 
[  397.796363] 0x00 

[  397.796428] bss_index = 0, tx_pkts_queued = 0
[  397.796468] -------- Dump info End---------
[  397.799854] SDIO Func0 (0x0-0x9): 32 02 02 02 03 00 00 02 03 00 
[  397.800053] SDIO Func1 (0x10-0x17): 00 00 00 00 00 00 00 00 
[  397.800165] SDIO Func1: (0x28) 00 (0x30) 08 (0x34) 07 (0x38) 10 (0x3c) 00 
[  397.800415] SDIO Func1 (0x60-0x6a): dc fe 1c 00 67 01 03 01 03 00 30 
[  397.902354] SDIO Func1 (0x60-0x6a): dc fe 26 00 71 01 03 01 03 00 30 
[  397.902442] woal_request_fw failed
[  397.902446] Firmware Init Failed
[  397.907748] Free module params
[  397.907760] woal_add_card failed
[  397.907825] wlan_sdio: probe of mmc1:0001:1 failed with error -1
[  397.908292] wlan: Register to Bus Driver Done
[  397.908297] wlan: Driver loaded successfully&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Oct 2024 14:04:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8801-LILY-W131-WiFI-SDIO-chip-not-responding-after-FW/m-p/1983893#M3499</guid>
      <dc:creator>luqtd</dc:creator>
      <dc:date>2024-10-29T14:04:52Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8801(LILY W131) WiFI SDIO chip -  not responding after FW download</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8801-LILY-W131-WiFI-SDIO-chip-not-responding-after-FW/m-p/1983898#M3500</link>
      <description>&lt;P class=""&gt;&lt;SPAN class=""&gt;nxp/new.bin is a copy of nxp/sd8801_uapsta.bin&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Oct 2024 14:07:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8801-LILY-W131-WiFI-SDIO-chip-not-responding-after-FW/m-p/1983898#M3500</guid>
      <dc:creator>luqtd</dc:creator>
      <dc:date>2024-10-29T14:07:17Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8801(LILY W131) WiFI SDIO chip -  not responding after FW download</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8801-LILY-W131-WiFI-SDIO-chip-not-responding-after-FW/m-p/1984110#M3501</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;What OS version are you using?&lt;/P&gt;
&lt;P&gt;What Driver and FW are you using?&lt;/P&gt;
&lt;P&gt;Could you please share with me the whole terminal output of your test (commands)?&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel.&lt;/P&gt;</description>
      <pubDate>Tue, 29 Oct 2024 19:08:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8801-LILY-W131-WiFI-SDIO-chip-not-responding-after-FW/m-p/1984110#M3501</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2024-10-29T19:08:58Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8801(LILY W131) WiFI SDIO chip -  not responding after FW download</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8801-LILY-W131-WiFI-SDIO-chip-not-responding-after-FW/m-p/1984555#M3502</link>
      <description>&lt;P class=""&gt;I am using a Linux OS based on Nvidia-Jetpack(v36.3) with kernel 5.15.136-l4t. I also tried it on kernel 5.10, but the result was the same.&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Driver:&amp;nbsp;github.com/nxp-imx/mwifiex.git - branch:&amp;nbsp;lf-5.15.71_2.2.0&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Firmware:&amp;nbsp;github.com/NXP/imx-firmware.git&amp;nbsp;- branch:&amp;nbsp;lf-5.15.71_2.2.0&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;The command i use:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;modprobe moal&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;I also tried but the result was the same&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;modprobe moal mfg_mode=1 cal_data_cfg=none drv_mode=1 fw_name=nxp/sd8801.bin&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Thanks in advance for help!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 30 Oct 2024 08:21:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8801-LILY-W131-WiFI-SDIO-chip-not-responding-after-FW/m-p/1984555#M3502</guid>
      <dc:creator>luqtd</dc:creator>
      <dc:date>2024-10-30T08:21:08Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8801(LILY W131) WiFI SDIO chip -  not responding after FW download</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8801-LILY-W131-WiFI-SDIO-chip-not-responding-after-FW/m-p/1984647#M3503</link>
      <description>&lt;LI-CODE lang="markup"&gt;[  121.555042] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[  121.555414] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[  121.556033] cfg80211: loaded regulatory.db is malformed or signature is missing/invalid
[  121.567292] wlan: Loading MWLAN driver
[  121.568170] wlan: Register to Bus Driver...
[  121.569339] vendor=0x02DF device=0x9139 class=0 function=1
[  121.569450] Attach moal handle ops, card interface type: 0x10a
[  121.569454] No module param cfg file specified
[  121.569457] SDIO: max_segs=128 max_seg_size=65535
[  121.569459] rx_work=1 cpu_num=12
[  121.569476] Attach mlan adapter operations.card_type is 0x10a.
[  121.569896] wlan: Enable TX SG mode
[  121.569898] wlan: Enable RX SG mode
[  121.571461] Request firmware: nxp/sd8801_uapsta.bin
[  121.572044] WLAN FW already running! Skip FW download
[  121.572113] WLAN FW is active
[  121.572116] on_time is 121568811104
[  121.572640] get fw info failed! status=-1, error_code=0x0
[  121.572644] woal_init_priv: get_fw_info failed 
[  121.573011] Register NXP 802.11 Adapter mlan0
[  121.573015] get fw info failed! status=-1, error_code=0x0
[  121.573017] woal_add_interface: get_fw_info failed 
[  121.619528] Failed to add interface
[  121.651405] woal_request_fw failed
[  121.651412] Firmware Init Failed
[  121.660746] Free module params
[  121.660769] woal_add_card failed
[  121.660867] wlan_sdio: probe of mmc1:0001:1 failed with error -1
[  121.661267] wlan: Register to Bus Driver Done
[  121.661275] wlan: Driver loaded successfully&lt;/LI-CODE&gt;&lt;P&gt;When i remove the module with "modprobe -r moal" and probe it again. I am getting also logs like this.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 30 Oct 2024 10:05:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8801-LILY-W131-WiFI-SDIO-chip-not-responding-after-FW/m-p/1984647#M3503</guid>
      <dc:creator>luqtd</dc:creator>
      <dc:date>2024-10-30T10:05:06Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8801(LILY W131) WiFI SDIO chip -  not responding after FW download</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8801-LILY-W131-WiFI-SDIO-chip-not-responding-after-FW/m-p/1984658#M3504</link>
      <description>&lt;LI-CODE lang="markup"&gt;modprobe moal req_fw_nowait=1&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;..
..
[  474.021924] wlan: Enable RX SG mode
[  474.023468] Request firmware: nxp/sd8801_uapsta.bin
[  474.023650] wlan: Register to Bus Driver Done
[  474.023652] wlan: Driver loaded successfully
[  474.025714] WLAN FW already running! Skip FW download
[  474.025780] WLAN FW is active
[  474.025782] on_time is 474022476992
[  479.199409] Timeout cmd id (479.196095) = 0xa9, act = 0x0
[  479.199623] a9 
[  479.199652] 00 
[  479.199673] 08 
[  479.199691] 00 
[  479.199710] 01 
[  479.199729] 00 
[  479.199747] 00 
[  479.199767] 00 
[  479.199786] 00 
[  479.199805] 00 
[  479.199823] 00 
[  479.199842] 00 
[  479.199860] 00 
[  479.199879] 00 
[  479.199898] 00 
[  479.199916] 00 

[  479.199957] BSS type = 0 BSS role= 0
[  479.199988] ------------Dump info-----------
[  479.200017] Commmand Timeout
[  479.200050] pending command id: 0x242 ioctl_buf=0000000000000000
[  479.200081] pending command id: 0x3 ioctl_buf=0000000000000000
[  479.200099] No pending scan command
[  479.200122] mlan_processing =0
[  479.200147] main_lock_flag =0
[  479.200171] main_process_cnt =1
[  479.200195] delay_task_flag =0
[  479.200216] mlan_rx_processing =0
[  479.200239] rx_pkts_queued=0
[  479.200261] more_task_flag = 0
[  479.200286] num_cmd_timeout = 1
[  479.200307] last_cmd_index = 1
[  479.200327] last_cmd_id = 
[  479.200349] 0x0 

.
.
[  479.201631] num_data_h2c_failure = 0
[  479.201651] num_cmd_h2c_failure = 0
[  479.201677] num_data_c2h_failure = 0
[  479.201707] num_cmdevt_c2h_failure = 0
[  479.201728] num_int_read_failure = 0
[  479.201752] last_int_status = 0
[  479.201783] num_alloc_buffer_failure = 0
[  479.201814] num_pkt_dropped = 0
[  479.201833] num_no_cmd_node = 0
[  479.201854] num_event_deauth = 0
[  479.201872] num_event_disassoc = 0
[  479.201911] num_event_link_lost = 0
[  479.201933] num_cmd_deauth = 0
[  479.201950] num_cmd_assoc_success = 0
[  479.201974] num_cmd_assoc_failure = 0
[  479.202005] num_cons_assoc_failure = 0
[  479.202026] cmd_resp_received=0
[  479.202044] event_received=0
[  479.202065] max_tx_buf_size=2048
[  479.202097] tx_buf_size=2048
[  479.202118] curr_tx_buf_size=2048
[  479.202142] data_sent=1 cmd_sent=1
[  479.202164] ps_mode=1 ps_state=0
[  479.202193] wakeup_dev_req=0 wakeup_tries=0 wakeup_timeout=0
[  479.202217] hs_configured=0 hs_activated=0
[  479.202240] pps_uapsd_mode=0 sleep_pd=0
[  479.202279] tx_lock_flag = 0
[  479.202299] scan_processing = 0
[  479.202318] scan_state = 0x0
[  479.202339] bypass_pkt_count=0
[  479.202371] mp_rd_bitmap=0x0 curr_rd_port=0x1
[  479.202395] mp_wr_bitmap=0x0 curr_wr_port=0x1
[  479.202414] mp_data_port_mask = 0xfffe
[  479.202441] last_recv_rd_bitmap=0x0 mp_invalid_update=0
[  479.202475] last_recv_wr_bitmap=0x0 last_mp_index=0
[  479.202501] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
.
.
.
[  479.204759] 0x00 
[  479.204776] 0x00 
[  479.204798] 0x00 

[  479.204857] mp_wr_bitmap: 0x0 mp_wr_ports=0x0 len=0 curr_wr_port=0x0
[  479.204892] 0x00 
[  479.204910] 0x00 
[  479.204928] 0x00 
[  479.204959] 0x00 
[  479.204991] 0x00 
[  479.205010] 0x00 
[  479.205027] 0x00 
[  479.205045] 0x00 

[  479.205108] bss_index = 0, tx_pkts_queued = 0
[  479.205134] -------- Dump info End---------
[  479.211648] SDIO Func0 (0x0-0x9): 32 02 02 02 03 00 00 02 03 00 
[  479.212488] SDIO Func1 (0x10-0x17): 00 00 00 00 00 00 00 00 
[  479.213010] SDIO Func1: (0x28) 00 (0x30) 08 (0x34) 07 (0x38) 10 (0x3c) 00 
[  479.214100] SDIO Func1 (0x60-0x6a): dc fe 19 00 2e 01 03 01 06 00 30 
[  479.319160] SDIO Func1 (0x60-0x6a): dc fe 24 00 38 01 03 01 06 00 30 
[  479.319185] woal_request_fw_dpc failed&lt;/LI-CODE&gt;</description>
      <pubDate>Wed, 30 Oct 2024 10:18:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8801-LILY-W131-WiFI-SDIO-chip-not-responding-after-FW/m-p/1984658#M3504</guid>
      <dc:creator>luqtd</dc:creator>
      <dc:date>2024-10-30T10:18:13Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8801(LILY W131) WiFI SDIO chip -  not responding after FW download</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8801-LILY-W131-WiFI-SDIO-chip-not-responding-after-FW/m-p/1985026#M3505</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I just did a test using an iMX8MP running Linux 5.15.71 and a 2DS wireless module and seems to be working on my side.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;root@imx8mpevk:~# uname -r
5.15.71+g50912be38601
root@imx8mpevk:~# modprobe moal mod_para=nxp/wifi_mod_para.conf
[   29.718678] mlan: loading out-of-tree module taints kernel.
[   29.743284] wlan: Loading MWLAN driver
[   29.747330] wlan: Register to Bus Driver...
[   29.758102] vendor=0x02DF device=0x9139 class=0 function=1
[   29.763683] Attach moal handle ops, card interface type: 0x10a
[   29.770597] SD8801: init module param from usr cfg
[   29.775450] card_type: SD8801, config block: 0
[   29.779910] cfg80211_wext=0xf
[   29.782888] max_vir_bss=1
[   29.785511] cal_data_cfg=none
[   29.788488] ps_mode = 1
[   29.790945] auto_ds = 1
[   29.793396] host_mlme=enable
[   29.796305] fw_name=nxp/sd8801_uapsta.bin
[   29.800344] SDIO: max_segs=128 max_seg_size=65535
[   29.805061] rx_work=1 cpu_num=4
[   29.808227] Attach mlan adapter operations.card_type is 0x10a.
[   29.815228] wlan: Enable TX SG mode
[   29.818755] wlan: Enable RX SG mode
[   29.829669] Request firmware: nxp/sd8801_uapsta.bin
[   30.114525] Wlan: FW download over, firmwarelen=256744 downloaded 256744
[   30.317972] WLAN FW is active
[   30.320953] on_time is 30319390625
[   30.353278] fw_cap_info=0xba3, dev_cap_mask=0xffffffff
[   30.483665] Register NXP 802.11 Adapter mlan0
[   30.489778] Register NXP 802.11 Adapter uap0
[   30.499256] Register NXP 802.11 Adapter wfd0
[   30.505382] wlan: version = SD8801----14.92.36.p178-MM5X14366.p5-GPL-(FP92)
[   30.514305] wlan: Register to Bus Driver Done
[   30.518750] wlan: Driver loaded successfully
root@imx8mpevk:~# ifconfig mlan0 up&lt;/LI-CODE&gt;
&lt;P&gt;This is the configuration for 8801:&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;SD8801 = {
        cfg80211_wext=0xf
        max_vir_bss=1
        cal_data_cfg=none
        ps_mode=1
        auto_ds=1
        host_mlme=1
        fw_name=nxp/sd8801_uapsta.bin
}&lt;/LI-CODE&gt;
&lt;P&gt;Please let me know if you notice any difference.&lt;BR /&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel.&lt;/P&gt;</description>
      <pubDate>Wed, 30 Oct 2024 19:32:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8801-LILY-W131-WiFI-SDIO-chip-not-responding-after-FW/m-p/1985026#M3505</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2024-10-30T19:32:54Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8801(LILY W131) WiFI SDIO chip -  not responding after FW download</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8801-LILY-W131-WiFI-SDIO-chip-not-responding-after-FW/m-p/1985372#M3506</link>
      <description>&lt;P class=""&gt;I think the main difference is that I’m using Nvidia’s board with a relatively newer kernel.&lt;/P&gt;&lt;P class=""&gt;I’ve noticed that my Nvidia’s board uses Clock Gating. Do you think that could be causing the issue?&lt;/P&gt;</description>
      <pubDate>Thu, 31 Oct 2024 08:10:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8801-LILY-W131-WiFI-SDIO-chip-not-responding-after-FW/m-p/1985372#M3506</guid>
      <dc:creator>luqtd</dc:creator>
      <dc:date>2024-10-31T08:10:39Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8801(LILY W131) WiFI SDIO chip -  not responding after FW download</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8801-LILY-W131-WiFI-SDIO-chip-not-responding-after-FW/m-p/1985404#M3507</link>
      <description>&lt;P&gt;If it’s not clock gating, do you have any idea why this might be happening?&lt;/P&gt;</description>
      <pubDate>Thu, 31 Oct 2024 08:44:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8801-LILY-W131-WiFI-SDIO-chip-not-responding-after-FW/m-p/1985404#M3507</guid>
      <dc:creator>luqtd</dc:creator>
      <dc:date>2024-10-31T08:44:50Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8801(LILY W131) WiFI SDIO chip -  not responding after FW download</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8801-LILY-W131-WiFI-SDIO-chip-not-responding-after-FW/m-p/1985733#M3508</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I'm not entirely sure.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Nevertheless, I notice the fw is not being downloaded to the SoC since you get a "WLAN FW already running! Skip FW download". Is there any step you execute before the logs you sent me?&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel.&lt;/P&gt;</description>
      <pubDate>Thu, 31 Oct 2024 17:50:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8801-LILY-W131-WiFI-SDIO-chip-not-responding-after-FW/m-p/1985733#M3508</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2024-10-31T17:50:30Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8801(LILY W131) WiFI SDIO chip -  not responding after FW download</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8801-LILY-W131-WiFI-SDIO-chip-not-responding-after-FW/m-p/1986943#M3509</link>
      <description>&lt;P&gt;I'm not entirely sure why, but removing the no-sd property and changing the bus-width from 4 to 1 in the device tree seems to have resolved the issue. I’ll investigate this further and will post updates here on what I find.&lt;/P&gt;&lt;P&gt;Interestingly, after the first firmware download, it started working even with the original device tree configuration. Really strange behavior.&lt;/P&gt;</description>
      <pubDate>Mon, 04 Nov 2024 09:54:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8801-LILY-W131-WiFI-SDIO-chip-not-responding-after-FW/m-p/1986943#M3509</guid>
      <dc:creator>luqtd</dc:creator>
      <dc:date>2024-11-04T09:54:34Z</dc:date>
    </item>
  </channel>
</rss>