<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SD8978 firmware load fail in Wi-Fi® + Bluetooth® + 802.15.4</title>
    <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SD8978-firmware-load-fail/m-p/1899454#M3250</link>
    <description>Yes that is all correct, 5.15.71, and the modification to the driver was to print out the value of the register for all the retries before retry limit is reached, which shows the register changing</description>
    <pubDate>Thu, 04 Jul 2024 10:03:54 GMT</pubDate>
    <dc:creator>vmbtech</dc:creator>
    <dc:date>2024-07-04T10:03:54Z</dc:date>
    <item>
      <title>SD8978 firmware load fail</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SD8978-firmware-load-fail/m-p/1893374#M3240</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;The driver and fw version is lf-5.15.71_2.2.0&lt;/P&gt;&lt;P&gt;After firmware load the driver reports with&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;[ &amp;nbsp;&amp;nbsp;94.244794] Fail to poll firmware status: firmwarestat=0x5f5f&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I did some modification to the driver and found that the firmwarestat initially comes back 0xf00a before settling on 0x5f5f&lt;/P&gt;&lt;P&gt;I'd like to know exactly what this means so I can diagnose why my driver is failing to get past the firmware load.&lt;/P&gt;&lt;P&gt;What I need is register definitions for the status_reg_0 and status_reg_1, or at least the meaning of 5f5f and f00a&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jun 2024 06:53:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SD8978-firmware-load-fail/m-p/1893374#M3240</guid>
      <dc:creator>vmbtech</dc:creator>
      <dc:date>2024-06-25T06:53:38Z</dc:date>
    </item>
    <item>
      <title>Re: SD8978 firmware load fail</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SD8978-firmware-load-fail/m-p/1893887#M3241</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;Could you please help me with the following information?&lt;/P&gt;
&lt;P&gt;- What host are you using?&lt;/P&gt;
&lt;P&gt;- Are you using a module?&lt;/P&gt;
&lt;P&gt;- Please share with me the FW (i.e. 17.92.1.p149.131) and Driver (i.e. MM6X17437.p3-GPL) version&lt;/P&gt;
&lt;P&gt;- Please share with me the whole terminal output of your test&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel.&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jun 2024 22:13:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SD8978-firmware-load-fail/m-p/1893887#M3241</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2024-06-25T22:13:37Z</dc:date>
    </item>
    <item>
      <title>Re: SD8978 firmware load fail</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SD8978-firmware-load-fail/m-p/1894420#M3242</link>
      <description>&lt;P&gt;host is an stm32mp133 soc&lt;/P&gt;&lt;P&gt;yes the module is a u-blox maya-w166&lt;/P&gt;&lt;P&gt;firmware and driver version are both &lt;SPAN&gt;lf-5.15.71_2.2.0&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I have tried lf-6.6.23_2.0.0 but no difference&lt;/P&gt;&lt;P&gt;Full output is&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;# modprobe moal mod_para=nxp/wifi_mod_para.conf
[   70.725070] mlan: loading out-of-tree module taints kernel.

[   70.859894] wlan: Loading MWLAN driver
[   70.862830] wlan: Register to Bus Driver...
[   70.869680] vendor=0x02DF device=0x9159 class=0 function=1
[   70.873902] Attach moal handle ops, card interface type: 0x108
[   70.887336] SDIW416: init module param from usr cfg
[   70.890831] card_type: SDIW416, config block: 0
[   70.895396] cfg80211_wext=0xf
[   70.902521] max_vir_bss=1
[   70.903992] cal_data_cfg=none
[   70.911343] ps_mode = 1
[   70.912607] auto_ds = 1
[   70.915041] host_mlme=enable
[   70.921864] fw_name=nxp/sdiouartiw416_combo_v0.bin
[   70.925568] SDIO: max_segs=341 max_seg_size=131040
[   70.933368] rx_work=0 cpu_num=1
[   70.935197] Attach mlan adapter operations.card_type is 0x108.
[   70.944556] wlan: Enable TX SG mode
[   70.948777] wlan: Enable RX SG mode
[   70.958168] Request firmware: nxp/sdiouartiw416_combo_v0.bin
[   71.259021] Wlan: FW download over, firmwarelen=534196 downloaded 534196
[   74.256252] Fail to poll firmware status: firmwarestat=0x5f5f
[   74.260646] FW failed to be active in time!
[   74.264819] wlan_dnld_fw fail ret=0xffffffff
[   74.274195] WLAN: Fail download FW with nowwait: 0
[   74.279665] SDIO Func0 (0x0-0x9): 43 03 02 02 03 00 00 02 03 00
[   74.284455] SDIO Func1 (0x10-0x17): 00 00 00 00 ff ff ff ff
[   74.293079] SDIO Func1: (0x8) 00 (0x58) 00 (0x5c) 08 (0x5d) 00 (0x60) 07 (0x61) 0c (0x62) 00 (0x64) 10 (0x65) 00 (0x66) 00 (0x68) 00 (0x69) 00 (0x6a) 00
[   74.316762] SDIO Func1 (0xe8-0xf2): 5f 5f 08 00 05 02 08 00 24 14 70
[   74.424442] SDIO Func1 (0xe8-0xf2): 5f 5f 08 00 05 02 08 00 24 14 70
[   74.429803] woal_request_fw failed
[   74.432856] Firmware Init Failed
[   74.440741] Free module params
[   74.442422] woal_add_card failed
[   74.446103] wlan_sdio: probe of mmc0:0001:1 failed with error -1
[   74.458360] wlan: Register to Bus Driver Done
[   74.461345] wlan: Driver loaded successfully&lt;/LI-CODE&gt;</description>
      <pubDate>Wed, 26 Jun 2024 12:44:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SD8978-firmware-load-fail/m-p/1894420#M3242</guid>
      <dc:creator>vmbtech</dc:creator>
      <dc:date>2024-06-26T12:44:57Z</dc:date>
    </item>
    <item>
      <title>Re: SD8978 firmware load fail</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SD8978-firmware-load-fail/m-p/1894665#M3243</link>
      <description>&lt;P&gt;Thanks for the information.&lt;/P&gt;
&lt;P&gt;I just did a test on my side using 1XK module with an iMX8MP EVK and it is working on my side in Linux 5.15.71.&lt;/P&gt;
&lt;LI-CODE lang="c"&gt;imx8mpevk login: root
root@imx8mpevk:~# clear

root@imx8mpevk:~# modprobe moal mod_para=nxp/wifi_mod_para.conf
[   29.265837] mlan: loading out-of-tree module taints kernel.
[   29.291622] wlan: Loading MWLAN driver
[   29.295727] wlan: Register to Bus Driver...
[   29.300097] vendor=0x02DF device=0x9159 class=0 function=1
[   29.305668] Attach moal handle ops, card interface type: 0x108
[   29.312528] SDIW416: init module param from usr cfg
[   29.317469] card_type: SDIW416, config block: 0
[   29.322081] cfg80211_wext=0xf
[   29.325051] max_vir_bss=1
[   29.327684] cal_data_cfg=none
[   29.330664] ps_mode = 1
[   29.333111] auto_ds = 1
[   29.335568] host_mlme=enable
[   29.338460] fw_name=nxp/sdiouartiw416_combo_v0.bin
[   29.343276] SDIO: max_segs=128 max_seg_size=65535
[   29.347989] rx_work=1 cpu_num=4
[   29.351159] Attach mlan adapter operations.card_type is 0x108.
[   29.357334] wlan: Enable TX SG mode
[   29.360845] wlan: Enable RX SG mode
[   29.365836] Request firmware: nxp/sdiouartiw416_combo_v0.bin
[   29.612519] Wlan: FW download over, firmwarelen=534196 downloaded 534196
[   30.882123] WLAN FW is active
[   30.885105] on_time is 30883373750
[   30.910641] fw_cap_info=0x187c4f03, dev_cap_mask=0xffffffff
[   30.916264] max_p2p_conn = 8, max_sta_conn = 8
[   30.932033] Register NXP 802.11 Adapter mlan0
[   30.937986] Register NXP 802.11 Adapter uap0
[   30.945449] Register NXP 802.11 Adapter wfd0
[   30.953892] wlan: version = SDIW416---16.92.21.p55.3-MM5X16366.p5-GPL-(FP92)
[   30.962991] wlan: Register to Bus Driver Done
[   30.967473] wlan: Driver loaded successfully
root@imx8mpevk:~# uname -r
5.15.71+g95448dd0dc9b
root@imx8mpevk:~#&lt;/LI-CODE&gt;
&lt;P&gt;Are you using a custom board for the Host? Have you double checked if a HW rework is needed on your board?&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel.&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jun 2024 20:18:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SD8978-firmware-load-fail/m-p/1894665#M3243</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2024-06-26T20:18:40Z</dc:date>
    </item>
    <item>
      <title>Re: SD8978 firmware load fail</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SD8978-firmware-load-fail/m-p/1895934#M3244</link>
      <description>&lt;P&gt;Yes this is a custom board, and it may be true that some power up conditions are not 100% true to the datasheet.&lt;/P&gt;&lt;P&gt;But...&lt;/P&gt;&lt;P&gt;It would be really helpful to get the meanings of those firmwarestat values though, if at all possible.&lt;/P&gt;&lt;P&gt;"firmwarestat=0x5f5f" and f00a&lt;/P&gt;&lt;P&gt;After all, they must have a specific meaning within the module/chipset itself&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jun 2024 12:34:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SD8978-firmware-load-fail/m-p/1895934#M3244</guid>
      <dc:creator>vmbtech</dc:creator>
      <dc:date>2024-06-28T12:34:47Z</dc:date>
    </item>
    <item>
      <title>Re: SD8978 firmware load fail</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SD8978-firmware-load-fail/m-p/1896089#M3245</link>
      <description>&lt;P&gt;Could you please take a look this &lt;A href="https://community.nxp.com/t5/Wireless-Connectivity/requesting-IW416-NXP-Driver/td-p/1757319" target="_blank" rel="noopener"&gt;thread&lt;/A&gt;? Seems like a similar issue.&lt;BR /&gt;Please share with me your wifi_mod_para.conf&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel.&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jun 2024 19:44:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SD8978-firmware-load-fail/m-p/1896089#M3245</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2024-06-28T19:44:07Z</dc:date>
    </item>
    <item>
      <title>Re: SD8978 firmware load fail</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SD8978-firmware-load-fail/m-p/1896783#M3246</link>
      <description>&lt;P&gt;This is the config file&lt;/P&gt;&lt;P&gt;I know it works because the firmware load works on some prototype boards but fail on some others&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;SDIW416 = {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;cfg80211_wext=0xf&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;max_vir_bss=1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;cal_data_cfg=none&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;ps_mode=1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;auto_ds=1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;host_mlme=1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;fw_name=nxp/sdiouartiw416_combo_v0.bin&lt;BR /&gt;}&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Would still love to know what those firmwarestat values mean&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 01 Jul 2024 16:32:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SD8978-firmware-load-fail/m-p/1896783#M3246</guid>
      <dc:creator>vmbtech</dc:creator>
      <dc:date>2024-07-01T16:32:21Z</dc:date>
    </item>
    <item>
      <title>Re: SD8978 firmware load fail</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SD8978-firmware-load-fail/m-p/1896835#M3248</link>
      <description>&lt;P&gt;I will need to check this internally.&lt;/P&gt;
&lt;P&gt;Give me some time to get an update.&lt;BR /&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel.&lt;/P&gt;</description>
      <pubDate>Mon, 01 Jul 2024 18:20:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SD8978-firmware-load-fail/m-p/1896835#M3248</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2024-07-01T18:20:28Z</dc:date>
    </item>
    <item>
      <title>Re: SD8978 firmware load fail</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SD8978-firmware-load-fail/m-p/1898797#M3249</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/211766"&gt;@vmbtech&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;Please confirm the following.&lt;BR /&gt;&lt;BR /&gt;1. The log you attached is with&amp;nbsp;5.15.71 driver (SDIW416---16.92.21.p55.3-MM5X16366.p5-GPL-(FP92)) in Linux 5.15.71.&lt;/P&gt;
&lt;P&gt;2. If you do not modify the driver, you only get 0x5f5f. But if you modify the driver, you get the same 0x5f5f value, but you notice that 0xf00a appears first, am I right?&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Daniel.&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jul 2024 21:15:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SD8978-firmware-load-fail/m-p/1898797#M3249</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2024-07-03T21:15:55Z</dc:date>
    </item>
    <item>
      <title>Re: SD8978 firmware load fail</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SD8978-firmware-load-fail/m-p/1899454#M3250</link>
      <description>Yes that is all correct, 5.15.71, and the modification to the driver was to print out the value of the register for all the retries before retry limit is reached, which shows the register changing</description>
      <pubDate>Thu, 04 Jul 2024 10:03:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SD8978-firmware-load-fail/m-p/1899454#M3250</guid>
      <dc:creator>vmbtech</dc:creator>
      <dc:date>2024-07-04T10:03:54Z</dc:date>
    </item>
    <item>
      <title>Re: SD8978 firmware load fail</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SD8978-firmware-load-fail/m-p/1910233#M3251</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;I am also facing same challenge in my board. I am waiting for response&amp;nbsp;&lt;SPAN&gt;Daniel.Could you please provide any quick response on this problem. Is this firmware loading timing issue?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;/home/root# modprobe moal mod_para=nxp/wifi_mod_para.conf&lt;BR /&gt;[ 89.683485] mlan: loading out-of-tree module taints kernel.&lt;BR /&gt;[ 89.797838] wlan: Loading MWLAN driver&lt;BR /&gt;[ 89.800832] wlan: Register to Bus Driver...&lt;BR /&gt;[ 89.805006] vendor=0x02DF device=0x9159 class=0 function=1&lt;BR /&gt;[ 89.813834] Attach moal handle ops, card interface type: 0x108&lt;BR /&gt;[ 89.825702] SDIW416: init module param from usr cfg&lt;BR /&gt;[ 89.830948] card_type: SDIW416, config block: 0&lt;BR /&gt;[ 89.834215] cfg80211_wext=0xf&lt;BR /&gt;[ 89.839777] max_vir_bss=1&lt;BR /&gt;[ 89.841135] cal_data_cfg=none&lt;BR /&gt;[ 89.844028] ps_mode = 1&lt;BR /&gt;[ 89.849993] auto_ds = 1&lt;BR /&gt;[ 89.851130] host_mlme=enable&lt;BR /&gt;[ 89.853928] fw_name=nxp/sdiouartiw416_combo_v0.bin&lt;BR /&gt;[ 89.862488] SDIO: max_segs=341 max_seg_size=131040&lt;BR /&gt;[ 89.865949] rx_work=0 cpu_num=1&lt;BR /&gt;[ 89.872003] Attach mlan adapter operations.card_type is 0x108.&lt;BR /&gt;[ 89.878881] wlan: Enable TX SG mode&lt;BR /&gt;[ 89.880956] wlan: Enable RX SG mode&lt;BR /&gt;[ 89.890215] Request firmware: nxp/sdiouartiw416_combo_v0.bin&lt;BR /&gt;[ 90.194082] Wlan: FW download over, firmwarelen=534196 downloaded 534196&lt;BR /&gt;[ 93.196164] Fail to poll firmware status: firmwarestat=0x5f5f&lt;BR /&gt;[ 93.200611] FW failed to be active in time!&lt;BR /&gt;[ 93.204700] wlan_dnld_fw fail ret=0xffffffff&lt;BR /&gt;[ 93.213292] WLAN: Fail download FW with nowwait: 0&lt;BR /&gt;[ 93.221083] SDIO Func0 (0x0-0x9): 43 03 02 02 03 00 00 02 03 00&lt;BR /&gt;[ 93.225921] SDIO Func1 (0x10-0x17): 00 00 00 00 ff ff ff ff&lt;BR /&gt;[ 93.234897] SDIO Func1: (0x8) 00 (0x58) 00 (0x5c) 08 (0x5d) 00 (0x60) 07 (0x61) 0c (0x62) 00 (0x64) 10 (0x65) 00 (0x66) 00 (0x68) 00 (0x69) 00 (0x6a) 00&lt;BR /&gt;[ 93.249649] SDIO Func1 (0xe8-0xf2): 5f 5f 0c 00 06 02 08 00 24 14 70&lt;BR /&gt;[ 93.356334] SDIO Func1 (0xe8-0xf2): 5f 5f 0c 00 06 02 08 00 24 14 70&lt;BR /&gt;[ 93.361690] woal_request_fw failed&lt;BR /&gt;[ 93.364795] Firmware Init Failed&lt;BR /&gt;[ 93.373538] Free module params&lt;BR /&gt;[ 93.375337] woal_add_card failed&lt;BR /&gt;[ 93.381436] wlan_sdio: probe of mmc0:0001:1 failed with error -1&lt;BR /&gt;[ 93.391612] wlan: Register to Bus Driver Done&lt;BR /&gt;[ 93.396755] wlan: Driver loaded successfully&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jul 2024 04:40:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SD8978-firmware-load-fail/m-p/1910233#M3251</guid>
      <dc:creator>masateesh</dc:creator>
      <dc:date>2024-07-17T04:40:14Z</dc:date>
    </item>
    <item>
      <title>Re: SD8978 firmware load fail</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SD8978-firmware-load-fail/m-p/1912513#M3252</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;The values 0x5f5f and 0xf00a indicates the FW is stuck during Init time. More details about these values are for internal use only, this is why we don't have any user manual or guide available.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel.&lt;/P&gt;</description>
      <pubDate>Fri, 19 Jul 2024 17:38:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/SD8978-firmware-load-fail/m-p/1912513#M3252</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2024-07-19T17:38:39Z</dc:date>
    </item>
  </channel>
</rss>