<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wi-Fi® + Bluetooth® + 802.15.4のトピックRe: Cannot stop RF test mode continuous wave</title>
    <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Cannot-stop-RF-test-mode-continuous-wave/m-p/1883658#M2827</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;From product page &lt;A href="http://nxp.com/IW612" target="_self"&gt;nxp.com/IW612&lt;/A&gt;, I see you are using driver version "Generic_SD-WLAN-UART-BT-IW612-LNX_6_6_3-IMX8-18.99.2.p66.17-18.99.2.p66.17-MM6X18437.P3-GPL" from 08/feb/2024 which isn't the last one.&lt;BR /&gt;Could you test with the latest one "Generic_SD-WLAN-UART-BT-IW612-LNX_6_6_23-IMX8-18.99.3.p10.1-18.99.3.p10.1-MM6X18437.P21-GPL" from 06/jun/2024 please ?&lt;/P&gt;</description>
    <pubDate>Fri, 07 Jun 2024 14:11:08 GMT</pubDate>
    <dc:creator>cdoumenc</dc:creator>
    <dc:date>2024-06-07T14:11:08Z</dc:date>
    <item>
      <title>Cannot stop RF test mode continuous wave</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Cannot-stop-RF-test-mode-continuous-wave/m-p/1883590#M2826</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;following&amp;nbsp;AN14114, I am trying to run a a TX test with a carrier wave.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Firmware&lt;/STRONG&gt;:&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;SDIW612---18.99.2.p66.17-MM6X18437.p3-GPL-(FP92) on a 6.6 kernel.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am sending the following lines one by one to&amp;nbsp;&lt;FONT face="courier new,courier"&gt;/proc/mwlan/adapter0/config&lt;/FONT&gt;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;rf_test_mode=1
radio_mode=11 0
rx_antenna=1
tx_antenna=1
band=0
bw=0
channel=4
tx_power=12 2 0
tx_continuous=1 1 0xaaa 0 3 0x2106&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;I see the waveform but when I try to stop the test with the following line, nothing happens, the DUT keeps transmitting.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;tx_continuous=0&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note that in continuous packet mode (tx_continuous=1 0) I do not see this issue to stop the test.&lt;/P&gt;&lt;P&gt;This is quite inconvenient as I have to power cycle the chip every time I need to change the test channel.&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jun 2024 12:22:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Cannot-stop-RF-test-mode-continuous-wave/m-p/1883590#M2826</guid>
      <dc:creator>arthur-pg</dc:creator>
      <dc:date>2024-06-07T12:22:34Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot stop RF test mode continuous wave</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Cannot-stop-RF-test-mode-continuous-wave/m-p/1883658#M2827</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;From product page &lt;A href="http://nxp.com/IW612" target="_self"&gt;nxp.com/IW612&lt;/A&gt;, I see you are using driver version "Generic_SD-WLAN-UART-BT-IW612-LNX_6_6_3-IMX8-18.99.2.p66.17-18.99.2.p66.17-MM6X18437.P3-GPL" from 08/feb/2024 which isn't the last one.&lt;BR /&gt;Could you test with the latest one "Generic_SD-WLAN-UART-BT-IW612-LNX_6_6_23-IMX8-18.99.3.p10.1-18.99.3.p10.1-MM6X18437.P21-GPL" from 06/jun/2024 please ?&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jun 2024 14:11:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Cannot-stop-RF-test-mode-continuous-wave/m-p/1883658#M2827</guid>
      <dc:creator>cdoumenc</dc:creator>
      <dc:date>2024-06-07T14:11:08Z</dc:date>
    </item>
  </channel>
</rss>