<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 88W8887 disconnects from access point during rekeying in Wi-Fi® + Bluetooth® + 802.15.4</title>
    <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8887-disconnects-from-access-point-during-rekeying/m-p/1627721#M2775</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you please help me with the following information ? Are you using a module from one of our partners or are you working directly with the chip ? Also, which host are you using for your device?&amp;nbsp; Could you also please help me with the driver and firmware used for this ? Also, could you please share some logs as well as some air logs ?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Regards&lt;/P&gt;</description>
    <pubDate>Tue, 04 Apr 2023 13:50:56 GMT</pubDate>
    <dc:creator>stephanie_m</dc:creator>
    <dc:date>2023-04-04T13:50:56Z</dc:date>
    <item>
      <title>88W8887 disconnects from access point during rekeying</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8887-disconnects-from-access-point-during-rekeying/m-p/1625053#M2774</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;we are using the 88W8887 WiFi and Bluetooth (&lt;A href="https://www.nxp.com/products/wireless/wi-fi-plus-bluetooth-plus-802-15-4/88w8887-automotive-2-4-ghz-dual-band-1x1-wi-fi-5-802-11ac-bluetooth-5-2-plus-fm-receive-solution:88W8887A" target="_self"&gt;link&lt;/A&gt;&amp;nbsp;) module as a wireless station in our yocto project.&lt;/P&gt;
&lt;P&gt;The module connects to the access point (AP) but disconnects after 10 mins when the AP requests a group rekeying. A few seconds later our station successfully reconnects to the AP.&lt;/P&gt;
&lt;P&gt;We are using wpa_supplicant to connect to the AP. The encryption used by the AP is AES.&lt;BR /&gt;The drivers (sd8xxx) are the latest from NXP. Our kernel version is 4.2.&lt;/P&gt;
&lt;P&gt;Has anyone else observed this problem or knows what could be the issue ?&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jan 2024 17:18:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8887-disconnects-from-access-point-during-rekeying/m-p/1625053#M2774</guid>
      <dc:creator>hbabar</dc:creator>
      <dc:date>2024-01-17T17:18:13Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8887 disconnects from access point during rekeying</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8887-disconnects-from-access-point-during-rekeying/m-p/1627721#M2775</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you please help me with the following information ? Are you using a module from one of our partners or are you working directly with the chip ? Also, which host are you using for your device?&amp;nbsp; Could you also please help me with the driver and firmware used for this ? Also, could you please share some logs as well as some air logs ?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 04 Apr 2023 13:50:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8887-disconnects-from-access-point-during-rekeying/m-p/1627721#M2775</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2023-04-04T13:50:56Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8887 disconnects from access point during rekeying</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8887-disconnects-from-access-point-during-rekeying/m-p/1633856#M2776</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Hello,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;the module is LBEQ6ZZ1CL-863 from Murata which uses the 88W8887 chipset.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;We are running linux, kernel 4.2, on our system. The driver (sd8xxx) and firmware are the latest from NXP (SD-WLAN-UART-BT-8887-U16-MMC-W15.44.19.p36-15.100.19.p36-C4X15657_A2-MGPL). Attached please find the driver log and wpa_supplicant log with extended debugging and the log from the AP.&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 14 Apr 2023 11:20:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8887-disconnects-from-access-point-during-rekeying/m-p/1633856#M2776</guid>
      <dc:creator>hbabar</dc:creator>
      <dc:date>2023-04-14T11:20:27Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8887 disconnects from access point during rekeying</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8887-disconnects-from-access-point-during-rekeying/m-p/1636542#M2777</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I was not able to locate the module mentioned available, by any chance , is this a custom module ? If that is the case, could you please help me contacting the module maker for further support on the issue ? This is because there might be some specific FW&amp;nbsp; or driver configurations that will depend on the module maker.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;regards&lt;/P&gt;</description>
      <pubDate>Wed, 19 Apr 2023 20:33:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8887-disconnects-from-access-point-during-rekeying/m-p/1636542#M2777</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2023-04-19T20:33:44Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8887 disconnects from access point during rekeying</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8887-disconnects-from-access-point-during-rekeying/m-p/1637030#M2778</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;the module is from Murata which uses the 88W8887. Host device is our own CPU module based on iMX. 6SoloX running linux kernel 4.2. You can find the drivers and BSP here &lt;A title="sd8887 driver" href="https://www.nxp.com/products/wireless/wi-fi-plus-bluetooth-plus-802-15-4/1x1-dual-band-wi-fi-5-802-11ac-and-bluetooth5-2-combo-solution:88W8887" target="_self"&gt;NXP product website&lt;/A&gt; .&lt;/P&gt;&lt;P&gt;I already shared the logs in my earlier post. The logs from the sniffer are quite large (86 MBs) and as far as I can see quite unintelligible.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;hbabar&lt;/P&gt;</description>
      <pubDate>Thu, 20 Apr 2023 08:31:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8887-disconnects-from-access-point-during-rekeying/m-p/1637030#M2778</guid>
      <dc:creator>hbabar</dc:creator>
      <dc:date>2023-04-20T08:31:27Z</dc:date>
    </item>
  </channel>
</rss>