<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Does the Linux 5.10.72_2.2.0 Demo Binary include the 88W8987 driver? in Wi-Fi® + Bluetooth® + 802.15.4</title>
    <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Does-the-Linux-5-10-72-2-2-0-Demo-Binary-include-the-88W8987/m-p/1392004#M2168</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/182806"&gt;@HiroakiOkoshi&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;See Below steps, please!&lt;/P&gt;
&lt;P&gt;1. exporting cross-compiling toolchain using Yocto&lt;/P&gt;
&lt;P&gt;open&amp;nbsp;i.MX_Linux_Users_Guide.pdf, and search standalone, you will see how to export the toolchain.&lt;/P&gt;
&lt;P&gt;2. installing the toolchain(.sh file) to /opt directory.&lt;/P&gt;
&lt;P&gt;3. using source command to configure environment, like below&lt;/P&gt;
&lt;P&gt;enter into wifi's wlan_src subdirectory, and run :&lt;/P&gt;
&lt;P&gt;#source /opt/fsl-imx-fb/5.4-zeus/environment-setup-cortexa9t2hf-neon-poky-linux-gnueabi&lt;/P&gt;
&lt;P&gt;[Note]&lt;/P&gt;
&lt;P&gt;above is mine , yours should be a little different.&lt;/P&gt;
&lt;P&gt;4. setting KERNELDIR&lt;/P&gt;
&lt;P&gt;It is in yocot build(tmp/work....) directory,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;5. run make build or make&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;after compilation is done, mlan.ko &amp;amp; moal.ko are generated.&lt;/P&gt;
&lt;P&gt;these 2 files are drivers.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a good day!&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;weidong&lt;/P&gt;</description>
    <pubDate>Mon, 27 Dec 2021 02:16:33 GMT</pubDate>
    <dc:creator>weidong_sun</dc:creator>
    <dc:date>2021-12-27T02:16:33Z</dc:date>
    <item>
      <title>Does the Linux 5.10.72_2.2.0 Demo Binary include the 88W8987 driver?</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Does-the-Linux-5-10-72-2-2-0-Demo-Binary-include-the-88W8987/m-p/1391648#M2161</link>
      <description>&lt;P&gt;I simply want to set up an evaluation environment for 88W8987 (JODY-W2). The materials I have are as follows. (By the way, in the environment of zeus, YOCTO is built and it works.)&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;i.MX6Qsabresd Board&lt;/LI&gt;&lt;LI&gt;EVK-JODY-W2&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;The downloaded binary is below.&lt;/P&gt;&lt;P&gt;&lt;EM&gt;LF_v5.10.72-2.2.0_images_IMX6QPDLSOLOX.zip&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;I run to the imx6QsabreSsd board with the following command.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;&amp;gt;uuu -b emmc_all u-boot-imx6qsabresd_sd-optee.imx imx-image-full-imx6qpdlsolox.wic
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.165-0-ge10b026

Success 1    Failure 0


1:3      8/ 8 [Done                                  ] FB: done&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The first thing that surprised me when I started it was that /lib/modules/5.10.72-lts-5.10.y+ga68e31b63f86 haven't&amp;nbsp; &amp;nbsp;88W8987 module.&lt;BR /&gt;There is a 88W8987 firm in /lib/firmware/nxp/.&lt;/P&gt;&lt;P&gt;I've tried the following just in case, but I don't see any signs that modules or firms are being read.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;# modprobe moal mod_para=nxp/wifi_mod_para_sd8987.conf
# dmesg | tail 
[   21.785922] wlan: Register to Bus Driver Done
[   35.033751] usb_otg_vbus: disabling
[   35.037271] wm8962-supply: disabling
[   35.040861] MPCIE_3V3: disabling
[   35.045428] VGEN1: disabling&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does the Linux 5.10.72_2.2.0 Demo Binary include the 88W8987 driver?&lt;/P&gt;&lt;P&gt;According to the document (SCR-5.10.72-2.2.0.txt) included in LF_v5.10.72-2.2.0_images_IMX6QPDLSOLOX.zip, the following notation is given, so it was judged that the driver was included.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;NXP Software Content Register

Release - Linux 5.10.72-2.2.0
 December 2021

Outgoing License: LA_OPT_NXP_Software_License v30 October 2021 - Additional distribution license granted - Section 2.3 applies
License File:     COPYING

Yocto Project recipe manifest:
repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-hardknott -m imx_5.10.72-2.2.0.xml

Release tag: rel_imx_5.10.72-2.2.0

--------------------------------------------
BSP Packages
--------------------------------------------

--------------------------------------------

Package:                     imx-firmware.git
Version:                     
Outgoing License:            LA_OPT_NXP_Software_License v27 July 2021 - Additional distribution license granted - Section 2.3 applies 
License File:                EULA.txt
Package Category:            BSP
Type of Content:             binary
Description and comments:    BSP firmware - Bluetooth and WIFI
Release Location:            https://github.com/NXP/imx-firmware -b master
Origin:                      brcm: Broadcom Corporation (proprietary)
                             cyw-wifi-bt: Cypress Semiconductor Corporation (proprietary)
                             nxp: NXP (proprietary)

--------------------------------------------

Package:                     mwifiex.git
Version:                     
Outgoing License:            GPL-2.0 
License File:                mxm_wifiex/wlan_src/gpl-2.0.txt
Package Category:            BSP
Type of Content:             source
Description and comments:    NXP Wi-Fi linux SDK
Release Location:            https://source.codeaurora.org/external/imx/mwifiex -b rel_imx_5.10.72-2.2.0
Origin:                      NXP (GPL-2.0)

--------------------------------------------&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried to build 5.10.72-lts-5.10 YOCTO simple(repo sync &amp;amp; bitbake), but after all, the Driver of 88W8987 was not included.&lt;BR /&gt;Currently, I want to use NXP drivers, so I'd like to somehow create the latest environment for this board.&lt;/P&gt;&lt;P&gt;What should I do?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The system information is below.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx6qpdlsolox:/etc# uname -a
Linux imx6qpdlsolox 5.10.72-lts-5.10.y+ga68e31b63f86 #1 SMP PREEMPT Tue Nov 23 06:02:20 UTC 2021 armv7l armv7l armv7l GNU/Linux
root@imx6qpdlsolox:/etc# lscpu
Architecture:        armv7l
Byte Order:          Little Endian
CPU(s):              4
On-line CPU(s) list: 0-3
Thread(s) per core:  1
Core(s) per socket:  4
Socket(s):           1
Vendor ID:           ARM
Model:               10
Model name:          Cortex-A9
Stepping:            r2p10
CPU max MHz:         996.0000
CPU min MHz:         396.0000
BogoMIPS:            6.00
Flags:               half thumb fastmult vfp edsp neon vfpv3 tls vfpd32&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 24 Dec 2021 05:08:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Does-the-Linux-5-10-72-2-2-0-Demo-Binary-include-the-88W8987/m-p/1391648#M2161</guid>
      <dc:creator>HiroakiOkoshi</dc:creator>
      <dc:date>2021-12-24T05:08:11Z</dc:date>
    </item>
    <item>
      <title>Re: Does the Linux 5.10.72_2.2.0 Demo Binary include the 88W8987 driver?</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Does-the-Linux-5-10-72-2-2-0-Demo-Binary-include-the-88W8987/m-p/1391711#M2162</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/182806"&gt;@HiroakiOkoshi&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;i.MX8MN-EVK board supports 88W8987 hardware, so it's default demo image includes 8987 driver.&lt;/P&gt;
&lt;P&gt;for i.mx6q serials, you should select it in linux kernel.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;then use modprobe to load it.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a good day!&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;weidong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 24 Dec 2021 07:17:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Does-the-Linux-5-10-72-2-2-0-Demo-Binary-include-the-88W8987/m-p/1391711#M2162</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2021-12-24T07:17:37Z</dc:date>
    </item>
    <item>
      <title>Re: Does the Linux 5.10.72_2.2.0 Demo Binary include the 88W8987 driver?</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Does-the-Linux-5-10-72-2-2-0-Demo-Binary-include-the-88W8987/m-p/1391725#M2163</link>
      <description>&lt;P&gt;Do you mean this selecting?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="HiroakiOkoshi_2-1640331993232.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/166191i57B5B2D497E8258E/image-size/large?v=v2&amp;amp;px=999" role="button" title="HiroakiOkoshi_2-1640331993232.png" alt="HiroakiOkoshi_2-1640331993232.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;</description>
      <pubDate>Fri, 24 Dec 2021 07:47:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Does-the-Linux-5-10-72-2-2-0-Demo-Binary-include-the-88W8987/m-p/1391725#M2163</guid>
      <dc:creator>HiroakiOkoshi</dc:creator>
      <dc:date>2021-12-24T07:47:36Z</dc:date>
    </item>
    <item>
      <title>Re: Does the Linux 5.10.72_2.2.0 Demo Binary include the 88W8987 driver?</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Does-the-Linux-5-10-72-2-2-0-Demo-Binary-include-the-88W8987/m-p/1391733#M2164</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/182806"&gt;@HiroakiOkoshi&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;sorry, correct it.&lt;/P&gt;
&lt;P&gt;In kernel, it's Marvel driver, not latest one. below is an example for getting driver:&lt;/P&gt;
&lt;P&gt;--driver&lt;BR /&gt;#git clone &lt;A href="http://source.codeaurora.org/external/imx/mwifiex.git" target="_blank"&gt;http://source.codeaurora.org/external/imx/mwifiex.git&lt;/A&gt;&lt;BR /&gt;#git tag&lt;BR /&gt;#git checkout lf-5.10.72_2.2.0&lt;/P&gt;
&lt;P&gt;--firmware&lt;BR /&gt;&lt;A href="https://github.com/NXP/imx-firmware/tree/lf-5.10.72_2.2.0/nxp" target="_blank"&gt;https://github.com/NXP/imx-firmware/tree/lf-5.10.72_2.2.0/nxp&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;you can select related driver and firmware according to your kernel version. and compile it&amp;nbsp;separately.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a good day!&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;weidong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 24 Dec 2021 08:13:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Does-the-Linux-5-10-72-2-2-0-Demo-Binary-include-the-88W8987/m-p/1391733#M2164</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2021-12-24T08:13:14Z</dc:date>
    </item>
    <item>
      <title>Re: Does the Linux 5.10.72_2.2.0 Demo Binary include the 88W8987 driver?</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Does-the-Linux-5-10-72-2-2-0-Demo-Binary-include-the-88W8987/m-p/1391817#M2166</link>
      <description>&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;I knew that this file could be obtained with this command, but I avoided it because it is not a YOCTO recipe.&lt;BR /&gt;I tried running it with imx6qsabresd, but the error code was as follows because various environments are different in the first place.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;root@imx6qpdlsolox:/usr/src/mwifiex/mxm_wifiex/wlan_src# make build
make -C /usr/src/arm/linux_5_10_y_kernel/linux-nxp M=/usr/src/mwifiex/mxm_wifiex/wlan_src ARCH=arm64 CROSS_COMPILE=/opt/fsl-imx-internal-xwayland/5.10-gatesgarth/sysroots/x86_64-pokysdk-linux/usr/bin/aarch64-poky-linux/aarch64-poky-linux- modules
make[1]: *** /usr/src/arm/linux_5_10_y_kernel/linux-nxp: No such file or directory.  Stop.
make: *** [Makefile:565: default] Error 2&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In other words, in YOCTO's HOST environment, I have to carefully set the compiler and linux source directory and build them.&lt;/P&gt;&lt;P&gt;understand. I will try it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;user@rz3900:/work/tmp_temp/mwifiex/mxm_wifiex/wlan_src$ export CROSS_COMPILE=/work/imx-5.10.72-2.2.0.xml/build-fb/tmp/work/cortexa9t2hf-neon-poky-linux-gnueabi/util-linux-libuuid/2.36.2-r0/recipe-sysroot-native/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/10.2.0/arm-poky-linux-gnueabi-&lt;BR /&gt;user@rz3900:/work/tmp_temp/mwifiex/mxm_wifiex/wlan_src$ export KERNELDIR=/work/imx-5.10.72-2.2.0.xml/build-fb/tmp/work-shared/imx6qsabresd/kernel-build-artifacts/&lt;BR /&gt;user@rz3900:/work/tmp_temp/mwifiex/mxm_wifiex/wlan_src$ make build&lt;BR /&gt;make -C /work/imx-5.10.72-2.2.0.xml/build-fb/tmp/work-shared/imx6qsabresd/kernel-build-artifacts/ M=/work/tmp_temp/mwifiex/mxm_wifiex/wlan_src ARCH=arm64 CROSS_COMPILE=/work/imx-5.10.72-2.2.0.xml/build-fb/tmp/work/cortexa9t2hf-neon-poky-linux-gnueabi/util-linux-libuuid/2.36.2-r0/recipe-sysroot-native/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/10.2.0/arm-poky-linux-gnueabi- modules&lt;BR /&gt;make[1]: ディレクトリ '/work/imx-5.10.72-2.2.0.xml/build-fb/tmp/work-shared/imx6qsabresd/kernel-build-artifacts' に入ります&lt;BR /&gt;CC [M] /work/tmp_temp/mwifiex/mxm_wifiex/wlan_src/mlan/mlan_module.o&lt;BR /&gt;In file included from /work/imx-5.10.72-2.2.0.xml/build-fb/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/types.h:6,&lt;BR /&gt;from /work/imx-5.10.72-2.2.0.xml/build-fb/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/list.h:5,&lt;BR /&gt;from /work/imx-5.10.72-2.2.0.xml/build-fb/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/module.h:12,&lt;BR /&gt;from /work/tmp_temp/mwifiex/mxm_wifiex/wlan_src/mlan/mlan_module.c:29:&lt;BR /&gt;/work/imx-5.10.72-2.2.0.xml/build-fb/tmp/work-shared/imx6qsabresd/kernel-source/include/uapi/linux/types.h:5:10: fatal error: asm/types.h: No such file or directory&lt;BR /&gt;5 | #include &amp;lt;asm/types.h&amp;gt;&lt;BR /&gt;| ^~~~~~~~~~~~~&lt;BR /&gt;compilation terminated.&lt;BR /&gt;/work/imx-5.10.72-2.2.0.xml/build-fb/tmp/work-shared/imx6qsabresd/kernel-source/scripts/Makefile.build:280: recipe for target '/work/tmp_temp/mwifiex/mxm_wifiex/wlan_src/mlan/mlan_module.o' failed&lt;BR /&gt;make[3]: *** [/work/tmp_temp/mwifiex/mxm_wifiex/wlan_src/mlan/mlan_module.o] Error 1&lt;BR /&gt;/work/imx-5.10.72-2.2.0.xml/build-fb/tmp/work-shared/imx6qsabresd/kernel-source/Makefile:1822: recipe for target '/work/tmp_temp/mwifiex/mxm_wifiex/wlan_src' failed&lt;BR /&gt;make[2]: *** [/work/tmp_temp/mwifiex/mxm_wifiex/wlan_src] Error 2&lt;BR /&gt;/work/imx-5.10.72-2.2.0.xml/build-fb/tmp/work-shared/imx6qsabresd/kernel-source/Makefile:185: recipe for target '__sub-make' failed&lt;BR /&gt;make[1]: *** [__sub-make] Error 2&lt;BR /&gt;make[1]: ディレクトリ '/work/imx-5.10.72-2.2.0.xml/build-fb/tmp/work-shared/imx6qsabresd/kernel-build-artifacts' から出ます&lt;BR /&gt;Makefile:565: recipe for target 'default' failed&lt;BR /&gt;make: *** [default] Error 2&lt;/PRE&gt;&lt;P&gt;I tried it, but it doesn't fit.&lt;BR /&gt;Give up and think about other things.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 24 Dec 2021 10:40:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Does-the-Linux-5-10-72-2-2-0-Demo-Binary-include-the-88W8987/m-p/1391817#M2166</guid>
      <dc:creator>HiroakiOkoshi</dc:creator>
      <dc:date>2021-12-24T10:40:02Z</dc:date>
    </item>
    <item>
      <title>Re: Does the Linux 5.10.72_2.2.0 Demo Binary include the 88W8987 driver?</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Does-the-Linux-5-10-72-2-2-0-Demo-Binary-include-the-88W8987/m-p/1392004#M2168</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/182806"&gt;@HiroakiOkoshi&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;See Below steps, please!&lt;/P&gt;
&lt;P&gt;1. exporting cross-compiling toolchain using Yocto&lt;/P&gt;
&lt;P&gt;open&amp;nbsp;i.MX_Linux_Users_Guide.pdf, and search standalone, you will see how to export the toolchain.&lt;/P&gt;
&lt;P&gt;2. installing the toolchain(.sh file) to /opt directory.&lt;/P&gt;
&lt;P&gt;3. using source command to configure environment, like below&lt;/P&gt;
&lt;P&gt;enter into wifi's wlan_src subdirectory, and run :&lt;/P&gt;
&lt;P&gt;#source /opt/fsl-imx-fb/5.4-zeus/environment-setup-cortexa9t2hf-neon-poky-linux-gnueabi&lt;/P&gt;
&lt;P&gt;[Note]&lt;/P&gt;
&lt;P&gt;above is mine , yours should be a little different.&lt;/P&gt;
&lt;P&gt;4. setting KERNELDIR&lt;/P&gt;
&lt;P&gt;It is in yocot build(tmp/work....) directory,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;5. run make build or make&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;after compilation is done, mlan.ko &amp;amp; moal.ko are generated.&lt;/P&gt;
&lt;P&gt;these 2 files are drivers.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a good day!&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;weidong&lt;/P&gt;</description>
      <pubDate>Mon, 27 Dec 2021 02:16:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Does-the-Linux-5-10-72-2-2-0-Demo-Binary-include-the-88W8987/m-p/1392004#M2168</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2021-12-27T02:16:33Z</dc:date>
    </item>
    <item>
      <title>Re: Does the Linux 5.10.72_2.2.0 Demo Binary include the 88W8987 driver?</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Does-the-Linux-5-10-72-2-2-0-Demo-Binary-include-the-88W8987/m-p/1392628#M2169</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Thanks weidong.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;However ...&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;I could build driver.(*1)&lt;/LI&gt;&lt;LI&gt;I can't find sd8987.ko in bin_wlan directory.(*1)&lt;/LI&gt;&lt;LI&gt;Building from mwifiex generated mlan.ko and moal.ko.&amp;nbsp; &amp;nbsp;mlan.ko and moal.ko were prepared.(*2)&lt;/LI&gt;&lt;LI&gt;If I think about another point of view, I suspect that there is a problem with the device tree selection, not with the driver build.&lt;/LI&gt;&lt;LI&gt;I checked dmesg and it seems that sdio is not found. (*3)&lt;/LI&gt;&lt;LI&gt;If so, which of should I select the dtb file, JODY-W2 (88W8987) is connected to SD3 of imx6qsabresd. (*4)&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;(*1)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;$ make build
make -C /work/imx-yocto-bsp-imx-5.10.72-2.2.0.xml/build-fb/tmp/work-shared/imx6qsabresd/kernel-build-artifacts/ M=/work/imx-yocto-bsp-imx-5.10.72-2.2.0.xml/wifi_src/mwifiex/mxm_wifiex/wlan_src ARCH=arm CROSS_COMPILE=arm
make[1]: ディレクトリ '/work/imx-yocto-bsp-imx-5.10.72-2.2.0.xml/build-fb/tmp/work-shared/imx6qsabresd/kernel-build-artifacts' に入ります
  CC [M]  /work/imx-yocto-bsp-imx-5.10.72-2.2.0.xml/wifi_src/mwifiex/mxm_wifiex/wlan_src/mlan/mlan_shim.o
  CC [M]  /work/imx-yocto-bsp-imx-5.10.72-2.2.0.xml/wifi_src/mwifiex/mxm_wifiex/wlan_src/mlan/mlan_init.o
..................................
arm-poky-linux-gnueabi-gcc  -mthumb -mfpu=neon -mfloat-abi=hard -mcpu=cortex-a9 -fstack-protector-strong  -O2 -D_FORTIFY_SOURCE=2 -Wformat -Wformat-security -Werror=format-security --sysroot=/opt/fsl-imx-fb/5.10-hardkno
make[1]: ディレクトリ '/work/imx-yocto-bsp-imx-5.10.72-2.2.0.xml/wifi_src/mwifiex/mxm_wifiex/wlan_src/mapp/mlanutl' から出ます

user@rz3900:/work/imx-yocto-bsp-imx-5.10.72-2.2.0.xml/wifi_src/mwifiex/mxm_wifiex/wlan_src$ ls  -al ../bin_wlan/
total 1748
drwxrwxr-x 3 user user   4096 Dec 28 17:01 .
drwxrwxr-x 4 user user   4096 Dec 28 17:01 ..
-rw-rw-r-- 1 user user  62609 Dec 28 17:52 README_MLAN
drwxrwxr-x 2 user user   4096 Dec 28 17:01 config
-rw-rw-r-- 1 user user    302 Dec 28 16:51 load
-rw-rw-r-- 1 user user 681056 Dec 28 17:52 mlan.ko
-rwxrwxr-x 1 user user  51100 Dec 28 17:52 mlanutl
-rw-rw-r-- 1 user user 964364 Dec 28 17:52 moal.ko
-rw-rw-r-- 1 user user    356 Dec 28 16:51 unload
user@rz3900:/work/imx-yocto-bsp-imx-5.10.72-2.2.0.xml/wifi_src/mwifiex/mxm_wifiex/wlan_src$&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;(*2)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx6qpdlsolox:~# ls -al /lib/modules/5.10.72-lts-5.10.y+ga68e31b63f86/extra/
total 1724
drwxr-xr-x 2 root root   4096 Mar  9  2018 .
drwxr-xr-x 4 root root   4096 Dec 23 09:37 ..
-rw-r--r-- 1 root root  63324 Mar  9  2018 cryptodev.ko
-rw-r--r-- 1 root root 698792 Mar  9  2018 mlan.ko
-rw-r--r-- 1 root root 987388 Mar  9  2018 moal.ko&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(*3)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx6qpdlsolox:~# dmesg | head
[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Linux version 5.10.72-lts-5.10.y+ga68e31b63f86 (oe-user@oe-host) (arm-poky-linux-gnueabi-gcc (GCC) 10.2.0, GNU ld (GNU Binutils) 2.36.1.20210209) #1 SMP PREEMPT Tue Nov 23 06:02:20 UTC 2021
[    0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c5787d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] OF: fdt: Machine model: Freescale i.MX6 Quad SABRE Smart Device Board
[    0.000000] Memory policy: Data cache writealloc
[    0.000000] Reserved memory: created CMA memory pool at 0x3c000000, size 320 MiB
[    0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[    0.000000] Zone ranges:
[    0.000000]   Normal   [mem 0x0000000010000000-0x000000004fffffff]&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(*4)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx6qpdlsolox:/lib/modules/5.10.72-lts-5.10.y+ga68e31b63f86/extra# ls -al /run/media/mmcblk3p1/imx6q-sabresd*
-rwxrwx--- 1 root disk 54201 Apr  5  2011 /run/media/mmcblk3p1/imx6q-sabresd-btwifi.dtb
-rwxrwx--- 1 root disk 53385 Apr  5  2011 /run/media/mmcblk3p1/imx6q-sabresd-enetirq.dtb
-rwxrwx--- 1 root disk 53249 Apr  5  2011 /run/media/mmcblk3p1/imx6q-sabresd-hdcp.dtb
-rwxrwx--- 1 root disk 53176 Apr  5  2011 /run/media/mmcblk3p1/imx6q-sabresd-ldo.dtb
-rwxrwx--- 1 root disk 53252 Apr  5  2011 /run/media/mmcblk3p1/imx6q-sabresd-pcie-ep.dtb
-rwxrwx--- 1 root disk 53252 Apr  5  2011 /run/media/mmcblk3p1/imx6q-sabresd-pcie.dtb
-rwxrwx--- 1 root disk 53340 Apr  5  2011 /run/media/mmcblk3p1/imx6q-sabresd-uart.dtb
-rwxrwx--- 1 root disk 53256 Dec 24 11:05 /run/media/mmcblk3p1/imx6q-sabresd.dtb
-rwxrwx--- 1 root disk 53256 Apr  5  2011 /run/media/mmcblk3p1/imx6q-sabresd.dtb.org&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks mush support.&lt;/P&gt;&lt;P&gt;Hiroaki.&lt;/P&gt;</description>
      <pubDate>Tue, 28 Dec 2021 09:47:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Does-the-Linux-5-10-72-2-2-0-Demo-Binary-include-the-88W8987/m-p/1392628#M2169</guid>
      <dc:creator>HiroakiOkoshi</dc:creator>
      <dc:date>2021-12-28T09:47:12Z</dc:date>
    </item>
    <item>
      <title>Re: Does the Linux 5.10.72_2.2.0 Demo Binary include the 88W8987 driver?</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Does-the-Linux-5-10-72-2-2-0-Demo-Binary-include-the-88W8987/m-p/1392681#M2170</link>
      <description>&lt;P&gt;Hi All.&lt;/P&gt;&lt;P&gt;The problem has been solved.&lt;/P&gt;&lt;P&gt;The root cause was &lt;STRONG&gt;less contact SDIO connector.&lt;/STRONG&gt;&lt;BR /&gt;Sorry for the misguided discussion&lt;/P&gt;&lt;P&gt;[Conclusion]&lt;/P&gt;&lt;P&gt;"Does the Linux 5.10.72_2.2.0 Demo Binary include the 88W8987 driver?"&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;"Yes!!!!"&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;[Procedure (imx6qsabresd emmc boot)]&lt;/P&gt;&lt;P&gt;1.Get LF_v5.10.72-2.2.0_images_IMX6QPDLSOLOX.zip from the NXP site.&lt;/P&gt;&lt;P&gt;2.Flash (SW6=[00000000] )&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;&amp;gt;uuu -b emmc_all u-boot-imx6qsabresd_sd-optee.imx imx-image-full-imx6qpdlsolox.wic&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;3.As follows (SW6=[01101011])&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx6qpdlsolox:~# modprobe moal mod_para=nxp/wifi_mod_para_sd8987.conf
[   23.157341] mlan: loading out-of-tree module taints kernel.
[   23.250455] wlan: Loading MWLAN driver
[   23.254750] wlan: Driver loaded successfully
[   23.259126] wlan: Register to Bus Driver...
[   23.269119] vendor=0x02DF device=0x9149 class=0 function=1
[   23.274969] Attach moal handle ops, card interface type: 0x105
[   23.287963] SD8987: init module param from usr cfg
[   23.292797] card_type: SD8987, config block: 0
[   23.297310] cfg80211_wext=0xf
[   23.300284] max_vir_bss=1
[   23.302911] cal_data_cfg=none
[   23.305923] ps_mode = 1
[   23.308382] auto_ds = 1
[   23.310845] host_mlme=enable
[   23.313775] fw_name=nxp/sdiouart8987_combo_v0.bin
[   23.318522] SDIO: max_segs=128 max_seg_size=65535
[   23.323237] rx_work=1 cpu_num=4
[   23.326615] Attach mlan adapter operations.card_type is 0x105.
[   23.338615] wlan: Enable TX SG mode
[   23.342110] wlan: Enable RX SG mode
[   23.363836] Request firmware: nxp/sdiouart8987_combo_v0.bin
[   23.871997] Wlan: FW download over, firmwarelen=568984 downloaded 568984
[   24.833953] WLAN FW is active
[   24.836945] on_time is 24833286335
[   24.873885] fw_cap_info=0x181c7f03, dev_cap_mask=0xffffffff
[   24.879505] max_p2p_conn = 8, max_sta_conn = 8
[   24.909831] wlan: version = SD8987----16.92.21.p11.1-MM5X16283.p2-GPL-(FP92)
[   24.918892] wlan: Register to Bus Driver Done

root@imx6qpdlsolox:~# iwconfig
lo        no wireless extensions.

eth0      no wireless extensions.

sit0      no wireless extensions.

mlan0     IEEE 802.11-DS  ESSID:""
          Mode:Managed  Access Point: Not-Associated   Bit Rate:1 Mb/s
          Tx-Power=24 dBm
          Retry limit:9   RTS thr=2347 B   Fragment thr=2346 B
          Encryption key:off
          Power Management:on
          Link Quality=0/5  Signal level=0 dBm  Noise level=0 dBm
          Rx invalid nwid:0  Rx invalid crypt:0  Rx invalid frag:2
          Tx excessive retries:0  Invalid misc:0   Missed beacon:0

uap0      IEEE 802.11-DS  ESSID:""
          Mode:Master  Frequency:2.437 GHz  Access Point: Not-Associated
          Encryption key:off
          Link Quality:0  Signal level:0  Noise level:0
          Rx invalid nwid:0  Rx invalid crypt:0  Rx invalid frag:0
          Tx excessive retries:0  Invalid misc:0   Missed beacon:0

wfd0      IEEE 802.11-DS  ESSID:""
          Mode:Managed  Access Point: Not-Associated   Bit Rate:1 Mb/s
          Tx-Power=24 dBm
          Retry limit:9   RTS thr=2347 B   Fragment thr=2346 B
          Encryption key:off
          Power Management:on
          Link Quality=0/5  Signal level=0 dBm  Noise level=0 dBm
          Rx invalid nwid:0  Rx invalid crypt:0  Rx invalid frag:2
          Tx excessive retries:0  Invalid misc:0   Missed beacon:0

root@imx6qpdlsolox:~# lscpu
Architecture:        armv7l
Byte Order:          Little Endian
CPU(s):              4
On-line CPU(s) list: 0-3
Thread(s) per core:  1
Core(s) per socket:  4
Socket(s):           1
Vendor ID:           ARM
Model:               10
Model name:          Cortex-A9
Stepping:            r2p10
CPU max MHz:         996.0000
CPU min MHz:         396.0000
BogoMIPS:            6.00
Flags:               half thumb fastmult vfp edsp neon vfpv3 tls vfpd32

root@imx6qpdlsolox:/etc# head -80  /lib/firmware/nxp/wifi_mod_para_sd8987.conf | tail -10

SD8987 = {
        cfg80211_wext=0xf
        max_vir_bss=1
        cal_data_cfg=none
        ps_mode=1
        auto_ds=1
        host_mlme=1
        fw_name=nxp/sdiouart8987_combo_v0.bin
}

root@imx6qpdlsolox:~# uname -a
Linux imx6qpdlsolox 5.10.72-lts-5.10.y+ga68e31b63f86 #1 SMP PREEMPT Tue Nov 23 06:02:20 UTC 2021 armv7l armv7l armv7l GNU/Linux

root@imx6qpdlsolox:/etc# lsmod
Module                  Size  Used by
moal                  671744  0
mlan                  540672  1 moal
caam_jr               143360  0
caamkeyblob_desc       16384  1 caam_jr
caamhash_desc          16384  1 caam_jr
caamalg_desc           57344  1 caam_jr
crypto_engine          16384  1 caam_jr
rng_core               20480  1 caam_jr
authenc                16384  1 caam_jr
libdes                 28672  1 caam_jr
mxc_v4l2_capture       32768  0
ipu_bg_overlay_sdc     16384  1 mxc_v4l2_capture
ipu_still              16384  1 mxc_v4l2_capture
ipu_prp_enc            16384  1 mxc_v4l2_capture
ipu_csi_enc            16384  1 mxc_v4l2_capture
ipu_fg_overlay_sdc     16384  1 mxc_v4l2_capture
imx_vdoa               16384  0
ov5640_camera_mipi_int    32768  0
ov5640_camera_int      32768  0
v4l2_int_device        16384  3 ov5640_camera_mipi_int,ov5640_camera_int,mxc_v4l2_capture
caam                   20480  1 caam_jr
secvio                 16384  0
error                  20480  6 caamkeyblob_desc,caamalg_desc,caamhash_desc,caam_jr,caam,secvio&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Very Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 28 Dec 2021 13:03:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Does-the-Linux-5-10-72-2-2-0-Demo-Binary-include-the-88W8987/m-p/1392681#M2170</guid>
      <dc:creator>HiroakiOkoshi</dc:creator>
      <dc:date>2021-12-28T13:03:03Z</dc:date>
    </item>
  </channel>
</rss>