<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wi-Fi® + Bluetooth® + 802.15.4中的主题 Re: Configuration for AW-CM358 M.2 Module with imx8mp</title>
    <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Configuration-for-AW-CM358-M-2-Module-with-imx8mp/m-p/1411164#M2051</link>
    <description>&lt;P&gt;Are there changes needed to the device tree for the imx8mp in order to use the AW-CM358MA radio module?&lt;/P&gt;</description>
    <pubDate>Wed, 09 Feb 2022 16:24:02 GMT</pubDate>
    <dc:creator>amberworth</dc:creator>
    <dc:date>2022-02-09T16:24:02Z</dc:date>
    <item>
      <title>Configuration for AW-CM358 M.2 Module with imx8mp</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Configuration-for-AW-CM358-M-2-Module-with-imx8mp/m-p/1404045#M2049</link>
      <description>&lt;P&gt;Trying to get an AW-CM 358 m.2 radio module to work with an imx8mp evk board running Linux.&lt;/P&gt;
&lt;P&gt;What configuration changes are needed to get the radio module to come up?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;After swapping the module that comes with the evk for the AW-CM358 m.2 module, the radio is not coming up.&lt;/P&gt;
&lt;P&gt;Just to make sure it was not our sw changes, I loaded the board with LF_v5.10.72-2.2.0_images_IMX8MPEVK.zip but the radio module is not being seen.&lt;/P&gt;
&lt;P&gt;Thank you,&lt;/P&gt;
&lt;P&gt;Amber&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jan 2024 18:45:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Configuration-for-AW-CM358-M-2-Module-with-imx8mp/m-p/1404045#M2049</guid>
      <dc:creator>amberworth</dc:creator>
      <dc:date>2024-01-17T18:45:03Z</dc:date>
    </item>
    <item>
      <title>Re: Configuration for AW-CM358 M.2 Module with imx8mp</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Configuration-for-AW-CM358-M-2-Module-with-imx8mp/m-p/1405592#M2050</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/130074"&gt;@amberworth&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I will suggest to check the following two applications notes:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;UM11483&lt;/LI&gt;
&lt;LI&gt;UM11490&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;These two application notes describe how to set the driver and enable the module and its different features.&lt;/P&gt;
&lt;P&gt;BR,&lt;/P&gt;
&lt;P&gt;Alexis Andalon&lt;/P&gt;</description>
      <pubDate>Thu, 27 Jan 2022 00:06:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Configuration-for-AW-CM358-M-2-Module-with-imx8mp/m-p/1405592#M2050</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2022-01-27T00:06:37Z</dc:date>
    </item>
    <item>
      <title>Re: Configuration for AW-CM358 M.2 Module with imx8mp</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Configuration-for-AW-CM358-M-2-Module-with-imx8mp/m-p/1411164#M2051</link>
      <description>&lt;P&gt;Are there changes needed to the device tree for the imx8mp in order to use the AW-CM358MA radio module?&lt;/P&gt;</description>
      <pubDate>Wed, 09 Feb 2022 16:24:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Configuration-for-AW-CM358-M-2-Module-with-imx8mp/m-p/1411164#M2051</guid>
      <dc:creator>amberworth</dc:creator>
      <dc:date>2022-02-09T16:24:02Z</dc:date>
    </item>
    <item>
      <title>Re: Configuration for AW-CM358 M.2 Module with imx8mp</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Configuration-for-AW-CM358-M-2-Module-with-imx8mp/m-p/1411431#M2052</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/130074"&gt;@amberworth&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;If you're using the image in the following &lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX?tab=In-Depth_Tab" target="_self"&gt;link&lt;/A&gt; you shouldn't need any change to the device tree and the other extra steps would be enable the SDIO interface as it mention in the&amp;nbsp;3.5 88W8987-based AzureWave AW-CM358MA module section in the app note that I previously mention.&lt;/P&gt;
&lt;P&gt;BR,&lt;/P&gt;
&lt;P&gt;Alexis Andalon&lt;/P&gt;</description>
      <pubDate>Thu, 10 Feb 2022 01:32:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Configuration-for-AW-CM358-M-2-Module-with-imx8mp/m-p/1411431#M2052</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2022-02-10T01:32:19Z</dc:date>
    </item>
    <item>
      <title>Re: Configuration for AW-CM358 M.2 Module with imx8mp</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Configuration-for-AW-CM358-M-2-Module-with-imx8mp/m-p/1416172#M2053</link>
      <description>&lt;P&gt;I was finally able to get the AW-CM358MA module to work by modifying the device tree to enable SDIO and disable pcie.&lt;/P&gt;&lt;P&gt;For anyone else that runs into this issue.&amp;nbsp; The DTB blob that worked for me is&amp;nbsp;imx8mp-evk-usdhc1-m2.dtb.&lt;/P&gt;</description>
      <pubDate>Fri, 18 Feb 2022 19:20:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/Configuration-for-AW-CM358-M-2-Module-with-imx8mp/m-p/1416172#M2053</guid>
      <dc:creator>amberworth</dc:creator>
      <dc:date>2022-02-18T19:20:23Z</dc:date>
    </item>
  </channel>
</rss>