<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wi-Fi® + Bluetooth® + 802.15.4のトピックRe: 88W8997 module command timeout issue (interface PCIE+UART, Host: iMX8MQ) - reopen</title>
    <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1901843#M1732</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186184"&gt;@ArthurC&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please find my inline response.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Why there is "Block woal_cfg80211_scan in abnormal driver state" in dmesg ?&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;[Christine] This message comes when driver receive debug_dump command, at that time driver start process hang because we need to read register values from the FW. And part of this process we are getting the message “&lt;STRONG&gt;&lt;I&gt;Block woal_cfg80211_scan in abnormal driver state&lt;/I&gt;&lt;/STRONG&gt;”, which is expected behavior when FW dump command executed.&lt;/P&gt;
&lt;P&gt;Please see below dmesg logs time stamp:&lt;/P&gt;
&lt;P&gt;=========&lt;/P&gt;
&lt;P&gt;Line 8913: [ 222.932159] wlan: Received &lt;STRONG&gt;disassociation&lt;/STRONG&gt; request on wlan0, reason: 3 //Christine&lt;BR /&gt;Line 8917: [ 222.950041] QUEUE_CMD: 802_11_DEAUTHENTICATE [0x24] is queued //Christine&lt;BR /&gt;Line 9900: [ 226.251348] wlan: HostMlme wlan0 &lt;STRONG&gt;Connected&lt;/STRONG&gt; to bssid bc:XX:XX:XX:03:1a successfully //Christine&lt;BR /&gt;Line 43302: [ 910.377127] &lt;STRONG&gt;Recevie debug_dump command&lt;/STRONG&gt; //Christine&lt;BR /&gt;Line 43449: [ 930.816864] ====PCIE DEBUG MODE OUTPUT END: 930.815566 ==== //Christine&lt;BR /&gt;Line 43457: [ 930.834633] Block woal_cfg80211_del_key in abnormal driver state //Christine&lt;BR /&gt;Line 43478: [ 930.904799] IOCTL is not allowed while the device is not present or hang //Christine&lt;BR /&gt;Line 43479: [ 930.946102] &lt;STRONG&gt;Block woal_cfg80211_scan in abnormal driver state&lt;/STRONG&gt; //Christine&lt;/P&gt;
&lt;P&gt;=============&lt;/P&gt;
&lt;P aria-hidden="true"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Why the ip is disapper during iperf3 test?&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;[Christine]&lt;/P&gt;
&lt;P&gt;- Is it disappear before driver receive debug_dump command or after? If after then expected behavior as explained in point 1.&lt;/P&gt;
&lt;P&gt;- Also, during re-connection process there might chance ip disappear.&lt;/P&gt;
&lt;P&gt;- And even this IP handling will done by Network Manager, FW and Driver will not do anything. Customer always debug in their Network Manager path.&lt;/P&gt;
&lt;P aria-hidden="true"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Why Wi-Fi feature is broken &amp;amp; no working any more?&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;[Christine] After debug_dump command, Wi-Fi features will break, if auto_fw_reload is enable then it will reset the FW and work well. But in the given logs, we didn't see any Wi-Fi features broke before manually execute FW dump.&lt;/P&gt;
&lt;P aria-hidden="true"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;How the NXP concluded there is no any issue?&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;[Christine] As per log analysis, we are not seeing any issue from Driver and FW perspective. DUT able to re-connect with the same AP after disconnection.&lt;/P&gt;
&lt;P aria-hidden="true"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Is the firmware sending cheatting command to software?&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;[Christine] Sorry, I could not understand this question. What we concluded above is based on given logs.&lt;/P&gt;
&lt;P&gt;One point from your older comment, you mentioned “&lt;STRONG&gt;&lt;I&gt;We think the system hang and 0x107 timeout are caused by auto_fw_reload when issue occurred&lt;/I&gt;&lt;/STRONG&gt;”, Is this behavior observed every time? If yes, then we can discuss this point with our internal team.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Christine.&lt;/P&gt;</description>
    <pubDate>Mon, 08 Jul 2024 07:01:56 GMT</pubDate>
    <dc:creator>Christine_Li</dc:creator>
    <dc:date>2024-07-08T07:01:56Z</dc:date>
    <item>
      <title>88W8997 module command timeout issue (interface PCIE+UART, Host: iMX8MQ) - reopen</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1824856#M1582</link>
      <description>&lt;P&gt;The FW crashed issue is still exist in Generic_PCIE-WLAN-UART-BT-8997-LNX_6_6_3-IMX8-16.92.21.p119.2-16.92.21.p119.2-MM6X16437.P3-GPL.&lt;/P&gt;&lt;P&gt;follow previous case:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Wireless-Connectivity/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1824807/emcs_t/S2h8ZW1haWx8dG9waWNfc3Vic2NyaXB0aW9ufExUTUswN1I5SlBGRDBLfDE4MjQ4MDd8U1VCU0NSSVBUSU9OU3xoSw" target="_blank"&gt;https://community.nxp.com/t5/Wireless-Connectivity/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1824807/emcs_t/S2h8ZW1haWx8dG9waWNfc3Vic2NyaXB0aW9ufExUTUswN1I5SlBGRDBLfDE4MjQ4MDd8U1VCU0NSSVBUSU9OU3xoSw&lt;/A&gt;&lt;/P&gt;&lt;P&gt;and reopen by this case.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186184" target="_blank"&gt;@ArthurC&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205377" target="_self"&gt;@Christine_Li&lt;/A&gt;&lt;BR /&gt;&lt;LI-PRODUCT title="88W8997" id="88W8997"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Mar 2024 07:24:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1824856#M1582</guid>
      <dc:creator>yao_feng</dc:creator>
      <dc:date>2024-03-11T07:24:59Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8997 module command timeout issue (interface PCIE+UART, Host: iMX8MQ) - reopen</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1824913#M1583</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/144174"&gt;@yao_feng&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Can you please help to provide the dmesg+ fw_dump +drv_dump logs based on the new release?&lt;/P&gt;
&lt;P&gt;Please pay attention to the parameter:&amp;nbsp;&lt;SPAN&gt;drvdbg&amp;nbsp;=&amp;nbsp;0xa0037​ when load drivers and make sure FW dump is available. After issue is occurred, directly export the logs without rebooting your device. Once device is reboot, FW dump will be lost.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Also do not use below command before export the failed logs because below command will automatically trigger another FW dump and it will override the real failed one.&lt;/SPAN&gt;&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;echo debug_dump &amp;gt; /proc/mwlan/adapter0/config &lt;/LI-CODE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Christine.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Mar 2024 08:12:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1824913#M1583</guid>
      <dc:creator>Christine_Li</dc:creator>
      <dc:date>2024-03-11T08:12:44Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8997 module command timeout issue (interface PCIE+UART, Host: iMX8MQ) - reopen</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1824922#M1584</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186184"&gt;@ArthurC&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Could you please help to share with NXP:&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;dmesg&lt;BR /&gt;fw_dump&lt;BR /&gt;drv_dump&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;based on new release.&lt;BR /&gt;&lt;SPAN&gt;parameter&amp;nbsp;&lt;/SPAN&gt;settings:&amp;nbsp;&lt;SPAN&gt;drvdbg&amp;nbsp;=&amp;nbsp;0xa0037&lt;BR /&gt;&lt;BR /&gt;After issue is occurred, directly export the logs without rebooting your device. Once device is reboot, FW dump will be lost.&lt;BR /&gt;&lt;BR /&gt;!!! Don't do below before export logs. it will overwrite the old one.&lt;/SPAN&gt;&lt;/P&gt;&lt;PRE&gt;echo debug_dump &amp;gt; /proc/mwlan/adapter0/config &lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;</description>
      <pubDate>Mon, 11 Mar 2024 08:26:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1824922#M1584</guid>
      <dc:creator>yao_feng</dc:creator>
      <dc:date>2024-03-11T08:26:22Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8997 module command timeout issue (interface PCIE+UART, Host: iMX8MQ) - reopen</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1824946#M1585</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/144174"&gt;@yao_feng&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As we know this is the same log showing in dmesg, but it is needed time to repoeduce (over 3 days test).&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please help to compare the difference between 16.92.21.p255 test_19_12 &amp;amp;&amp;nbsp;&lt;SPAN&gt;Generic_PCIE-WLAN-UART-BT-8997-LNX_6_6_3-IMX8-16.92.21.p119.2-16.92.21.p119.2-MM6X16437.P3-GPL first.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;We will provide the log with parameter&amp;nbsp;settings:&amp;nbsp;drvdbg&amp;nbsp;=&amp;nbsp;0xa0037 when issue&amp;nbsp;repoeduced again.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Mar 2024 08:50:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1824946#M1585</guid>
      <dc:creator>ArthurC</dc:creator>
      <dc:date>2024-03-11T08:50:47Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8997 module command timeout issue (interface PCIE+UART, Host: iMX8MQ) - reopen</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1825671#M1586</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205377"&gt;@Christine_Li&lt;/a&gt;,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;On waiting the official release about Wi-Fi FW crashing issue fixed.&lt;/P&gt;</description>
      <pubDate>Tue, 12 Mar 2024 03:15:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1825671#M1586</guid>
      <dc:creator>ArthurC</dc:creator>
      <dc:date>2024-03-12T03:15:03Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8997 module command timeout issue (interface PCIE+UART, Host: iMX8MQ) - reopen</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1825692#M1587</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186184"&gt;@ArthurC&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;I am checking with our internal team, will share with you once have any updates.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Christine.&lt;/P&gt;</description>
      <pubDate>Tue, 12 Mar 2024 03:33:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1825692#M1587</guid>
      <dc:creator>Christine_Li</dc:creator>
      <dc:date>2024-03-12T03:33:49Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8997 module command timeout issue (interface PCIE+UART, Host: iMX8MQ) - reopen</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1826952#M1588</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/144174"&gt;@yao_feng&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;During the test thease days as 88W8997 Wi-Fi driver probing with parameter "&lt;SPAN&gt;drvdbg&amp;nbsp;=&amp;nbsp;0xa0037"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We found the FW&amp;nbsp;Generic_PCIE-WLAN-UART-BT-8997-LNX_6_6_3-IMX8-16.92.21.p119.2-16.92.21.p119.2-MM6X16437.P3-GPL which will cause host system hanging &amp;amp; crashed.&lt;/P&gt;&lt;P&gt;So we can't dump the internal logs by following command.&lt;/P&gt;&lt;PRE&gt;echo debug_dump &amp;gt; /proc/mwlan/adapter0/config &lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What's the power consumption about the module 88W8997 caused by FW&amp;nbsp;Generic_PCIE-WLAN-UART-BT-8997-LNX_6_6_3-IMX8-16.92.21.p119.2-16.92.21.p119.2-MM6X16437.P3-GPL ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The dmesg about driver probed with parameter "&lt;SPAN&gt;drvdbg&amp;nbsp;=&amp;nbsp;0xa0037" from start to&amp;nbsp;host system hanging &amp;amp; crashed is as attached.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please to analysis and fix issue.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Mar 2024 08:27:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1826952#M1588</guid>
      <dc:creator>ArthurC</dc:creator>
      <dc:date>2024-03-13T08:27:40Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8997 module command timeout issue (interface PCIE+UART, Host: iMX8MQ) - reopen</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1826976#M1589</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186184"&gt;@ArthurC&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Please help to share your bring up commands.&lt;BR /&gt;for the current log, there is no WiFi FW hang message.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 13 Mar 2024 08:45:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1826976#M1589</guid>
      <dc:creator>yao_feng</dc:creator>
      <dc:date>2024-03-13T08:45:20Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8997 module command timeout issue (interface PCIE+UART, Host: iMX8MQ) - reopen</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1827005#M1590</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/144174"&gt;@yao_feng&lt;/a&gt;&amp;nbsp;,&lt;BR /&gt;&lt;BR /&gt;The bring-up command:&lt;BR /&gt;&lt;BR /&gt;modprobe moal mod_para=nxp/wifi_mod_para.conf drvdbg=0xa0037&lt;BR /&gt;&lt;BR /&gt;There is no WiFi FW hang message because the whole system have been hang by the module 88W8997 with FW Generic_PCIE-WLAN-UART-BT-8997-LNX_6_6_3-IMX8-16.92.21.p119.2-16.92.21.p119.2-MM6X16437.P3-GPL.&lt;/P&gt;&lt;P&gt;Worse than previous version!&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;That's the current final dmesg log record to the log file stored to EMMC.&lt;BR /&gt;&lt;BR /&gt;It's caused every time in 2.4G WiFi connection.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Mar 2024 09:15:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1827005#M1590</guid>
      <dc:creator>ArthurC</dc:creator>
      <dc:date>2024-03-13T09:15:49Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8997 module command timeout issue (interface PCIE+UART, Host: iMX8MQ) - reopen</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1827009#M1591</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186184"&gt;@ArthurC&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;could you please help to try&amp;nbsp;&lt;SPAN&gt;modprobe moal mod_para=nxp/wifi_mod_para.conf&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;without debug level setting, check if it still have system hang issue or not.&lt;/P&gt;&lt;P&gt;and please share&amp;nbsp;&lt;SPAN&gt;wifi_mod_para.conf with us.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thanks.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Mar 2024 09:19:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1827009#M1591</guid>
      <dc:creator>yao_feng</dc:creator>
      <dc:date>2024-03-13T09:19:47Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8997 module command timeout issue (interface PCIE+UART, Host: iMX8MQ) - reopen</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1828042#M1592</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/144174"&gt;@yao_feng&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Without&amp;nbsp;&lt;SPAN&gt;debug level setting, it's on working but the 88W8997 will be caused FW crashing.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Our used wifi_mod_para.conf&amp;nbsp;is as attached.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Mar 2024 05:48:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1828042#M1592</guid>
      <dc:creator>ArthurC</dc:creator>
      <dc:date>2024-03-14T05:48:29Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8997 module command timeout issue (interface PCIE+UART, Host: iMX8MQ) - reopen</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1828135#M1593</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205377"&gt;@Christine_Li&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;drvdbg=0xa0037 seems cause system hang and can't test normally, any suggestion or other settings is ok for FW dump correctly?&lt;/P&gt;&lt;P&gt;The driver parameters settings are below&lt;BR /&gt;Please help to review if its ok?&lt;/P&gt;&lt;P&gt;PCIE8997 = {&lt;BR /&gt;cfg80211_wext=0xf&lt;BR /&gt;max_vir_bss=1&lt;BR /&gt;cal_data_cfg=none&lt;BR /&gt;ps_mode=1&lt;BR /&gt;auto_ds=1&lt;BR /&gt;host_mlme=1&lt;BR /&gt;fw_name=nxp/pcie8997_wlan_v4.bin&lt;BR /&gt;sta_name=wlan&lt;BR /&gt;drv_mode=3&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Thu, 14 Mar 2024 07:10:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1828135#M1593</guid>
      <dc:creator>yao_feng</dc:creator>
      <dc:date>2024-03-14T07:10:15Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8997 module command timeout issue (interface PCIE+UART, Host: iMX8MQ) - reopen</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1829113#M1594</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186184"&gt;@ArthurC&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you please have a try with&amp;nbsp;&lt;SPAN&gt;drvdbg=0x20037?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;At the same time, I will double confirm with our internal team whether Q1-24 release surely include the fix of this issue as promised before.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Christine.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 15 Mar 2024 06:53:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1829113#M1594</guid>
      <dc:creator>Christine_Li</dc:creator>
      <dc:date>2024-03-15T06:53:56Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8997 module command timeout issue (interface PCIE+UART, Host: iMX8MQ) - reopen</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1829123#M1595</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205377"&gt;@Christine_Li&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, I have tried for 10 times.&lt;/P&gt;&lt;P&gt;The FW &lt;SPAN&gt;with&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;drvdbg=0x20037 in 2.4G connection&lt;/SPAN&gt; caused whole system hang everytimes.&lt;/P&gt;</description>
      <pubDate>Fri, 15 Mar 2024 07:03:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1829123#M1595</guid>
      <dc:creator>ArthurC</dc:creator>
      <dc:date>2024-03-15T07:03:34Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8997 module command timeout issue (interface PCIE+UART, Host: iMX8MQ) - reopen</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1829130#M1596</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186184"&gt;@ArthurC&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;So for both&amp;nbsp;&lt;SPAN&gt;drvdbg=0x20037 and&amp;nbsp;drvdbg=0xa0037,&amp;nbsp;&amp;nbsp;in 2.4G connection&amp;nbsp;, will cause whole system hang every time. But without drvdbg parameter, system will not hang but still have FW crash.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Am I right?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Christine.&lt;/P&gt;</description>
      <pubDate>Fri, 15 Mar 2024 07:08:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1829130#M1596</guid>
      <dc:creator>Christine_Li</dc:creator>
      <dc:date>2024-03-15T07:08:29Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8997 module command timeout issue (interface PCIE+UART, Host: iMX8MQ) - reopen</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1829187#M1597</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205377"&gt;@Christine_Li&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, thank you.&lt;/P&gt;</description>
      <pubDate>Fri, 15 Mar 2024 08:18:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1829187#M1597</guid>
      <dc:creator>ArthurC</dc:creator>
      <dc:date>2024-03-15T08:18:20Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8997 module command timeout issue (interface PCIE+UART, Host: iMX8MQ) - reopen</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1829213#M1598</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186184"&gt;@ArthurC&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Could you please help to try&lt;/P&gt;&lt;P&gt;1. Replace FW to combo one:&amp;nbsp;pcieuart8997_combo_v4.bin with drvdbg=0xa0037&lt;BR /&gt;&lt;BR /&gt;2.&amp;nbsp;Set&lt;BR /&gt;&lt;SPAN&gt;ps_mode=2&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;auto_ds=2&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;with drvdbg=0xa0037&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;= = =&lt;BR /&gt;in my experience, drvdbg level will not cause system hang, did you upgrade i.MX8 image or not?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 15 Mar 2024 08:39:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1829213#M1598</guid>
      <dc:creator>yao_feng</dc:creator>
      <dc:date>2024-03-15T08:39:32Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8997 module command timeout issue (interface PCIE+UART, Host: iMX8MQ) - reopen</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1829288#M1599</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/144174"&gt;@yao_feng&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;With&lt;SPAN&gt;&amp;nbsp;pcieuart8997_combo_v4.bin, the default uart speed is 115200. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;It is out of our requirement about audio play via A2DP.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;As we known, if we need Bluetooth uart working in baud 3M.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;There are flows including killing hciattach.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;It's not OK for production.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;So we will not use&amp;nbsp;pcieuart8997_combo_v4.bin.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 15 Mar 2024 09:44:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1829288#M1599</guid>
      <dc:creator>ArthurC</dc:creator>
      <dc:date>2024-03-15T09:44:52Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8997 module command timeout issue (interface PCIE+UART, Host: iMX8MQ) - reopen</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1829319#M1600</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205377"&gt;@Christine_Li&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The FW crashed dmesg log about probe without&lt;SPAN&gt;&amp;nbsp;both&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;drvdbg=0x20037 and&amp;nbsp;drvdbg=0xa0037 is as attached.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 15 Mar 2024 10:20:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1829319#M1600</guid>
      <dc:creator>ArthurC</dc:creator>
      <dc:date>2024-03-15T10:20:42Z</dc:date>
    </item>
    <item>
      <title>Re: 88W8997 module command timeout issue (interface PCIE+UART, Host: iMX8MQ) - reopen</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1830650#M1601</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/186184"&gt;@ArthurC&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your logs and information.&lt;/P&gt;&lt;P&gt;I checked internally about this release, our internal team mentioned they have raised a JIRA ticket and fixes have been merged. So it might be a new issue because of some other submits.&lt;/P&gt;&lt;P&gt;According to the given logs, we will continue to track.&lt;/P&gt;&lt;P&gt;Also about the issue that drvdbg=0x20037 and&amp;nbsp; drvdbg=0xa0037 will cause system hang, I will report internally and may try to reproduce locally.&lt;/P&gt;&lt;P&gt;Once have any feedback, I will sync with you at the first time.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Christine.&lt;/P&gt;</description>
      <pubDate>Tue, 19 Mar 2024 02:54:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/88W8997-module-command-timeout-issue-interface-PCIE-UART-Host/m-p/1830650#M1601</guid>
      <dc:creator>Christine_Li</dc:creator>
      <dc:date>2024-03-19T02:54:36Z</dc:date>
    </item>
  </channel>
</rss>