<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wi-Fi® + Bluetooth® + 802.15.4中的主题 Re: PWM using CTimer</title>
    <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/PWM-using-CTimer/m-p/1831429#M1549</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I just send you a private message, can you please help me checking this.&lt;/P&gt;</description>
    <pubDate>Tue, 19 Mar 2024 20:11:08 GMT</pubDate>
    <dc:creator>nxf77486</dc:creator>
    <dc:date>2024-03-19T20:11:08Z</dc:date>
    <item>
      <title>PWM using CTimer</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/PWM-using-CTimer/m-p/1829233#M1546</link>
      <description>&lt;P&gt;I am trying to generate PWM using CTimer but there isn't any sample code provided by NXP. I am using RW6xx series MCU. Could you help me with this?&lt;/P&gt;</description>
      <pubDate>Fri, 15 Mar 2024 08:54:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/PWM-using-CTimer/m-p/1829233#M1546</guid>
      <dc:creator>hrm2519</dc:creator>
      <dc:date>2024-03-15T08:54:47Z</dc:date>
    </item>
    <item>
      <title>Re: PWM using CTimer</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/PWM-using-CTimer/m-p/1829644#M1547</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Thank you in advance for contacting NXP support.&lt;/P&gt;
&lt;P&gt;As this product has not&amp;nbsp; been yet released t mass market the only information we have available is the one you can find in the product page or SDK release.&lt;/P&gt;
&lt;P&gt;By any chance do you already have a board with you of the RW6xx?&lt;/P&gt;</description>
      <pubDate>Fri, 15 Mar 2024 22:09:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/PWM-using-CTimer/m-p/1829644#M1547</guid>
      <dc:creator>nxf77486</dc:creator>
      <dc:date>2024-03-15T22:09:21Z</dc:date>
    </item>
    <item>
      <title>Re: PWM using CTimer</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/PWM-using-CTimer/m-p/1829969#M1548</link>
      <description>&lt;P&gt;Thank you for the response.&lt;BR /&gt;&lt;BR /&gt;Yes, I do have the RW6xx EVKit with me.&lt;BR /&gt;&lt;BR /&gt;Let me explain the scenario:&lt;/P&gt;&lt;P&gt;1. I flashed the zephyr blinky_pwm sample to the nRF5340 development kit. It works as expected since the logic analyzer output shows frequency being doubled after every 4 seconds.&lt;BR /&gt;&lt;BR /&gt;2. I tried the same sample on NXP RW6xx EVKit. I added an overlay file where I used the SCTimer to generate the PWM. I used channel 9. But this output isn't the same as the Nordic board. After digging into the driver code, I got to know that the driver itself is designed such that it will generate 2 events for every frequency change. Since there are a total of 16 events, this causes the driver to throw an error since the events get used after frequency is changed 8 times. There is a fix in the zephyr repo&amp;nbsp;&lt;A href="https://github.com/zephyrproject-rtos/zephyr/pull/66301" target="_blank"&gt;https://github.com/zephyrproject-rtos/zephyr/pull/66301&lt;/A&gt;&amp;nbsp;but I am not sure why this wasn't included in the NXP release. If I modify the sctimer driver code as per the Zephyr PR, then the behavior is identical to the Nordic board. Due to the above issue, I thought of trying CTimer to generate the PWM.&lt;BR /&gt;&lt;BR /&gt;Any guidance as per the above scenario would be helpful.&lt;/P&gt;</description>
      <pubDate>Mon, 18 Mar 2024 06:06:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/PWM-using-CTimer/m-p/1829969#M1548</guid>
      <dc:creator>hrm2519</dc:creator>
      <dc:date>2024-03-18T06:06:43Z</dc:date>
    </item>
    <item>
      <title>Re: PWM using CTimer</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/PWM-using-CTimer/m-p/1831429#M1549</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I just send you a private message, can you please help me checking this.&lt;/P&gt;</description>
      <pubDate>Tue, 19 Mar 2024 20:11:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/PWM-using-CTimer/m-p/1831429#M1549</guid>
      <dc:creator>nxf77486</dc:creator>
      <dc:date>2024-03-19T20:11:08Z</dc:date>
    </item>
  </channel>
</rss>