<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to set up dual mac 88W9098 in Wi-Fi® + Bluetooth® + 802.15.4</title>
    <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/How-to-set-up-dual-mac-88W9098/m-p/1805057#M1528</link>
    <description>&lt;P&gt;This is the log when installing the driver.&lt;/P&gt;&lt;PRE&gt;root@colibri-imx6ull-06984422:~# cat /etc/modprobe.d/jody-w3-module.conf&lt;BR /&gt;blacklist btmrvl_sdio&lt;BR /&gt;blacklist btmrvl&lt;BR /&gt;blacklist bluetooth&lt;BR /&gt;blacklist mwifiex_sdio&lt;BR /&gt;blacklist mwifiex&lt;BR /&gt;&lt;BR /&gt;alias sdio:c*v02DFd9149* jody-w3-sdio&lt;BR /&gt;options jody-w3-sdio fw_name=nxp/sdiouart9098_combo_v1.bin&lt;BR /&gt;options jody-w3-sdio cal_data_cfg=none&lt;BR /&gt;options jody-w3-sdio cfg80211_wext=0xf&lt;BR /&gt;options jody-w3-sdio drv_mode=3&lt;BR /&gt;options jody-w3-sdio drvdbg=7&lt;BR /&gt;install mlan_jody-w3-sdio :&lt;BR /&gt;install jody-w3-sdio \&lt;BR /&gt;/sbin/modprobe -i mlan; \&lt;BR /&gt;/sbin/modprobe -i moal $CMDLINE_OPTS&lt;BR /&gt;remove jody-w3-sdio \&lt;BR /&gt;/sbin/rmmod sd8xxx mlan&lt;BR /&gt;&lt;BR /&gt;root@colibri-imx6ull-06984422:~# modprobe jody-w3-sdio&lt;BR /&gt;[ 52.666772] mlan: loading out-of-tree module taints kernel.&lt;BR /&gt;[ 52.841735] wlan: Loading MWLAN driver&lt;BR /&gt;[ 52.846234] wlan: Register to Bus Driver...&lt;BR /&gt;[ 52.856548] vendor=0x02DF device=0x914D class=0 function=1&lt;BR /&gt;[ 52.862431] Attach moal handle ops, card interface type: 0x106&lt;BR /&gt;[ 52.869606] rps set to 0 from module param&lt;BR /&gt;[ 52.873867] No module param cfg file specified&lt;BR /&gt;[ 52.879670] SDIO: max_segs=128 max_seg_size=65535&lt;BR /&gt;[ 52.884673] rx_work=0 cpu_num=1&lt;BR /&gt;[ 52.888892] Attach mlan adapter operations.card_type is 0x106.&lt;BR /&gt;[ 52.896497] wlan: Enable TX SG mode&lt;BR /&gt;[ 52.900145] wlan: Enable RX SG mode&lt;BR /&gt;[ 52.914334] Request firmware: nxp/sdiouart9098_combo_v1.bin&lt;BR /&gt;[ 53.510047] Wlan: FW download over, firmwarelen=845044 downloaded 685820&lt;BR /&gt;[ 53.757884] WLAN FW is active&lt;BR /&gt;[ 53.761297] on_time is 53757319297&lt;BR /&gt;[ 53.776425] VDLL image: len=159224&lt;BR /&gt;[ 53.783413] fw_cap_info=0xc8fcffa3, dev_cap_mask=0xffffffff&lt;BR /&gt;[ 53.789406] max_p2p_conn = 8, max_sta_conn = 64&lt;BR /&gt;[ 53.911180] Register NXP 802.11 Adapter mlan0&lt;BR /&gt;[ 53.939689] wlan: uap%d set max_mtu 2000&lt;BR /&gt;[ 53.999044] Register NXP 802.11 Adapter uap0&lt;BR /&gt;[ 54.005107] wlan: version = SD9098----17.92.1.p116.1-MM5X17391.p3-GPL-(FP92)&lt;BR /&gt;[ 54.087482] vendor=0x02DF device=0x914E class=0 function=2&lt;BR /&gt;[ 54.156332] Attach moal handle ops, card interface type: 0x106&lt;BR /&gt;[ 54.203269] rps set to 0 from module param&lt;BR /&gt;[ 54.210296] No module param cfg file specified&lt;BR /&gt;[ 54.254256] SDIO: max_segs=128 max_seg_size=65535&lt;BR /&gt;[ 54.261724] rx_work=0 cpu_num=1&lt;BR /&gt;[ 54.294364] Attach mlan adapter operations.card_type is 0x106.&lt;BR /&gt;[ 54.319658] wlan: Enable TX SG mode&lt;BR /&gt;[ 54.325989] wlan: Enable RX SG mode&lt;BR /&gt;[ 54.374404] Request firmware: nxp/sdiouart9098_combo_v1.bin&lt;BR /&gt;[ 54.407259] WLAN FW already running! Skip FW download&lt;BR /&gt;[ 54.516243] WLAN FW is active&lt;BR /&gt;[ 54.521823] on_time is 54517847464&lt;BR /&gt;[ 54.667756] VDLL image: len=159224&lt;BR /&gt;[ 54.742841] fw_cap_info=0x68fcffa3, dev_cap_mask=0xffffffff&lt;BR /&gt;[ 54.751169] max_p2p_conn = 8, max_sta_conn = 64&lt;BR /&gt;[ 54.926357] Register NXP 802.11 Adapter mmlan0&lt;BR /&gt;[ 54.935121] wlan: muap%d set max_mtu 2000&lt;BR /&gt;[ 55.025671] Register NXP 802.11 Adapter muap0&lt;BR /&gt;[ 55.032804] wlan: version = SD9098----17.92.1.p116.1-MM5X17391.p3-GPL-(FP92)&lt;BR /&gt;[ 55.185587] wlan: Register to Bus Driver Done&lt;BR /&gt;[ 55.192553] wlan: Driver loaded successfully&lt;BR /&gt;root@colibri-imx6ull-06984422:~# [ 55.891740] muap0: Skip change virtual intf type on uap: from 3 to 2&lt;BR /&gt;[ 56.712079] wlan: mlan0 START SCAN&lt;BR /&gt;[ 56.802376] wlan: mmlan0 START SCAN&lt;BR /&gt;&lt;BR /&gt;root@colibri-imx6ull-06984422:~# ifconfig&lt;BR /&gt;eth0 Link encap:Ethernet HWaddr 00:14:2D:6A:92:E6&lt;BR /&gt;UP BROADCAST MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)&lt;BR /&gt;&lt;BR /&gt;lo Link encap:Local Loopback&lt;BR /&gt;inet addr:127.0.0.1 Mask:255.0.0.0&lt;BR /&gt;inet6 addr: ::1/128 Scope:Host&lt;BR /&gt;UP LOOPBACK RUNNING MTU:65536 Metric:1&lt;BR /&gt;RX packets:169 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:169 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:12584 (12.2 KiB) TX bytes:12584 (12.2 KiB)&lt;BR /&gt;&lt;BR /&gt;mlan0 Link encap:Ethernet HWaddr 5E:0C:5F:53:C7:87&lt;BR /&gt;UP BROADCAST MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)&lt;BR /&gt;&lt;BR /&gt;mmlan0 Link encap:Ethernet HWaddr 1A:5F:A0:49:0B:8A&lt;BR /&gt;UP BROADCAST MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)&lt;BR /&gt;&lt;BR /&gt;muap0 Link encap:Ethernet HWaddr A6:89:B1:4C:7E:57&lt;BR /&gt;UP BROADCAST MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)&lt;BR /&gt;&lt;BR /&gt;uap0 Link encap:Ethernet HWaddr 62:09:C3:81:F7:0D&lt;BR /&gt;UP BROADCAST MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)&lt;BR /&gt;&lt;BR /&gt;usb0 Link encap:Ethernet HWaddr AA:25:17:F6:9D:9E&lt;BR /&gt;UP BROADCAST MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is the error log when trying to disable mmlan0 (change second MAC/PHY to uAP mode).&lt;/P&gt;&lt;PRE&gt;root@colibri-imx6ull-06984422:~# echo drv_mode=2 &amp;gt; /proc/mwlan/adapter1/config&lt;BR /&gt;[ 279.284811] woal_close: woal_disconnect failed&lt;BR /&gt;[ 279.297436] 8&amp;lt;--- cut here ---&lt;BR /&gt;[ 279.302843] Unable to handle kernel paging request at virtual address 00002d24&lt;BR /&gt;[ 279.314972] [00002d24] *pgd=00000000&lt;BR /&gt;[ 279.320939] Internal error: Oops: 5 [#1] SMP ARM&lt;BR /&gt;[ 279.327925] Modules linked in: l2tp_ppp pppox moal(O) mlan(O) mcp251x imx_sdma fuse&lt;BR /&gt;[ 279.340512] CPU: 0 PID: 225 Comm: kworker/0:5 Tainted: G O 6.1.22-6.2.0-devel+git.3b29299e5f60 #1&lt;BR /&gt;[ 279.355924] Hardware name: Freescale i.MX6 Ultralite (Device Tree)&lt;BR /&gt;[ 279.364763] Workqueue: events sdio_irq_work&lt;BR /&gt;[ 279.371623] PC is at mlan_interrupt+0x4/0xc [mlan]&lt;BR /&gt;[ 279.379439] LR is at woal_sdio_interrupt+0x50/0xa8 [moal]&lt;BR /&gt;[ 279.388093] pc : [&amp;lt;bf03265c&amp;gt;] lr : [&amp;lt;bf14ea70&amp;gt;] psr: 400f0113&lt;BR /&gt;[ 279.397058] sp : e0e2dee0 ip : 2c000000 fp : 00000000&lt;BR /&gt;[ 279.404974] r10: c1004bbc r9 : c1004b8c r8 : c2584bc4&lt;BR /&gt;[ 279.412884] r7 : c2569a40 r6 : bf174b2c r5 : c3581000 r4 : c3580000&lt;BR /&gt;[ 279.422129] r3 : 00002000 r2 : 00000001 r1 : 00000000 r0 : 00000000&lt;BR /&gt;[ 279.431368] Flags: nZcv IRQs on FIQs on Mode SVC_32 ISA ARM Segment none&lt;BR /&gt;[ 279.441334] Control: 10c5387d Table: 835b806a DAC: 00000051&lt;BR /&gt;[ 279.449919] Register r0 information: NULL pointer&lt;BR /&gt;[ 279.457467] Register r1 information: NULL pointer&lt;BR /&gt;[ 279.464944] Register r2 information: non-paged memory&lt;BR /&gt;[ 279.472743] Register r3 information: non-paged memory&lt;BR /&gt;[ 279.480537] Register r4 information: non-slab/vmalloc memory&lt;BR /&gt;[ 279.488924] Register r5 information: non-slab/vmalloc memory&lt;BR /&gt;[ 279.497245] Register r6 information: 199-page vmalloc region starting at 0xbf0c8000 allocated at load_module+0x9b0/0x1e48&lt;BR /&gt;[ 279.513573] Register r7 information: slab task_struct start c2569a40 pointer offset 0&lt;BR /&gt;[ 279.526941] Register r8 information: slab kmalloc-2k start c2584800 pointer offset 964 size 2048&lt;BR /&gt;[ 279.541371] Register r9 information: non-slab/vmalloc memory&lt;BR /&gt;[ 279.549921] Register r10 information: non-slab/vmalloc memory&lt;BR /&gt;[ 279.558560] Register r11 information: NULL pointer&lt;BR /&gt;[ 279.566158] Register r12 information: non-paged memory&lt;BR /&gt;[ 279.574018] Process kworker/0:5 (pid: 225, stack limit = 0x99df7eb9)&lt;BR /&gt;[ 279.583119] Stack: (0xe0e2dee0 to 0xe0e2e000)&lt;BR /&gt;[ 279.590180] dee0: 00000002 00000000 c2584800 c08a0478 00000000 e0e2defa 00040122 03410e75&lt;BR /&gt;[ 279.603757] df00: e0e2df54 c24fd2ec c24fd000 d3b769c0 d3b79c00 00000000 c2569a40 d3b79c05&lt;BR /&gt;[ 279.617544] df20: 00000000 c08a074c c24fd2ec c2b41980 d3b769c0 c013e388 d3b769c0 d3b769c0&lt;BR /&gt;[ 279.631492] df40: d3b769dc c2b41980 d3b769c0 c2b41998 d3b769dc c1203d40 00000008 c2569a40&lt;BR /&gt;[ 279.645658] df60: d3b769c0 c013e5d4 00000000 c288b9c0 c2569a40 c013e598 c2b41980 c288b140&lt;BR /&gt;[ 279.660013] df80: e0939ebc 00000000 00000000 c014645c c288b9c0 c0146394 00000000 00000000&lt;BR /&gt;[ 279.674460] dfa0: 00000000 00000000 00000000 c0100168 00000000 00000000 00000000 00000000&lt;BR /&gt;[ 279.689284] dfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000&lt;BR /&gt;[ 279.704530] dfe0: 00000000 00000000 00000000 00000000 00000013 00000000 00000000 00000000&lt;BR /&gt;[ 279.720184] mlan_interrupt [mlan] from woal_sdio_interrupt+0x50/0xa8 [moal]&lt;BR /&gt;[ 279.732010] woal_sdio_interrupt [moal] from process_sdio_pending_irqs+0xf8/0x1f4&lt;BR /&gt;[ 279.747491] process_sdio_pending_irqs from sdio_irq_work+0x3c/0x64&lt;BR /&gt;[ 279.757585] sdio_irq_work from process_one_work+0x1dc/0x3ec&lt;BR /&gt;[ 279.767021] process_one_work from worker_thread+0x3c/0x538&lt;BR /&gt;[ 279.776340] worker_thread from kthread+0xc8/0xe8&lt;BR /&gt;[ 279.784789] kthread from ret_from_fork+0x14/0x2c&lt;BR /&gt;[ 279.793240] Exception stack(0xe0e2dfb0 to 0xe0e2dff8)&lt;BR /&gt;[ 279.802064] dfa0: 00000000 00000000 00000000 00000000&lt;BR /&gt;[ 279.817741] dfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000&lt;BR /&gt;[ 279.833420] dfe0: 00000000 00000000 00000000 00000000 00000013 00000000&lt;BR /&gt;[ 279.843842] Code: bf0a6bd4 0000012e bf0a6bf0 e2813a02 (e5933d24)&lt;BR /&gt;[ 279.853873] ---[ end trace 0000000000000000 ]---&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.320939] Internal error: Oops: 5 [#1] SMP ARM&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.574018] Process kworker/0:5 (pid: 225, stack limit = 0x99df7eb9)&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.583119] Stack: (0xe0e2dee0 to 0xe0e2e000)&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.590180] dee0: 00000002 00000000 c2584800 c08a0478 00000000 e0e2defa 00040122 03410e75&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.603757] df00: e0e2df54 c24fd2ec c24fd000 d3b769c0 d3b79c00 00000000 c2569a40 d3b79c05&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.617544] df20: 00000000 c08a074c c24fd2ec c2b41980 d3b769c0 c013e388 d3b769c0 d3b769c0&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.631492] df40: d3b769dc c2b41980 d3b769c0 c2b41998 d3b769dc c1203d40 00000008 c2569a40&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.645658] df60: d3b769c0 c013e5d4 00000000 c288b9c0 c2569a40 c013e598 c2b41980 c288b140&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.660013] df80: e0939ebc 00000000 00000000 c014645c c288b9c0 c0146394 00000000 00000000&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.674460] dfa0: 00000000 00000000 00000000 c0100168 00000000 00000000 00000000 00000000&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.689284] dfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.704530] dfe0: 00000000 00000000 00000000 00000000 00000013 00000000 00000000 00000000&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.720184] mlan_interrupt [mlan] from woal_sdio_interrupt+0x50/0xa8 [moal]&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.732010] woal_sdio_interrupt [moal] from process_sdio_pending_irqs+0xf8/0x1f4&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.747491] process_sdio_pending_irqs from sdio_irq_work+0x3c/0x64&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.757585] sdio_irq_work from process_one_work+0x1dc/0x3ec&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.767021] process_one_work from worker_thread+0x3c/0x538&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.776340] worker_thread from kthread+0xc8/0xe8&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.784789] kthread from ret_from_fork+0x14/0x2c&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.793240] Exception stack(0xe0e2dfb0 to 0xe0e2dff8)&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.802064] dfa0: 00000000 00000000 00000000 00000000&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.817741] dfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.833420] dfe0: 00000000 00000000 00000000 00000000 00000013 00000000&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.843842] Code: bf0a6bd4 0000012e bf0a6bf0 e2813a02 (e5933d24)&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 12 Feb 2024 01:15:05 GMT</pubDate>
    <dc:creator>masakiyo</dc:creator>
    <dc:date>2024-02-12T01:15:05Z</dc:date>
    <item>
      <title>How to set up dual mac 88W9098</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/How-to-set-up-dual-mac-88W9098/m-p/1805040#M1527</link>
      <description>&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;We are evaluating 88W9098.&lt;/P&gt;&lt;P&gt;Now, the following four interfaces are visible on the dual-mac 88W9098.&lt;/P&gt;&lt;PRE&gt;mlan0 Link encap:Ethernet HWaddr 60:09:C3:81:F6:0D&lt;BR /&gt;UP BROADCAST MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)&lt;BR /&gt;&lt;BR /&gt;mmlan0 Link encap:Ethernet HWaddr 60:09:C3:81:F6:0E&lt;BR /&gt;UP BROADCAST MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)&lt;BR /&gt;&lt;BR /&gt;muap0 Link encap:Ethernet HWaddr 62:09:C3:81:F7:0E&lt;BR /&gt;UP BROADCAST MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)&lt;BR /&gt;&lt;BR /&gt;uap0 Link encap:Ethernet HWaddr 62:09:C3:81:F7:0D&lt;BR /&gt;UP BROADCAST MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The mlan0 and uap0 are first MAC/PHY, and the mmlan0 and muap0 are the second MAC/PHY.&lt;/P&gt;&lt;P&gt;We want to use the first MAC/PHY with mlan0 only and the second MAC/PHY with muap0 only.&lt;/P&gt;&lt;P&gt;Is this possible? And please tell me the driver settings for that.&lt;/P&gt;</description>
      <pubDate>Sun, 11 Feb 2024 15:33:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/How-to-set-up-dual-mac-88W9098/m-p/1805040#M1527</guid>
      <dc:creator>masakiyo</dc:creator>
      <dc:date>2024-02-11T15:33:37Z</dc:date>
    </item>
    <item>
      <title>Re: How to set up dual mac 88W9098</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/How-to-set-up-dual-mac-88W9098/m-p/1805057#M1528</link>
      <description>&lt;P&gt;This is the log when installing the driver.&lt;/P&gt;&lt;PRE&gt;root@colibri-imx6ull-06984422:~# cat /etc/modprobe.d/jody-w3-module.conf&lt;BR /&gt;blacklist btmrvl_sdio&lt;BR /&gt;blacklist btmrvl&lt;BR /&gt;blacklist bluetooth&lt;BR /&gt;blacklist mwifiex_sdio&lt;BR /&gt;blacklist mwifiex&lt;BR /&gt;&lt;BR /&gt;alias sdio:c*v02DFd9149* jody-w3-sdio&lt;BR /&gt;options jody-w3-sdio fw_name=nxp/sdiouart9098_combo_v1.bin&lt;BR /&gt;options jody-w3-sdio cal_data_cfg=none&lt;BR /&gt;options jody-w3-sdio cfg80211_wext=0xf&lt;BR /&gt;options jody-w3-sdio drv_mode=3&lt;BR /&gt;options jody-w3-sdio drvdbg=7&lt;BR /&gt;install mlan_jody-w3-sdio :&lt;BR /&gt;install jody-w3-sdio \&lt;BR /&gt;/sbin/modprobe -i mlan; \&lt;BR /&gt;/sbin/modprobe -i moal $CMDLINE_OPTS&lt;BR /&gt;remove jody-w3-sdio \&lt;BR /&gt;/sbin/rmmod sd8xxx mlan&lt;BR /&gt;&lt;BR /&gt;root@colibri-imx6ull-06984422:~# modprobe jody-w3-sdio&lt;BR /&gt;[ 52.666772] mlan: loading out-of-tree module taints kernel.&lt;BR /&gt;[ 52.841735] wlan: Loading MWLAN driver&lt;BR /&gt;[ 52.846234] wlan: Register to Bus Driver...&lt;BR /&gt;[ 52.856548] vendor=0x02DF device=0x914D class=0 function=1&lt;BR /&gt;[ 52.862431] Attach moal handle ops, card interface type: 0x106&lt;BR /&gt;[ 52.869606] rps set to 0 from module param&lt;BR /&gt;[ 52.873867] No module param cfg file specified&lt;BR /&gt;[ 52.879670] SDIO: max_segs=128 max_seg_size=65535&lt;BR /&gt;[ 52.884673] rx_work=0 cpu_num=1&lt;BR /&gt;[ 52.888892] Attach mlan adapter operations.card_type is 0x106.&lt;BR /&gt;[ 52.896497] wlan: Enable TX SG mode&lt;BR /&gt;[ 52.900145] wlan: Enable RX SG mode&lt;BR /&gt;[ 52.914334] Request firmware: nxp/sdiouart9098_combo_v1.bin&lt;BR /&gt;[ 53.510047] Wlan: FW download over, firmwarelen=845044 downloaded 685820&lt;BR /&gt;[ 53.757884] WLAN FW is active&lt;BR /&gt;[ 53.761297] on_time is 53757319297&lt;BR /&gt;[ 53.776425] VDLL image: len=159224&lt;BR /&gt;[ 53.783413] fw_cap_info=0xc8fcffa3, dev_cap_mask=0xffffffff&lt;BR /&gt;[ 53.789406] max_p2p_conn = 8, max_sta_conn = 64&lt;BR /&gt;[ 53.911180] Register NXP 802.11 Adapter mlan0&lt;BR /&gt;[ 53.939689] wlan: uap%d set max_mtu 2000&lt;BR /&gt;[ 53.999044] Register NXP 802.11 Adapter uap0&lt;BR /&gt;[ 54.005107] wlan: version = SD9098----17.92.1.p116.1-MM5X17391.p3-GPL-(FP92)&lt;BR /&gt;[ 54.087482] vendor=0x02DF device=0x914E class=0 function=2&lt;BR /&gt;[ 54.156332] Attach moal handle ops, card interface type: 0x106&lt;BR /&gt;[ 54.203269] rps set to 0 from module param&lt;BR /&gt;[ 54.210296] No module param cfg file specified&lt;BR /&gt;[ 54.254256] SDIO: max_segs=128 max_seg_size=65535&lt;BR /&gt;[ 54.261724] rx_work=0 cpu_num=1&lt;BR /&gt;[ 54.294364] Attach mlan adapter operations.card_type is 0x106.&lt;BR /&gt;[ 54.319658] wlan: Enable TX SG mode&lt;BR /&gt;[ 54.325989] wlan: Enable RX SG mode&lt;BR /&gt;[ 54.374404] Request firmware: nxp/sdiouart9098_combo_v1.bin&lt;BR /&gt;[ 54.407259] WLAN FW already running! Skip FW download&lt;BR /&gt;[ 54.516243] WLAN FW is active&lt;BR /&gt;[ 54.521823] on_time is 54517847464&lt;BR /&gt;[ 54.667756] VDLL image: len=159224&lt;BR /&gt;[ 54.742841] fw_cap_info=0x68fcffa3, dev_cap_mask=0xffffffff&lt;BR /&gt;[ 54.751169] max_p2p_conn = 8, max_sta_conn = 64&lt;BR /&gt;[ 54.926357] Register NXP 802.11 Adapter mmlan0&lt;BR /&gt;[ 54.935121] wlan: muap%d set max_mtu 2000&lt;BR /&gt;[ 55.025671] Register NXP 802.11 Adapter muap0&lt;BR /&gt;[ 55.032804] wlan: version = SD9098----17.92.1.p116.1-MM5X17391.p3-GPL-(FP92)&lt;BR /&gt;[ 55.185587] wlan: Register to Bus Driver Done&lt;BR /&gt;[ 55.192553] wlan: Driver loaded successfully&lt;BR /&gt;root@colibri-imx6ull-06984422:~# [ 55.891740] muap0: Skip change virtual intf type on uap: from 3 to 2&lt;BR /&gt;[ 56.712079] wlan: mlan0 START SCAN&lt;BR /&gt;[ 56.802376] wlan: mmlan0 START SCAN&lt;BR /&gt;&lt;BR /&gt;root@colibri-imx6ull-06984422:~# ifconfig&lt;BR /&gt;eth0 Link encap:Ethernet HWaddr 00:14:2D:6A:92:E6&lt;BR /&gt;UP BROADCAST MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)&lt;BR /&gt;&lt;BR /&gt;lo Link encap:Local Loopback&lt;BR /&gt;inet addr:127.0.0.1 Mask:255.0.0.0&lt;BR /&gt;inet6 addr: ::1/128 Scope:Host&lt;BR /&gt;UP LOOPBACK RUNNING MTU:65536 Metric:1&lt;BR /&gt;RX packets:169 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:169 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:12584 (12.2 KiB) TX bytes:12584 (12.2 KiB)&lt;BR /&gt;&lt;BR /&gt;mlan0 Link encap:Ethernet HWaddr 5E:0C:5F:53:C7:87&lt;BR /&gt;UP BROADCAST MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)&lt;BR /&gt;&lt;BR /&gt;mmlan0 Link encap:Ethernet HWaddr 1A:5F:A0:49:0B:8A&lt;BR /&gt;UP BROADCAST MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)&lt;BR /&gt;&lt;BR /&gt;muap0 Link encap:Ethernet HWaddr A6:89:B1:4C:7E:57&lt;BR /&gt;UP BROADCAST MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)&lt;BR /&gt;&lt;BR /&gt;uap0 Link encap:Ethernet HWaddr 62:09:C3:81:F7:0D&lt;BR /&gt;UP BROADCAST MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)&lt;BR /&gt;&lt;BR /&gt;usb0 Link encap:Ethernet HWaddr AA:25:17:F6:9D:9E&lt;BR /&gt;UP BROADCAST MULTICAST MTU:1500 Metric:1&lt;BR /&gt;RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;collisions:0 txqueuelen:1000&lt;BR /&gt;RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is the error log when trying to disable mmlan0 (change second MAC/PHY to uAP mode).&lt;/P&gt;&lt;PRE&gt;root@colibri-imx6ull-06984422:~# echo drv_mode=2 &amp;gt; /proc/mwlan/adapter1/config&lt;BR /&gt;[ 279.284811] woal_close: woal_disconnect failed&lt;BR /&gt;[ 279.297436] 8&amp;lt;--- cut here ---&lt;BR /&gt;[ 279.302843] Unable to handle kernel paging request at virtual address 00002d24&lt;BR /&gt;[ 279.314972] [00002d24] *pgd=00000000&lt;BR /&gt;[ 279.320939] Internal error: Oops: 5 [#1] SMP ARM&lt;BR /&gt;[ 279.327925] Modules linked in: l2tp_ppp pppox moal(O) mlan(O) mcp251x imx_sdma fuse&lt;BR /&gt;[ 279.340512] CPU: 0 PID: 225 Comm: kworker/0:5 Tainted: G O 6.1.22-6.2.0-devel+git.3b29299e5f60 #1&lt;BR /&gt;[ 279.355924] Hardware name: Freescale i.MX6 Ultralite (Device Tree)&lt;BR /&gt;[ 279.364763] Workqueue: events sdio_irq_work&lt;BR /&gt;[ 279.371623] PC is at mlan_interrupt+0x4/0xc [mlan]&lt;BR /&gt;[ 279.379439] LR is at woal_sdio_interrupt+0x50/0xa8 [moal]&lt;BR /&gt;[ 279.388093] pc : [&amp;lt;bf03265c&amp;gt;] lr : [&amp;lt;bf14ea70&amp;gt;] psr: 400f0113&lt;BR /&gt;[ 279.397058] sp : e0e2dee0 ip : 2c000000 fp : 00000000&lt;BR /&gt;[ 279.404974] r10: c1004bbc r9 : c1004b8c r8 : c2584bc4&lt;BR /&gt;[ 279.412884] r7 : c2569a40 r6 : bf174b2c r5 : c3581000 r4 : c3580000&lt;BR /&gt;[ 279.422129] r3 : 00002000 r2 : 00000001 r1 : 00000000 r0 : 00000000&lt;BR /&gt;[ 279.431368] Flags: nZcv IRQs on FIQs on Mode SVC_32 ISA ARM Segment none&lt;BR /&gt;[ 279.441334] Control: 10c5387d Table: 835b806a DAC: 00000051&lt;BR /&gt;[ 279.449919] Register r0 information: NULL pointer&lt;BR /&gt;[ 279.457467] Register r1 information: NULL pointer&lt;BR /&gt;[ 279.464944] Register r2 information: non-paged memory&lt;BR /&gt;[ 279.472743] Register r3 information: non-paged memory&lt;BR /&gt;[ 279.480537] Register r4 information: non-slab/vmalloc memory&lt;BR /&gt;[ 279.488924] Register r5 information: non-slab/vmalloc memory&lt;BR /&gt;[ 279.497245] Register r6 information: 199-page vmalloc region starting at 0xbf0c8000 allocated at load_module+0x9b0/0x1e48&lt;BR /&gt;[ 279.513573] Register r7 information: slab task_struct start c2569a40 pointer offset 0&lt;BR /&gt;[ 279.526941] Register r8 information: slab kmalloc-2k start c2584800 pointer offset 964 size 2048&lt;BR /&gt;[ 279.541371] Register r9 information: non-slab/vmalloc memory&lt;BR /&gt;[ 279.549921] Register r10 information: non-slab/vmalloc memory&lt;BR /&gt;[ 279.558560] Register r11 information: NULL pointer&lt;BR /&gt;[ 279.566158] Register r12 information: non-paged memory&lt;BR /&gt;[ 279.574018] Process kworker/0:5 (pid: 225, stack limit = 0x99df7eb9)&lt;BR /&gt;[ 279.583119] Stack: (0xe0e2dee0 to 0xe0e2e000)&lt;BR /&gt;[ 279.590180] dee0: 00000002 00000000 c2584800 c08a0478 00000000 e0e2defa 00040122 03410e75&lt;BR /&gt;[ 279.603757] df00: e0e2df54 c24fd2ec c24fd000 d3b769c0 d3b79c00 00000000 c2569a40 d3b79c05&lt;BR /&gt;[ 279.617544] df20: 00000000 c08a074c c24fd2ec c2b41980 d3b769c0 c013e388 d3b769c0 d3b769c0&lt;BR /&gt;[ 279.631492] df40: d3b769dc c2b41980 d3b769c0 c2b41998 d3b769dc c1203d40 00000008 c2569a40&lt;BR /&gt;[ 279.645658] df60: d3b769c0 c013e5d4 00000000 c288b9c0 c2569a40 c013e598 c2b41980 c288b140&lt;BR /&gt;[ 279.660013] df80: e0939ebc 00000000 00000000 c014645c c288b9c0 c0146394 00000000 00000000&lt;BR /&gt;[ 279.674460] dfa0: 00000000 00000000 00000000 c0100168 00000000 00000000 00000000 00000000&lt;BR /&gt;[ 279.689284] dfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000&lt;BR /&gt;[ 279.704530] dfe0: 00000000 00000000 00000000 00000000 00000013 00000000 00000000 00000000&lt;BR /&gt;[ 279.720184] mlan_interrupt [mlan] from woal_sdio_interrupt+0x50/0xa8 [moal]&lt;BR /&gt;[ 279.732010] woal_sdio_interrupt [moal] from process_sdio_pending_irqs+0xf8/0x1f4&lt;BR /&gt;[ 279.747491] process_sdio_pending_irqs from sdio_irq_work+0x3c/0x64&lt;BR /&gt;[ 279.757585] sdio_irq_work from process_one_work+0x1dc/0x3ec&lt;BR /&gt;[ 279.767021] process_one_work from worker_thread+0x3c/0x538&lt;BR /&gt;[ 279.776340] worker_thread from kthread+0xc8/0xe8&lt;BR /&gt;[ 279.784789] kthread from ret_from_fork+0x14/0x2c&lt;BR /&gt;[ 279.793240] Exception stack(0xe0e2dfb0 to 0xe0e2dff8)&lt;BR /&gt;[ 279.802064] dfa0: 00000000 00000000 00000000 00000000&lt;BR /&gt;[ 279.817741] dfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000&lt;BR /&gt;[ 279.833420] dfe0: 00000000 00000000 00000000 00000000 00000013 00000000&lt;BR /&gt;[ 279.843842] Code: bf0a6bd4 0000012e bf0a6bf0 e2813a02 (e5933d24)&lt;BR /&gt;[ 279.853873] ---[ end trace 0000000000000000 ]---&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.320939] Internal error: Oops: 5 [#1] SMP ARM&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.574018] Process kworker/0:5 (pid: 225, stack limit = 0x99df7eb9)&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.583119] Stack: (0xe0e2dee0 to 0xe0e2e000)&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.590180] dee0: 00000002 00000000 c2584800 c08a0478 00000000 e0e2defa 00040122 03410e75&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.603757] df00: e0e2df54 c24fd2ec c24fd000 d3b769c0 d3b79c00 00000000 c2569a40 d3b79c05&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.617544] df20: 00000000 c08a074c c24fd2ec c2b41980 d3b769c0 c013e388 d3b769c0 d3b769c0&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.631492] df40: d3b769dc c2b41980 d3b769c0 c2b41998 d3b769dc c1203d40 00000008 c2569a40&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.645658] df60: d3b769c0 c013e5d4 00000000 c288b9c0 c2569a40 c013e598 c2b41980 c288b140&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.660013] df80: e0939ebc 00000000 00000000 c014645c c288b9c0 c0146394 00000000 00000000&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.674460] dfa0: 00000000 00000000 00000000 c0100168 00000000 00000000 00000000 00000000&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.689284] dfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.704530] dfe0: 00000000 00000000 00000000 00000000 00000013 00000000 00000000 00000000&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.720184] mlan_interrupt [mlan] from woal_sdio_interrupt+0x50/0xa8 [moal]&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.732010] woal_sdio_interrupt [moal] from process_sdio_pending_irqs+0xf8/0x1f4&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.747491] process_sdio_pending_irqs from sdio_irq_work+0x3c/0x64&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.757585] sdio_irq_work from process_one_work+0x1dc/0x3ec&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.767021] process_one_work from worker_thread+0x3c/0x538&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.776340] worker_thread from kthread+0xc8/0xe8&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.784789] kthread from ret_from_fork+0x14/0x2c&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.793240] Exception stack(0xe0e2dfb0 to 0xe0e2dff8)&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.802064] dfa0: 00000000 00000000 00000000 00000000&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.817741] dfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.833420] dfe0: 00000000 00000000 00000000 00000000 00000013 00000000&lt;BR /&gt;&lt;BR /&gt;Message from syslogd@colibri-imx6ull-06984422 at Feb 12 10:13:18 ...&lt;BR /&gt;kernel:[ 279.843842] Code: bf0a6bd4 0000012e bf0a6bf0 e2813a02 (e5933d24)&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 12 Feb 2024 01:15:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/How-to-set-up-dual-mac-88W9098/m-p/1805057#M1528</guid>
      <dc:creator>masakiyo</dc:creator>
      <dc:date>2024-02-12T01:15:05Z</dc:date>
    </item>
    <item>
      <title>Re: How to set up dual mac 88W9098</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/How-to-set-up-dual-mac-88W9098/m-p/1805359#M1529</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I am checking internally. I will let you know.&lt;/P&gt;
&lt;P&gt;In the meantime, did you check User Manual&amp;nbsp;&lt;SPAN class="meta-item"&gt;UM11583&lt;/SPAN&gt; &lt;A id="relatedDocsClickPDF_4" class="dtmcustomrulelink" href="https://www.nxp.com/webapp/Download?colCode=UM11583&amp;amp;appType=license" target="_blank" rel="noopener" data-dtmaction="Documentation Section - Results Link Click" data-dtmsubaction="Getting Started with 88W9098/88Q9098 Evaluation Board – User manual (confidential) - Secure Files - User Manual - English"&gt;&lt;SPAN&gt;Getting Started with 88W9098/88Q9098 Evaluation Board – User manual&lt;/SPAN&gt;&lt;/A&gt; you will find on product page &lt;A href="https://www.nxp.com/products/wireless-connectivity/wi-fi-plus-bluetooth-plus-802-15-4/2-4-5-ghz-dual-band-2x2-wi-fi-6-802-11ax-plus-bluetooth-5-3:88W9098#documentation" target="_blank"&gt;https://www.nxp.com/products/wireless-connectivity/wi-fi-plus-bluetooth-plus-802-15-4/2-4-5-ghz-dual-band-2x2-wi-fi-6-802-11ax-plus-bluetooth-5-3:88W9098#documentation&lt;/A&gt; (see chapter "7 Wi-Fi bring-up and testing") ?&lt;/P&gt;
&lt;P&gt;Aren't the following commands matching your needs :&lt;BR /&gt;"ifconfig &lt;SPAN class="test-id__field-value slds-form-element__static slds-grow word-break-ie11"&gt;uap0&lt;/SPAN&gt; down"&lt;BR /&gt;"ifconfig mmlan&lt;SPAN class="test-id__field-value slds-form-element__static slds-grow word-break-ie11"&gt;0&lt;/SPAN&gt; down"&lt;BR /&gt;?&lt;/P&gt;</description>
      <pubDate>Mon, 12 Feb 2024 16:41:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/How-to-set-up-dual-mac-88W9098/m-p/1805359#M1529</guid>
      <dc:creator>cdoumenc</dc:creator>
      <dc:date>2024-02-12T16:41:57Z</dc:date>
    </item>
    <item>
      <title>Re: How to set up dual mac 88W9098</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/How-to-set-up-dual-mac-88W9098/m-p/1810045#M1530</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You can also use the parameters as below to disable mmlan0 and uap0 interface :&lt;BR /&gt;- SD9098_0 use drv_mode=1&lt;BR /&gt;- SD9098_1 use drv_mode=2&lt;/P&gt;
&lt;P&gt;set drv_mode in a configuration file when loading driver (ex : modprobe moal mod_para=nxp/wifi_mod_para.conf) as the following :&lt;/P&gt;
&lt;P&gt;Verified configurations: &lt;BR /&gt;SD9098_0 = {&lt;BR /&gt;cfg80211_wext=0xf&lt;BR /&gt;max_vir_bss=1&lt;BR /&gt;cal_data_cfg=none&lt;BR /&gt;ps_mode=1&lt;BR /&gt;auto_ds=1&lt;BR /&gt;host_mlme=1&lt;BR /&gt;drv_mode=1&lt;BR /&gt;fw_name=nxp/sdiouart9098_combo_v1.bin&lt;BR /&gt;}&lt;BR /&gt;&lt;BR /&gt;SD9098_1 = {&lt;BR /&gt;cfg80211_wext=0xf&lt;BR /&gt;max_vir_bss=1&lt;BR /&gt;cal_data_cfg=none&lt;BR /&gt;ps_mode=1&lt;BR /&gt;auto_ds=1&lt;BR /&gt;host_mlme=1&lt;BR /&gt;drv_mode=2&lt;BR /&gt;fw_name=nxp/sdiouart9098_combo_v1.bin&lt;BR /&gt;}&lt;/P&gt;</description>
      <pubDate>Fri, 16 Feb 2024 14:21:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/How-to-set-up-dual-mac-88W9098/m-p/1810045#M1530</guid>
      <dc:creator>cdoumenc</dc:creator>
      <dc:date>2024-02-16T14:21:23Z</dc:date>
    </item>
    <item>
      <title>Re: How to set up dual mac 88W9098</title>
      <link>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/How-to-set-up-dual-mac-88W9098/m-p/1813727#M1531</link>
      <description>&lt;P&gt;Sorry for the delay in checking. I solved it that way. Thank you !&lt;/P&gt;</description>
      <pubDate>Thu, 22 Feb 2024 10:32:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/How-to-set-up-dual-mac-88W9098/m-p/1813727#M1531</guid>
      <dc:creator>masakiyo</dc:creator>
      <dc:date>2024-02-22T10:32:03Z</dc:date>
    </item>
  </channel>
</rss>