<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can't compile imx-voiceui in Voice Technology</title>
    <link>https://community.nxp.com/t5/Voice-Technology/Can-t-compile-imx-voiceui/m-p/1924848#M66</link>
    <description>I solved the issue. Instead of using 'sudo' to run the make command from a regular user account, I used the root account and successfully compiled the project.</description>
    <pubDate>Mon, 05 Aug 2024 03:02:02 GMT</pubDate>
    <dc:creator>dpcivl</dc:creator>
    <dc:date>2024-08-05T03:02:02Z</dc:date>
    <item>
      <title>Can't compile imx-voiceui</title>
      <link>https://community.nxp.com/t5/Voice-Technology/Can-t-compile-imx-voiceui/m-p/1924836#M65</link>
      <description>&lt;P&gt;Hi, I'm working on a project with the iMX93 EVK board and am currently facing an issue with compiling imx-voiceui.&lt;/P&gt;&lt;P&gt;I need to compile it to get the 'voice_ui_app' with my VIT_KO model. However, whenever I run "make," I always encounter the following error:&lt;/P&gt;&lt;P&gt;/usr/bin/ld: ./platforms/iMX9_CortexA55/lib/libvoiceseeker_no_aec.a(VOICESEEKER_OBJ_0.o): Relocations in generic ELF (EM: 183)&lt;BR /&gt;/usr/bin/ld: ./platforms/iMX9_CortexA55/lib/libvoiceseeker_no_aec.a(VOICESEEKER_OBJ_0.o): Relocations in generic ELF (EM: 183)&lt;BR /&gt;/usr/bin/ld: ./platforms/iMX9_CortexA55/lib/libvoiceseeker_no_aec.a(VOICESEEKER_OBJ_0.o): Relocations in generic ELF (EM: 183)&lt;BR /&gt;/usr/bin/ld: ./platforms/iMX9_CortexA55/lib/libvoiceseeker_no_aec.a: error adding symbols: file in wrong format&lt;BR /&gt;collect2: error: ld returned 1 exit status&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;I tried installing the SDK and adjusting the toolchain for the iMX93, but it didn't resolve the issue. Additionally, I modified the 'Makefile' to use the ${CC} and ${CXX} toolchain variables, yet the problem persists.&lt;/P&gt;&lt;P&gt;How can I fix this? Any help would be greatly appreciated.&lt;/P&gt;</description>
      <pubDate>Mon, 05 Aug 2024 02:43:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Voice-Technology/Can-t-compile-imx-voiceui/m-p/1924836#M65</guid>
      <dc:creator>dpcivl</dc:creator>
      <dc:date>2024-08-05T02:43:44Z</dc:date>
    </item>
    <item>
      <title>Re: Can't compile imx-voiceui</title>
      <link>https://community.nxp.com/t5/Voice-Technology/Can-t-compile-imx-voiceui/m-p/1924848#M66</link>
      <description>I solved the issue. Instead of using 'sudo' to run the make command from a regular user account, I used the root account and successfully compiled the project.</description>
      <pubDate>Mon, 05 Aug 2024 03:02:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Voice-Technology/Can-t-compile-imx-voiceui/m-p/1924848#M66</guid>
      <dc:creator>dpcivl</dc:creator>
      <dc:date>2024-08-05T03:02:02Z</dc:date>
    </item>
  </channel>
</rss>