<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>TapLinx SDK, TagWriter and TagInfo中的主题 In-App Offline Registration for applications questions</title>
    <link>https://community.nxp.com/t5/TapLinx-SDK-TagWriter-and/In-App-Offline-Registration-for-applications-questions/m-p/1975825#M39</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am considering using the "TapLinx SDK for Android" with an application that will be used in environments with differing levels of connectivity.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Will the offline registration method be successful in these environments:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Device that never has an internet connection&lt;/LI&gt;&lt;LI&gt;Device that is connected to a network without an internet connection&lt;/LI&gt;&lt;LI&gt;Device that is connected to a network with internet access, however non-standard internet traffic is blocked (communication with the registration server blocked)&lt;/LI&gt;&lt;LI&gt;What happens if the registration server is down?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Would it also be possible to clarify whether an application that uses the SDK is classified as a derivative work in the license agreement?&lt;/P&gt;&lt;P&gt;Thank you in advanced for your help.&lt;/P&gt;&lt;P&gt;Kind Regards,&lt;/P&gt;&lt;P&gt;Liam&lt;/P&gt;</description>
    <pubDate>Thu, 17 Oct 2024 07:53:02 GMT</pubDate>
    <dc:creator>Liam_H</dc:creator>
    <dc:date>2024-10-17T07:53:02Z</dc:date>
    <item>
      <title>In-App Offline Registration for applications questions</title>
      <link>https://community.nxp.com/t5/TapLinx-SDK-TagWriter-and/In-App-Offline-Registration-for-applications-questions/m-p/1975825#M39</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am considering using the "TapLinx SDK for Android" with an application that will be used in environments with differing levels of connectivity.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Will the offline registration method be successful in these environments:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Device that never has an internet connection&lt;/LI&gt;&lt;LI&gt;Device that is connected to a network without an internet connection&lt;/LI&gt;&lt;LI&gt;Device that is connected to a network with internet access, however non-standard internet traffic is blocked (communication with the registration server blocked)&lt;/LI&gt;&lt;LI&gt;What happens if the registration server is down?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Would it also be possible to clarify whether an application that uses the SDK is classified as a derivative work in the license agreement?&lt;/P&gt;&lt;P&gt;Thank you in advanced for your help.&lt;/P&gt;&lt;P&gt;Kind Regards,&lt;/P&gt;&lt;P&gt;Liam&lt;/P&gt;</description>
      <pubDate>Thu, 17 Oct 2024 07:53:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/TapLinx-SDK-TagWriter-and/In-App-Offline-Registration-for-applications-questions/m-p/1975825#M39</guid>
      <dc:creator>Liam_H</dc:creator>
      <dc:date>2024-10-17T07:53:02Z</dc:date>
    </item>
    <item>
      <title>Re: In-App Offline Registration for applications questions</title>
      <link>https://community.nxp.com/t5/TapLinx-SDK-TagWriter-and/In-App-Offline-Registration-for-applications-questions/m-p/1984495#M47</link>
      <description>&lt;P&gt;Dear Liam_H,&lt;/P&gt;
&lt;P&gt;Please find answers below.&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Device that never has an internet connection&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Yes if the user sends the ancillary key required for the offline license key verification in the register API, this shall work.&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Device that is connected to a network without an internet connection&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Answer same as above.&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Device that is connected to a network with internet access, however non-standard internet traffic is blocked (communication with the registration server blocked)&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Answer same as above.&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;What happens if the registration server is down?&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;If the registration server is down , online license verification will not go through but if the ancillary key is included in the request for offline verification, offline license verification shall work.&lt;/P&gt;
&lt;P&gt;We will come back for licensing question.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;TapLinx team&lt;/P&gt;</description>
      <pubDate>Wed, 30 Oct 2024 07:18:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/TapLinx-SDK-TagWriter-and/In-App-Offline-Registration-for-applications-questions/m-p/1984495#M47</guid>
      <dc:creator>ukcas</dc:creator>
      <dc:date>2024-10-30T07:18:40Z</dc:date>
    </item>
    <item>
      <title>Re: In-App Offline Registration for applications questions</title>
      <link>https://community.nxp.com/t5/TapLinx-SDK-TagWriter-and/In-App-Offline-Registration-for-applications-questions/m-p/1991890#M65</link>
      <description>&lt;P&gt;Dear Ukcas,&lt;/P&gt;&lt;P&gt;Excellent, thank you very much for your help.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Liam&lt;/P&gt;</description>
      <pubDate>Mon, 11 Nov 2024 09:49:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/TapLinx-SDK-TagWriter-and/In-App-Offline-Registration-for-applications-questions/m-p/1991890#M65</guid>
      <dc:creator>Liam_H</dc:creator>
      <dc:date>2024-11-11T09:49:47Z</dc:date>
    </item>
  </channel>
</rss>