<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Transceive failed in TapLinx SDK, TagWriter and TagInfo</title>
    <link>https://community.nxp.com/t5/TapLinx-SDK-TagWriter-and/Transceive-failed/m-p/2181776#M213</link>
    <description>&lt;P&gt;Dear NXP TapLinx Support Team,&lt;/P&gt;&lt;P&gt;I am currently integrating the &lt;STRONG&gt;TapLinx SDK &lt;/STRONG&gt;with a &lt;STRONG&gt;Urovo i9100 POS device&lt;/STRONG&gt; running &lt;STRONG&gt;Android 13&lt;/STRONG&gt;. The POS device has a built-in NFC reader.&lt;/P&gt;&lt;P&gt;When I attempt to detect and initialize a MIFARE DESFire EV3 card using the following&lt;/P&gt;&lt;P&gt;libInstance.getCardType(intent);&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;the function throws an exception:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Transceive failed&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;From the NFC intent, I can confirm that the tag technologies are:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Tech: [android.nfc.tech.IsoDep, android.nfc.tech.NfcA]&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The same DESFire EV3 card works correctly on standard Android phones (e.g., Samsung devices) using the same TapLinx integration, so the issue appears specific to the Urovo POS NFC interface.&lt;/P&gt;&lt;P&gt;Could you please advise:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;Whether TapLinx supports NFC readers on Urovo POS devices (such as the i9100), and&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;If there is a recommended method or configuration for integrating TapLinx with a POS device’s NFC interface (for example, via a custom communication channel or adapter)?&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Any guidance or example for proper initialization on this hardware would be greatly appreciated.&lt;/P&gt;</description>
    <pubDate>Wed, 08 Oct 2025 10:07:15 GMT</pubDate>
    <dc:creator>musabeni</dc:creator>
    <dc:date>2025-10-08T10:07:15Z</dc:date>
    <item>
      <title>Transceive failed</title>
      <link>https://community.nxp.com/t5/TapLinx-SDK-TagWriter-and/Transceive-failed/m-p/2181776#M213</link>
      <description>&lt;P&gt;Dear NXP TapLinx Support Team,&lt;/P&gt;&lt;P&gt;I am currently integrating the &lt;STRONG&gt;TapLinx SDK &lt;/STRONG&gt;with a &lt;STRONG&gt;Urovo i9100 POS device&lt;/STRONG&gt; running &lt;STRONG&gt;Android 13&lt;/STRONG&gt;. The POS device has a built-in NFC reader.&lt;/P&gt;&lt;P&gt;When I attempt to detect and initialize a MIFARE DESFire EV3 card using the following&lt;/P&gt;&lt;P&gt;libInstance.getCardType(intent);&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;the function throws an exception:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Transceive failed&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;From the NFC intent, I can confirm that the tag technologies are:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Tech: [android.nfc.tech.IsoDep, android.nfc.tech.NfcA]&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The same DESFire EV3 card works correctly on standard Android phones (e.g., Samsung devices) using the same TapLinx integration, so the issue appears specific to the Urovo POS NFC interface.&lt;/P&gt;&lt;P&gt;Could you please advise:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;Whether TapLinx supports NFC readers on Urovo POS devices (such as the i9100), and&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;If there is a recommended method or configuration for integrating TapLinx with a POS device’s NFC interface (for example, via a custom communication channel or adapter)?&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Any guidance or example for proper initialization on this hardware would be greatly appreciated.&lt;/P&gt;</description>
      <pubDate>Wed, 08 Oct 2025 10:07:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/TapLinx-SDK-TagWriter-and/Transceive-failed/m-p/2181776#M213</guid>
      <dc:creator>musabeni</dc:creator>
      <dc:date>2025-10-08T10:07:15Z</dc:date>
    </item>
    <item>
      <title>Re: Transceive failed</title>
      <link>https://community.nxp.com/t5/TapLinx-SDK-TagWriter-and/Transceive-failed/m-p/2182016#M214</link>
      <description>&lt;P&gt;Hello, Thank you for your interest in our products.&lt;/P&gt;
&lt;P&gt;As you may already know, Taplinx for Android is a Java-based API that should run in almost any Andorid OS. The&amp;nbsp; Android integration with Taplinx is quite straightforward but, Taplinx doesn't directly manage the communication with the NFC reader IC. This is managed by the OS.&lt;/P&gt;
&lt;P&gt;Since you are using a POS solution from Urovo, my recommendation is to please check with them a correct integration of the Driver to successfully connect it with your Application.&lt;/P&gt;</description>
      <pubDate>Wed, 08 Oct 2025 17:11:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/TapLinx-SDK-TagWriter-and/Transceive-failed/m-p/2182016#M214</guid>
      <dc:creator>Fabian_R</dc:creator>
      <dc:date>2025-10-08T17:11:06Z</dc:date>
    </item>
  </channel>
</rss>