<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: mfrc522 in TapLinx SDK, TagWriter and TagInfo</title>
    <link>https://community.nxp.com/t5/TapLinx-SDK-TagWriter-and/mfrc522/m-p/2117746#M173</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/251627"&gt;@wael_fakher&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;It is recommended that you use a logic analyzer to check whether the SPI communication between ESP32 and MFRC522 is correct or not.&lt;/P&gt;</description>
    <pubDate>Tue, 17 Jun 2025 12:04:09 GMT</pubDate>
    <dc:creator>KaiLi</dc:creator>
    <dc:date>2025-06-17T12:04:09Z</dc:date>
    <item>
      <title>mfrc522</title>
      <link>https://community.nxp.com/t5/TapLinx-SDK-TagWriter-and/mfrc522/m-p/2117538#M172</link>
      <description>&lt;P&gt;I designed a PCB that integrates an ESP32 and an MFRC522 RFID module. However, the ESP32 was initially unable to communicate with the MFRC522 until I reduced the SPI communication speed to 200 kHz. Even then, the reader was still unable to detect RFID tags.&lt;/P&gt;&lt;P&gt;Additionally, I need the MFRC522 to support three external antennas via IPEX connectors.&lt;/P&gt;&lt;P&gt;I would appreciate guidance on improving my design to ensure stable communication between the ESP32 and MFRC522, and to properly support external antennas.&lt;BR /&gt;&lt;BR /&gt;please see my pcb design&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jun 2025 07:53:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/TapLinx-SDK-TagWriter-and/mfrc522/m-p/2117538#M172</guid>
      <dc:creator>wael_fakher</dc:creator>
      <dc:date>2025-06-17T07:53:49Z</dc:date>
    </item>
    <item>
      <title>Re: mfrc522</title>
      <link>https://community.nxp.com/t5/TapLinx-SDK-TagWriter-and/mfrc522/m-p/2117746#M173</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/251627"&gt;@wael_fakher&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;It is recommended that you use a logic analyzer to check whether the SPI communication between ESP32 and MFRC522 is correct or not.&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jun 2025 12:04:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/TapLinx-SDK-TagWriter-and/mfrc522/m-p/2117746#M173</guid>
      <dc:creator>KaiLi</dc:creator>
      <dc:date>2025-06-17T12:04:09Z</dc:date>
    </item>
    <item>
      <title>Re: mfrc522</title>
      <link>https://community.nxp.com/t5/TapLinx-SDK-TagWriter-and/mfrc522/m-p/2117821#M174</link>
      <description>&lt;P&gt;and what about the antenna ?&lt;BR /&gt;is it possible to have 3 ipex in parallel ?&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jun 2025 13:23:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/TapLinx-SDK-TagWriter-and/mfrc522/m-p/2117821#M174</guid>
      <dc:creator>wael_fakher</dc:creator>
      <dc:date>2025-06-17T13:23:15Z</dc:date>
    </item>
    <item>
      <title>Re: mfrc522</title>
      <link>https://community.nxp.com/t5/TapLinx-SDK-TagWriter-and/mfrc522/m-p/2123687#M177</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/251627"&gt;@wael_fakher&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You mentioned that "I need the MFRC522 to support three external antennas via IPEX connectors." From the schematic you provided, I did not see this part design. In your design, there is an MFRC522 and a PN5321. Why has two readers? what are they using for?&lt;/P&gt;</description>
      <pubDate>Thu, 26 Jun 2025 06:51:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/TapLinx-SDK-TagWriter-and/mfrc522/m-p/2123687#M177</guid>
      <dc:creator>KaiLi</dc:creator>
      <dc:date>2025-06-26T06:51:14Z</dc:date>
    </item>
  </channel>
</rss>