<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: P71D600 Secure element SDK ? in Smart Cards and Secure Element</title>
    <link>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/P71D600-Secure-element-SDK/m-p/2411146#M315</link>
    <description>&lt;P&gt;Hi when you say SDK version this could mean several things:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;If you are talking about the compliance level of the card, it is specifically Java Card 3.0.5 and Global Platform 2.3 and this is likely not to change I would imagine (though certain features and fixes may change over time).&lt;/LI&gt;&lt;LI&gt;If you mean which OS level, patch, modules and OS features available, etc most of it you can get from the GET DATA (IDENTIFY) command which you can find details on in the JCOP 4.5 User Guidance and Admin manual under NDA.&lt;/LI&gt;&lt;LI&gt;If you mean which packages / libraries are loaded in the ISD, this can be read using the GlobalPlatform GET STATUS command (no NDA needed for this).&lt;/LI&gt;&lt;/UL&gt;</description>
    <pubDate>Fri, 04 Sep 2026 01:30:29 GMT</pubDate>
    <dc:creator>makinako</dc:creator>
    <dc:date>2026-09-04T01:30:29Z</dc:date>
    <item>
      <title>P71D600 Secure element SDK ?</title>
      <link>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/P71D600-Secure-element-SDK/m-p/2411049#M314</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have been working with the SE P71D600 and would like to know how I can check which SDK is preloaded on the chip.&lt;/P&gt;&lt;P&gt;Could you please guide me on how to verify the SDK version or details?&lt;/P&gt;&lt;P&gt;Thanks.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 03 Sep 2026 12:44:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/P71D600-Secure-element-SDK/m-p/2411049#M314</guid>
      <dc:creator>elgin_1950</dc:creator>
      <dc:date>2026-09-03T12:44:25Z</dc:date>
    </item>
    <item>
      <title>Re: P71D600 Secure element SDK ?</title>
      <link>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/P71D600-Secure-element-SDK/m-p/2411146#M315</link>
      <description>&lt;P&gt;Hi when you say SDK version this could mean several things:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;If you are talking about the compliance level of the card, it is specifically Java Card 3.0.5 and Global Platform 2.3 and this is likely not to change I would imagine (though certain features and fixes may change over time).&lt;/LI&gt;&lt;LI&gt;If you mean which OS level, patch, modules and OS features available, etc most of it you can get from the GET DATA (IDENTIFY) command which you can find details on in the JCOP 4.5 User Guidance and Admin manual under NDA.&lt;/LI&gt;&lt;LI&gt;If you mean which packages / libraries are loaded in the ISD, this can be read using the GlobalPlatform GET STATUS command (no NDA needed for this).&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Fri, 04 Sep 2026 01:30:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/P71D600-Secure-element-SDK/m-p/2411146#M315</guid>
      <dc:creator>makinako</dc:creator>
      <dc:date>2026-09-04T01:30:29Z</dc:date>
    </item>
    <item>
      <title>Re: P71D600 Secure element SDK ?</title>
      <link>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/P71D600-Secure-element-SDK/m-p/2411574#M316</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/263973"&gt;@elgin_1950&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Based on P71D600 - is it JCOP 4.5?&amp;nbsp;On JCOP 4.5 we don't call it SDKs, there we have modules and applets. The configuration can be identified by reading the OEF number or checking the exact type name. Please clarify.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 07 Sep 2026 02:25:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/P71D600-Secure-element-SDK/m-p/2411574#M316</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2026-09-07T02:25:41Z</dc:date>
    </item>
    <item>
      <title>Re: P71D600 Secure element SDK ?</title>
      <link>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/P71D600-Secure-element-SDK/m-p/2411590#M317</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/59276"&gt;@Kan_Li&lt;/a&gt;&amp;nbsp; and &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/180285"&gt;@makinako&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thanks for your response.&lt;/P&gt;&lt;P&gt;Yes, you are right,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/59276"&gt;@Kan_Li&lt;/a&gt;&amp;nbsp; it is JCOP 4.5, My mistake Let me clarify what I was asking.&lt;/P&gt;&lt;P&gt;I am working on a biometric matching algorithm, where the Match-on-Card (MoC) functionality is provided by third-party vendors. NXP offers products that support different MoC biometric providers.&amp;nbsp; For example, the MoC functionality may be provided by ID3 or Neurotechnology (NT).&lt;/P&gt;&lt;P&gt;My question is: &lt;STRONG&gt;How can I identify which MoC solution or biometric provider is already preloaded on a particular card?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I have SDKs for both providers and can build the corresponding applets and modules. However, I am a little confused about how the preloaded components work and how I can determine which solution is present on the card.&lt;/P&gt;&lt;P&gt;Could you please clarify how this can be identified?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 07 Sep 2026 05:09:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/P71D600-Secure-element-SDK/m-p/2411590#M317</guid>
      <dc:creator>elgin_1950</dc:creator>
      <dc:date>2026-09-07T05:09:00Z</dc:date>
    </item>
  </channel>
</rss>