<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic secure element se051 revers current in Smart Cards and Secure Element</title>
    <link>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/secure-element-se051-revers-current/m-p/2161766#M259</link>
    <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using&amp;nbsp; &lt;LI-PRODUCT title="SE051" id="SE051"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to use the secure element feature to meet the Matter security criteria and the 14443A feature to implement Tap to Pair.&lt;/P&gt;&lt;P&gt;VIN Pin : in 3.3V DC Global net&lt;/P&gt;&lt;P&gt;Vout Pin pad to VCC Pin pad Connection.&lt;/P&gt;&lt;P&gt;SE051 switches on/off between VIN and Vout via the ENA pin.&lt;/P&gt;&lt;P&gt;When the switch is turned off, 14443a is activated..&lt;/P&gt;&lt;P&gt;Can the magnetically induced power from the NFC reader to the 14443 antenna affect the VIN?&lt;/P&gt;&lt;P&gt;Is the internal power switch of the SE051 protected against reverse current?&lt;/P&gt;&lt;P&gt;If this is not taken into consideration, can you suggest a solution?&lt;/P&gt;&lt;P&gt;Can I implement Matter's Tap to pair using SE051's 14443 feature?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 02 Sep 2025 04:23:42 GMT</pubDate>
    <dc:creator>Devkun</dc:creator>
    <dc:date>2025-09-02T04:23:42Z</dc:date>
    <item>
      <title>secure element se051 revers current</title>
      <link>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/secure-element-se051-revers-current/m-p/2161766#M259</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using&amp;nbsp; &lt;LI-PRODUCT title="SE051" id="SE051"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to use the secure element feature to meet the Matter security criteria and the 14443A feature to implement Tap to Pair.&lt;/P&gt;&lt;P&gt;VIN Pin : in 3.3V DC Global net&lt;/P&gt;&lt;P&gt;Vout Pin pad to VCC Pin pad Connection.&lt;/P&gt;&lt;P&gt;SE051 switches on/off between VIN and Vout via the ENA pin.&lt;/P&gt;&lt;P&gt;When the switch is turned off, 14443a is activated..&lt;/P&gt;&lt;P&gt;Can the magnetically induced power from the NFC reader to the 14443 antenna affect the VIN?&lt;/P&gt;&lt;P&gt;Is the internal power switch of the SE051 protected against reverse current?&lt;/P&gt;&lt;P&gt;If this is not taken into consideration, can you suggest a solution?&lt;/P&gt;&lt;P&gt;Can I implement Matter's Tap to pair using SE051's 14443 feature?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Sep 2025 04:23:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/secure-element-se051-revers-current/m-p/2161766#M259</guid>
      <dc:creator>Devkun</dc:creator>
      <dc:date>2025-09-02T04:23:42Z</dc:date>
    </item>
    <item>
      <title>Re: secure element se051 revers current</title>
      <link>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/secure-element-se051-revers-current/m-p/2161826#M260</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/254330"&gt;@Devkun&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Can the magnetically induced power from the NFC reader to the 14443 antenna affect the VIN?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;-No, it just supplies power to the same domain powered by VCC pin.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 02 Sep 2025 06:10:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/secure-element-se051-revers-current/m-p/2161826#M260</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2025-09-02T06:10:02Z</dc:date>
    </item>
    <item>
      <title>Re: secure element se051 revers current</title>
      <link>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/secure-element-se051-revers-current/m-p/2162092#M261</link>
      <description>Thanks for the quick feedback.&lt;BR /&gt;i have a one more question.&lt;BR /&gt;According to the datasheet of SE051&lt;BR /&gt;The chosen interface is the only interface the SE051 will receive commands for processing. To select a different interface the IC needs to be reset.&lt;BR /&gt;&lt;BR /&gt;My question is : can a reset be performed by controlling the ENA pin, thereby changing the interface?&lt;BR /&gt;&lt;BR /&gt;</description>
      <pubDate>Tue, 02 Sep 2025 10:40:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/secure-element-se051-revers-current/m-p/2162092#M261</guid>
      <dc:creator>Devkun</dc:creator>
      <dc:date>2025-09-02T10:40:07Z</dc:date>
    </item>
  </channel>
</rss>