<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Smart Cards and Secure Element中的主题 Re: Using ISO14443-connected SE05x from mobile apps</title>
    <link>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/Using-ISO14443-connected-SE05x-from-mobile-apps/m-p/2099269#M219</link>
    <description>&lt;P&gt;Thank you&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/59276"&gt;@Kan_Li&lt;/a&gt;&amp;nbsp;there is a little code snippet for Android in appendix A. That might be a good start for me.&lt;/P&gt;</description>
    <pubDate>Sat, 17 May 2025 10:33:26 GMT</pubDate>
    <dc:creator>psvz</dc:creator>
    <dc:date>2025-05-17T10:33:26Z</dc:date>
    <item>
      <title>Using ISO14443-connected SE05x from mobile apps</title>
      <link>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/Using-ISO14443-connected-SE05x-from-mobile-apps/m-p/2098104#M217</link>
      <description>&lt;P&gt;Both iPhone and Android-based mobiles have NFC reader with native API...&lt;/P&gt;&lt;P&gt;I noticed that SE05x middleware I use (downloaded as&amp;nbsp;se05x_mw_v04.05.00.zip file) is mostly focused on Raspberry PI's T1oI2C connectivity e.g., the build folder is named as&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;simw-top_build/raspbian_native_se050_t1oi2c/&lt;/LI-CODE&gt;&lt;P&gt;from which I compile it to work with PCSC/ third party USB reader.&lt;/P&gt;&lt;P&gt;Do we have any other middleware or any documentation on integration with NFC capabilities of mobiles devices? Essentially, I am to develop an app that talks to SE05x over&amp;nbsp;ISO14443.&lt;/P&gt;&lt;P&gt;If not, do we have such documentation and/or middleware in JCOP ID2 realm?&lt;/P&gt;</description>
      <pubDate>Thu, 15 May 2025 11:05:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/Using-ISO14443-connected-SE05x-from-mobile-apps/m-p/2098104#M217</guid>
      <dc:creator>psvz</dc:creator>
      <dc:date>2025-05-15T11:05:49Z</dc:date>
    </item>
    <item>
      <title>Re: Using ISO14443-connected SE05x from mobile apps</title>
      <link>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/Using-ISO14443-connected-SE05x-from-mobile-apps/m-p/2098985#M218</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210414"&gt;@psvz&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I am sorry, but so far the MW for se05x doesn't support mobile platform, we just have an AN on the NFC related development, please kindly refer to&amp;nbsp;&lt;A href="https://www.nxp.com.cn/docs/en/nxp/application-notes/AN12664.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/nxp/application-notes/AN12664.pdf&lt;/A&gt;&amp;nbsp;for details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope that helps,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 16 May 2025 11:45:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/Using-ISO14443-connected-SE05x-from-mobile-apps/m-p/2098985#M218</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2025-05-16T11:45:45Z</dc:date>
    </item>
    <item>
      <title>Re: Using ISO14443-connected SE05x from mobile apps</title>
      <link>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/Using-ISO14443-connected-SE05x-from-mobile-apps/m-p/2099269#M219</link>
      <description>&lt;P&gt;Thank you&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/59276"&gt;@Kan_Li&lt;/a&gt;&amp;nbsp;there is a little code snippet for Android in appendix A. That might be a good start for me.&lt;/P&gt;</description>
      <pubDate>Sat, 17 May 2025 10:33:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/Using-ISO14443-connected-SE05x-from-mobile-apps/m-p/2099269#M219</guid>
      <dc:creator>psvz</dc:creator>
      <dc:date>2025-05-17T10:33:26Z</dc:date>
    </item>
  </channel>
</rss>