<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SE051 Key Diverisification Algorithm in Smart Cards and Secure Element</title>
    <link>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/SE051-Key-Diverisification-Algorithm/m-p/2051092#M182</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have an SE051 which I am storing symmetric keys on. I am using the Plug and Trust Nano-Package, and am building an app using Zephyr.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Generally, I am able to use the SE051 and the Nano Package in order to generate and use diversified keys on the SE051.&lt;BR /&gt;&lt;BR /&gt;However, I was wondering, am I able to change the algorithm on the SE051 by which keys are diversified? My understanding based on AN12543, is that keys are diversified in a means described by AN10922.&lt;BR /&gt;&lt;BR /&gt;Is there a way to change this? Or is the method described in AN10922 the only way the SE051 can diversify keys?&lt;BR /&gt;&lt;BR /&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Tue, 25 Feb 2025 20:07:17 GMT</pubDate>
    <dc:creator>trink185</dc:creator>
    <dc:date>2025-02-25T20:07:17Z</dc:date>
    <item>
      <title>SE051 Key Diverisification Algorithm</title>
      <link>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/SE051-Key-Diverisification-Algorithm/m-p/2051092#M182</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have an SE051 which I am storing symmetric keys on. I am using the Plug and Trust Nano-Package, and am building an app using Zephyr.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Generally, I am able to use the SE051 and the Nano Package in order to generate and use diversified keys on the SE051.&lt;BR /&gt;&lt;BR /&gt;However, I was wondering, am I able to change the algorithm on the SE051 by which keys are diversified? My understanding based on AN12543, is that keys are diversified in a means described by AN10922.&lt;BR /&gt;&lt;BR /&gt;Is there a way to change this? Or is the method described in AN10922 the only way the SE051 can diversify keys?&lt;BR /&gt;&lt;BR /&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Tue, 25 Feb 2025 20:07:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/SE051-Key-Diverisification-Algorithm/m-p/2051092#M182</guid>
      <dc:creator>trink185</dc:creator>
      <dc:date>2025-02-25T20:07:17Z</dc:date>
    </item>
    <item>
      <title>Re: SE051 Key Diverisification Algorithm</title>
      <link>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/SE051-Key-Diverisification-Algorithm/m-p/2051357#M183</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/247329"&gt;@trink185&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The&amp;nbsp;&lt;SPAN&gt;algorithm on the SE051 to&amp;nbsp;diversify key is fixed, but of course you may determine which key to be&amp;nbsp;diversified.&amp;nbsp;AN12543 addresses this explicitly as below:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Create a Diversified Key according [AN10922]. Input is divInput of 1 up to 31 bytes.&lt;BR /&gt;Note that users need to create the diversified key object before calling this function.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;It is also recommended creating&amp;nbsp;the diversified key object as a transient object to avoid memory consumption.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Hope that helps,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 26 Feb 2025 06:15:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/SE051-Key-Diverisification-Algorithm/m-p/2051357#M183</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2025-02-26T06:15:42Z</dc:date>
    </item>
  </channel>
</rss>