<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic JCShell 6.9.0.12 problem connecting to card reader on Windows 10 x64 in Smart Cards and Secure Element</title>
    <link>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/JCShell-6-9-0-12-problem-connecting-to-card-reader-on-Windows-10/m-p/1964689#M168</link>
    <description>&lt;P&gt;With&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;/list-readers&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can see 4 PC SC card readers connected, one physical card reader I want to use here and 3 virtual ones inluding Windows Hello which I can't remove.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The manual describes how to connect to a PC SC card reader but does not specify how to select the desired one if there are multiple. How can I select a specific reader after I have the list from "/list-readers"?&lt;/P&gt;</description>
    <pubDate>Mon, 30 Sep 2024 19:02:37 GMT</pubDate>
    <dc:creator>fus</dc:creator>
    <dc:date>2024-09-30T19:02:37Z</dc:date>
    <item>
      <title>JCShell 6.9.0.12 problem connecting to card reader on Windows 10 x64</title>
      <link>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/JCShell-6-9-0-12-problem-connecting-to-card-reader-on-Windows-10/m-p/1964689#M168</link>
      <description>&lt;P&gt;With&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;/list-readers&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can see 4 PC SC card readers connected, one physical card reader I want to use here and 3 virtual ones inluding Windows Hello which I can't remove.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The manual describes how to connect to a PC SC card reader but does not specify how to select the desired one if there are multiple. How can I select a specific reader after I have the list from "/list-readers"?&lt;/P&gt;</description>
      <pubDate>Mon, 30 Sep 2024 19:02:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/JCShell-6-9-0-12-problem-connecting-to-card-reader-on-Windows-10/m-p/1964689#M168</guid>
      <dc:creator>fus</dc:creator>
      <dc:date>2024-09-30T19:02:37Z</dc:date>
    </item>
    <item>
      <title>Re: JCShell 6.9.0.12 problem connecting to card reader on Windows 10 x64</title>
      <link>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/JCShell-6-9-0-12-problem-connecting-to-card-reader-on-Windows-10/m-p/1964818#M169</link>
      <description>&lt;P&gt;Try this:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;/term SCComm:1:"The reader name from /list-readers":protocol=1&lt;/LI-CODE&gt;&lt;P&gt;Replace protocol with 0 for T=1. Keep in mind the name of the reader as it appears in your Device Manager will not necessarily be exactly the same as from /list-readers.&lt;/P&gt;&lt;P&gt;Example:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;/term SCComm:1:"Identiv uTrust 2700 R Smart Card Reader 0":protocol=1
# Do a bunch of commands here
/close&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 30 Sep 2024 22:42:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/JCShell-6-9-0-12-problem-connecting-to-card-reader-on-Windows-10/m-p/1964818#M169</guid>
      <dc:creator>makinako</dc:creator>
      <dc:date>2024-09-30T22:42:13Z</dc:date>
    </item>
  </channel>
</rss>