<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Store private key in SE050 chip in Smart Cards and Secure Element</title>
    <link>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/Store-private-key-in-SE050-chip/m-p/1874580#M125</link>
    <description>&lt;P&gt;Hallo,&lt;/P&gt;&lt;P&gt;Currently we are working with SE050 crypto chip with S32K146 micro controllers.&lt;BR /&gt;We have two binaries.&lt;/P&gt;&lt;P&gt;Firmware 1. Writes the private key to the SE050 during start up of the system&lt;/P&gt;&lt;P&gt;Firmware 2. Do not write the private key because it already writtern with Firmware1 and loads the same private key during init.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We want to avoid maintaining two firmwares.&lt;/P&gt;&lt;P&gt;Can we write multiple times (every start up) the private key on SE050 chip ? Does the private key stores in eeprom of SE050 crypto chip?&lt;/P&gt;&lt;P&gt;Is there any possibility to read stored private key and avoid writing duplicate key?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Saidhi reddy Sareddy&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;@&amp;nbsp;Christine_Li&lt;/P&gt;</description>
    <pubDate>Fri, 24 May 2024 10:37:58 GMT</pubDate>
    <dc:creator>saireddy_saredd</dc:creator>
    <dc:date>2024-05-24T10:37:58Z</dc:date>
    <item>
      <title>Store private key in SE050 chip</title>
      <link>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/Store-private-key-in-SE050-chip/m-p/1874580#M125</link>
      <description>&lt;P&gt;Hallo,&lt;/P&gt;&lt;P&gt;Currently we are working with SE050 crypto chip with S32K146 micro controllers.&lt;BR /&gt;We have two binaries.&lt;/P&gt;&lt;P&gt;Firmware 1. Writes the private key to the SE050 during start up of the system&lt;/P&gt;&lt;P&gt;Firmware 2. Do not write the private key because it already writtern with Firmware1 and loads the same private key during init.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We want to avoid maintaining two firmwares.&lt;/P&gt;&lt;P&gt;Can we write multiple times (every start up) the private key on SE050 chip ? Does the private key stores in eeprom of SE050 crypto chip?&lt;/P&gt;&lt;P&gt;Is there any possibility to read stored private key and avoid writing duplicate key?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Saidhi reddy Sareddy&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;@&amp;nbsp;Christine_Li&lt;/P&gt;</description>
      <pubDate>Fri, 24 May 2024 10:37:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/Store-private-key-in-SE050-chip/m-p/1874580#M125</guid>
      <dc:creator>saireddy_saredd</dc:creator>
      <dc:date>2024-05-24T10:37:58Z</dc:date>
    </item>
    <item>
      <title>Re: Store private key in SE050 chip</title>
      <link>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/Store-private-key-in-SE050-chip/m-p/1875139#M126</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/134480"&gt;@saireddy_saredd&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, it is ok to&amp;nbsp;&lt;SPAN&gt;write multiple times (every start up) the private key on SE050 chip, and&amp;nbsp;the private key stores in eeprom/internal flash of SE050 crypto chip, but it consumes the flash/eeprom endurance . Why not check the key availability on start up? There is such APDU command available, please refer to the section for&amp;nbsp;CheckObjectExists in the APDU command spec for details.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Please also note any private key stored in SE050 can not be read out, I assume you are referring to the public key , right?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 27 May 2024 03:31:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Smart-Cards-and-Secure-Element/Store-private-key-in-SE050-chip/m-p/1875139#M126</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2024-05-27T03:31:17Z</dc:date>
    </item>
  </channel>
</rss>