<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to properly create and configure a project for the R52 core with S32Z2 in S32Z/E</title>
    <link>https://community.nxp.com/t5/S32Z-E/How-to-properly-create-and-configure-a-project-for-the-R52-core/m-p/2364034#M331</link>
    <description>&lt;P class=""&gt;&lt;SPAN&gt;Hi Team,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;I am working with the S32Z280 development board and I installed RTD version 2.0.1.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;I successfully ran the &lt;/SPAN&gt;&lt;SPAN&gt;Dio_Example_S32Z2XX_SMU&lt;/SPAN&gt;&lt;SPAN&gt; example project (D12 LED blinking) on the M33 core.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;Next, I tried to blink the same D12 LED using the R52 core. I created a new R52 project and configured the same LED pin based on the example project. The project builds successfully without any errors.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;However, after flashing, the LED is not blinking.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;Currently, I do not have a debugger. So I am generating the flash image using IVT and flashing it through the J119 USB port.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;Could anyone help me understand:&lt;/SPAN&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;SPAN&gt;How to properly create and configure a project for the R52 core?&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;Are there any additional startup or clock configurations required for R52?&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;Is there any specific procedure for generating and flashing the R52 image using IVT?&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P class=""&gt;&lt;SPAN&gt;Any guidance or reference examples would be very helpful.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 12 May 2026 10:00:13 GMT</pubDate>
    <dc:creator>karthik_nikil</dc:creator>
    <dc:date>2026-05-12T10:00:13Z</dc:date>
    <item>
      <title>How to properly create and configure a project for the R52 core with S32Z2</title>
      <link>https://community.nxp.com/t5/S32Z-E/How-to-properly-create-and-configure-a-project-for-the-R52-core/m-p/2364034#M331</link>
      <description>&lt;P class=""&gt;&lt;SPAN&gt;Hi Team,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;I am working with the S32Z280 development board and I installed RTD version 2.0.1.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;I successfully ran the &lt;/SPAN&gt;&lt;SPAN&gt;Dio_Example_S32Z2XX_SMU&lt;/SPAN&gt;&lt;SPAN&gt; example project (D12 LED blinking) on the M33 core.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;Next, I tried to blink the same D12 LED using the R52 core. I created a new R52 project and configured the same LED pin based on the example project. The project builds successfully without any errors.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;However, after flashing, the LED is not blinking.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;Currently, I do not have a debugger. So I am generating the flash image using IVT and flashing it through the J119 USB port.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;Could anyone help me understand:&lt;/SPAN&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;SPAN&gt;How to properly create and configure a project for the R52 core?&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;Are there any additional startup or clock configurations required for R52?&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;Is there any specific procedure for generating and flashing the R52 image using IVT?&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P class=""&gt;&lt;SPAN&gt;Any guidance or reference examples would be very helpful.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 12 May 2026 10:00:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32Z-E/How-to-properly-create-and-configure-a-project-for-the-R52-core/m-p/2364034#M331</guid>
      <dc:creator>karthik_nikil</dc:creator>
      <dc:date>2026-05-12T10:00:13Z</dc:date>
    </item>
    <item>
      <title>Re: How to properly create and configure a project for the R52 core with S32Z2</title>
      <link>https://community.nxp.com/t5/S32Z-E/How-to-properly-create-and-configure-a-project-for-the-R52-core/m-p/2364203#M332</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/259291"&gt;@karthik_nikil&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;Currently in the default setup, many S32E examples are configured to run on the Cortex-R52 cores, while S32Z examples are designed to run on the SMU (System Manager Unit) core.&lt;/P&gt;
&lt;P&gt;My colleague once wrote the following reference &lt;A href="https://community.nxp.com/t5/S32Z-E-Knowledge-Base/Change-boot-core-of-the-examples-for-S32Z2-E2/ta-p/2161604" target="_self"&gt;document&lt;/A&gt;, which provided the method for changing the default R52 booting to SMU case, it is just an opposite example which would be valuable reference for your requirement.&lt;/P&gt;
&lt;P&gt;I hope it will help on your case&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Tue, 12 May 2026 13:30:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32Z-E/How-to-properly-create-and-configure-a-project-for-the-R52-core/m-p/2364203#M332</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2026-05-12T13:30:57Z</dc:date>
    </item>
    <item>
      <title>Re: How to properly create and configure a project for the R52 core with S32Z2</title>
      <link>https://community.nxp.com/t5/S32Z-E/How-to-properly-create-and-configure-a-project-for-the-R52-core/m-p/2364539#M333</link>
      <description>&lt;P class=""&gt;&lt;SPAN&gt;Hi Chenyin,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;Thank you for the information.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;I would like to confirm one point — does the S32Z2 board support running applications on the R52 core directly, or is additional boot configuration required to start the R52 core?&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;Currently, I can run the SMU/M33 example successfully, but my R52 LED blink project is not running after flashing.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;BR,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Karthik&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 13 May 2026 06:19:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32Z-E/How-to-properly-create-and-configure-a-project-for-the-R52-core/m-p/2364539#M333</guid>
      <dc:creator>karthik_nikil</dc:creator>
      <dc:date>2026-05-13T06:19:17Z</dc:date>
    </item>
    <item>
      <title>Re: How to properly create and configure a project for the R52 core with S32Z2</title>
      <link>https://community.nxp.com/t5/S32Z-E/How-to-properly-create-and-configure-a-project-for-the-R52-core/m-p/2364776#M334</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/259291"&gt;@karthik_nikil&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your reply.&lt;/P&gt;
&lt;P&gt;Yes, I am able to confirm that the&lt;SPAN&gt;&amp;nbsp;S32Z2 board support running applications from the R52 cores.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Chenyin&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 13 May 2026 09:45:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32Z-E/How-to-properly-create-and-configure-a-project-for-the-R52-core/m-p/2364776#M334</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2026-05-13T09:45:54Z</dc:date>
    </item>
    <item>
      <title>Re: How to properly create and configure a project for the R52 core with S32Z2</title>
      <link>https://community.nxp.com/t5/S32Z-E/How-to-properly-create-and-configure-a-project-for-the-R52-core/m-p/2364851#M335</link>
      <description>Hi Chenyin,&lt;BR /&gt;&lt;BR /&gt;Thank you for the confirmation.&lt;BR /&gt;&lt;BR /&gt;In my case, I created a simple R52 LED blink project and generated the flash image using IVT, then flashed it through the J119 USB port. The project builds successfully, but the LED is not blinking.&lt;BR /&gt;&lt;BR /&gt;Could you please guide me on:&lt;BR /&gt;&lt;BR /&gt;the correct procedure to boot and run an R52 application on the S32Z2 board,&lt;BR /&gt;whether any special boot configuration or startup settings are required,&lt;BR /&gt;and if there is any reference example available for R52 standalone execution?&lt;BR /&gt;&lt;BR /&gt;Thank you.&lt;BR /&gt;&lt;BR /&gt;BR,&lt;BR /&gt;Karthik</description>
      <pubDate>Wed, 13 May 2026 11:22:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32Z-E/How-to-properly-create-and-configure-a-project-for-the-R52-core/m-p/2364851#M335</guid>
      <dc:creator>karthik_nikil</dc:creator>
      <dc:date>2026-05-13T11:22:35Z</dc:date>
    </item>
    <item>
      <title>Re: How to properly create and configure a project for the R52 core with S32Z2</title>
      <link>https://community.nxp.com/t5/S32Z-E/How-to-properly-create-and-configure-a-project-for-the-R52-core/m-p/2366623#M349</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/259291"&gt;@karthik_nikil&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your reply.&lt;/P&gt;
&lt;P&gt;1. As mentioned, there is not a formal example existed for your reference, since the default example which match your requirement is done by booting from SMU.(Dio_Example_S32Z2XX_SMU)&lt;/P&gt;
&lt;P&gt;2. For creating a similar project booting from R52, you may firstly creating a S32 application project, and then add/set the corresponding modules needed referencing the&amp;nbsp;Dio_Example_S32Z2XX_SMU.&lt;/P&gt;
&lt;P&gt;3. Once finished, creating IVT based binary with the following guide, and then flashed it to the board to have a try.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32Z-E/creating-a-Blob-Image-using-IVT-S32Z2/td-p/2362406" target="_blank"&gt;creating a Blob Image using IVT S32Z2&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32Z-E/How-to-reduce-the-binary-size-in-S32Z2/td-p/2361543" target="_blank"&gt;How to reduce the binary size in S32Z2&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;4. I am preparing writing a document to introduce the details, but it may take some time due internal writing/review process&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Mon, 18 May 2026 03:03:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32Z-E/How-to-properly-create-and-configure-a-project-for-the-R52-core/m-p/2366623#M349</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2026-05-18T03:03:46Z</dc:date>
    </item>
  </channel>
</rss>