<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LLCE in S32Z/E</title>
    <link>https://community.nxp.com/t5/S32Z-E/LLCE/m-p/2326753#M249</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;1. OCT is the On-chip transmitter,&amp;nbsp;The logic determines if any of the CAN modules contributing to a network have won arbitration and are now the bus transmitter.&lt;/P&gt;
&lt;P&gt;2. FQ is the&amp;nbsp;Fault qualifier,&amp;nbsp;&amp;nbsp;the&amp;nbsp;&lt;SPAN class="fontstyle0"&gt;logic will qualify any of the 6 FCCU fault reactions with a configuration register&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;3. STXA is the Suppress TX arbitration&lt;/P&gt;
&lt;P&gt;4. AW is Arbitration win, the last two signals are used for the internal arbitration in CAN HUB&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
    <pubDate>Thu, 05 Mar 2026 06:31:02 GMT</pubDate>
    <dc:creator>chenyin_h</dc:creator>
    <dc:date>2026-03-05T06:31:02Z</dc:date>
    <item>
      <title>LLCE</title>
      <link>https://community.nxp.com/t5/S32Z-E/LLCE/m-p/2326226#M247</link>
      <description>&lt;P&gt;In Figure 787 of the CAN HUB (CE_CAN_HUB) section within Part 10 LLCE of the 32E series, what do the abbreviations OCT/FQ/STXA/AW signify, and what are their specific functions? Particularly, STXA and AW are not explained anywhere in the entire document.&lt;/P&gt;</description>
      <pubDate>Wed, 04 Mar 2026 09:41:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32Z-E/LLCE/m-p/2326226#M247</guid>
      <dc:creator>yuancz</dc:creator>
      <dc:date>2026-03-04T09:41:46Z</dc:date>
    </item>
    <item>
      <title>Re: LLCE</title>
      <link>https://community.nxp.com/t5/S32Z-E/LLCE/m-p/2326753#M249</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;1. OCT is the On-chip transmitter,&amp;nbsp;The logic determines if any of the CAN modules contributing to a network have won arbitration and are now the bus transmitter.&lt;/P&gt;
&lt;P&gt;2. FQ is the&amp;nbsp;Fault qualifier,&amp;nbsp;&amp;nbsp;the&amp;nbsp;&lt;SPAN class="fontstyle0"&gt;logic will qualify any of the 6 FCCU fault reactions with a configuration register&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;3. STXA is the Suppress TX arbitration&lt;/P&gt;
&lt;P&gt;4. AW is Arbitration win, the last two signals are used for the internal arbitration in CAN HUB&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Thu, 05 Mar 2026 06:31:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32Z-E/LLCE/m-p/2326753#M249</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2026-03-05T06:31:02Z</dc:date>
    </item>
    <item>
      <title>Re: LLCE</title>
      <link>https://community.nxp.com/t5/S32Z-E/LLCE/m-p/2328678#M250</link>
      <description>Is it correct to understand that the acceleration method for the LLCE in the S32 series is primarily achieved through software-based routing and forwarding? In reality, the hardware only contains a lookup table, while the forwarding of destinations is entirely handled by software?</description>
      <pubDate>Mon, 09 Mar 2026 07:02:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32Z-E/LLCE/m-p/2328678#M250</guid>
      <dc:creator>yuancz</dc:creator>
      <dc:date>2026-03-09T07:02:09Z</dc:date>
    </item>
  </channel>
</rss>