<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32Z/EのトピックS32E288 multicore</title>
    <link>https://community.nxp.com/t5/S32Z-E/S32E288-multicore/m-p/2312873#M193</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I am a bit new to this whole multicore ordeal and would need a bit of guidance.&lt;/P&gt;&lt;P&gt;What I would like to achieve is the following:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Use the M33 as the boot core and run FreeRTOS and distribute commands&lt;/LI&gt;&lt;LI&gt;Use all the other (R52_0_0, R52_0_1, R52_1_0 and R52_1_1) cores as designated workers with their own state machines&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;I have managed to run FreeRTOS on the M33 as the boot core, but I don't quite understand how to enable the other cores from the M33 core.&amp;nbsp;&lt;/P&gt;&lt;P&gt;AI has suggested that I would need to basically just flash my code to the correct place in memory and then wake the cores/enable the core clock from the boot core, which generally makes sense to me.&lt;/P&gt;&lt;P&gt;But what I don't understand is:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Is there a specific RTD that I would need to enable for the boot core that would handle starting of other cores?&lt;/LI&gt;&lt;LI&gt;The S32 Design Studio creates different projects for each core, so how can I be sure that each project is built and loaded as one flash image?&lt;/LI&gt;&lt;LI&gt;How can I use the S32 Debugger for debugging the entire stack (all the cores) and which settings should I apply or check, since the debugging is done from RAM I believe?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;My setup:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;S32 Design Studio 3.6.4&lt;/LI&gt;&lt;LI&gt;S32 Debugger&lt;/LI&gt;&lt;LI&gt;S32E288-975EVB&lt;/LI&gt;&lt;/UL&gt;</description>
    <pubDate>Thu, 05 Feb 2026 11:23:34 GMT</pubDate>
    <dc:creator>HiddenSquid</dc:creator>
    <dc:date>2026-02-05T11:23:34Z</dc:date>
    <item>
      <title>S32E288 multicore</title>
      <link>https://community.nxp.com/t5/S32Z-E/S32E288-multicore/m-p/2312873#M193</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I am a bit new to this whole multicore ordeal and would need a bit of guidance.&lt;/P&gt;&lt;P&gt;What I would like to achieve is the following:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Use the M33 as the boot core and run FreeRTOS and distribute commands&lt;/LI&gt;&lt;LI&gt;Use all the other (R52_0_0, R52_0_1, R52_1_0 and R52_1_1) cores as designated workers with their own state machines&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;I have managed to run FreeRTOS on the M33 as the boot core, but I don't quite understand how to enable the other cores from the M33 core.&amp;nbsp;&lt;/P&gt;&lt;P&gt;AI has suggested that I would need to basically just flash my code to the correct place in memory and then wake the cores/enable the core clock from the boot core, which generally makes sense to me.&lt;/P&gt;&lt;P&gt;But what I don't understand is:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Is there a specific RTD that I would need to enable for the boot core that would handle starting of other cores?&lt;/LI&gt;&lt;LI&gt;The S32 Design Studio creates different projects for each core, so how can I be sure that each project is built and loaded as one flash image?&lt;/LI&gt;&lt;LI&gt;How can I use the S32 Debugger for debugging the entire stack (all the cores) and which settings should I apply or check, since the debugging is done from RAM I believe?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;My setup:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;S32 Design Studio 3.6.4&lt;/LI&gt;&lt;LI&gt;S32 Debugger&lt;/LI&gt;&lt;LI&gt;S32E288-975EVB&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Thu, 05 Feb 2026 11:23:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32Z-E/S32E288-multicore/m-p/2312873#M193</guid>
      <dc:creator>HiddenSquid</dc:creator>
      <dc:date>2026-02-05T11:23:34Z</dc:date>
    </item>
    <item>
      <title>Re: S32E288 multicore</title>
      <link>https://community.nxp.com/t5/S32Z-E/S32E288-multicore/m-p/2313203#M194</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/257370"&gt;@HiddenSquid&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Thanks for reaching out to us. Regarding your questions, we do not offer a bootloader implementation using FreeRTOS for the M33, we offer an AUTOSAR project called GreenVIP for the S32Z/E family, it includes a bootloader for the SMU/M33 core. My recommendation at the moment would be to compile and debug one of the projects (SMU_LA or SMU_LAV) and check which registers are configured to load the binary and start the RTU cores. You can check section&amp;nbsp;&lt;EM&gt;3.2 GreenVIP booting sequence for S32E2 device&lt;/EM&gt;&amp;nbsp;and&amp;nbsp;&lt;EM&gt;3.1.3 Boot Service Mode&lt;/EM&gt;&amp;nbsp;of the GreenVIP user guide for mode details on how it works. I would recommend using SMU_LA, which is simpler that SMU_LAV.&lt;/P&gt;
&lt;P&gt;You can download the GreenVIP in&amp;nbsp;&lt;A href="https://www.nxp.com/app-autopackagemgr/automotive-software-package-manager:AUTO-SW-PACKAGE-MANAGER" target="_blank"&gt;AUTO-SW-PACKAGE-MANAGER&lt;/A&gt;:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="alejandro_e_0-1770324087612.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/375734i3DF8CFDC7A757BF5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="alejandro_e_0-1770324087612.png" alt="alejandro_e_0-1770324087612.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;alejandro_e_0-1770324087612.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please check the documentation carefully to know how to build it, it can be somewhat confusing sometimes since it is quite a big project.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Let me know if you have more questions&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 05 Feb 2026 21:05:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32Z-E/S32E288-multicore/m-p/2313203#M194</guid>
      <dc:creator>alejandro_e</dc:creator>
      <dc:date>2026-02-05T21:05:59Z</dc:date>
    </item>
    <item>
      <title>Re: S32E288 multicore</title>
      <link>https://community.nxp.com/t5/S32Z-E/S32E288-multicore/m-p/2314449#M195</link>
      <description>&lt;P&gt;Hey,&lt;/P&gt;&lt;P&gt;Thanks for the answer and I am now trying to use the greenVIP package, but I am unable to find a proper user manual or a getting started page.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;I have managed to download and install the required packages from the suggested package manager.&lt;/LI&gt;&lt;LI&gt;There is suggested &lt;A href="https://community.nxp.com/t5/forums/filteredbylabelpage/board-id/ap-software-support/label-name/green_vip" target="_self"&gt;link&lt;/A&gt; at the &lt;A href="https://www.nxp.com/design/design-center/software/automotive-software-and-tools/s32z-e-vehicle-integration-platform-greenvip:GREENVIP" target="_self"&gt;offical greenVIP&lt;/A&gt; page, but it seems to be restricted.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Could you post a link or a specific tutorial on how to get greenVIP package up and running in the S32 Design Studio 3.6.4?&lt;/P&gt;&lt;P&gt;Thanks in advance for bearing with me! &lt;LI-EMOJI id="lia_grinning-face-with-smiling-eyes" title=":grinning_face_with_smiling_eyes:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 09 Feb 2026 08:30:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32Z-E/S32E288-multicore/m-p/2314449#M195</guid>
      <dc:creator>HiddenSquid</dc:creator>
      <dc:date>2026-02-09T08:30:24Z</dc:date>
    </item>
    <item>
      <title>Re: S32E288 multicore</title>
      <link>https://community.nxp.com/t5/S32Z-E/S32E288-multicore/m-p/2314929#M196</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/257370"&gt;@HiddenSquid&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;you should be able to find the user guide and user manual in your installation directory, if you are using the default installation path you can find them in&amp;nbsp;&lt;EM&gt;C:\NXP\S32ZE_GreenVIP_1.3.1\doc&lt;/EM&gt;. It can get somewhat tricky to configure all dependencies to build the SMU_LA/SMU_LAV projects, you can see all dependencies in&amp;nbsp;&lt;EM&gt;Table 2. Software Products Integrated in GreenVIP&lt;/EM&gt;, in the User Manual. Then you can check section&amp;nbsp;&lt;EM&gt;9.2.3 Setup EB ACP Partition&lt;/EM&gt; of the user guide.&lt;/P&gt;
&lt;P&gt;The SMU_LA and SMU_LAV projects are not meant for S32 Design Studio they are for EB Tresos Studio, you can check this &lt;A href="https://community.nxp.com/t5/S32Z-E-Knowledge-Base/S32Z-E-Compile-and-debug-with-S32-Design-Studio-and-EB-Tresos/ta-p/2207181" target="_blank"&gt;guide&lt;/A&gt; to know how to install and get the license for EB Tresos Studio, although the installation is a little different because you need EB Tresos AutoCore, the installation steps are the same it is just a different product. In the same guide you can see how to debug EB Tresos Projects.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Let me know if you have more questions.&lt;/P&gt;</description>
      <pubDate>Mon, 09 Feb 2026 20:14:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32Z-E/S32E288-multicore/m-p/2314929#M196</guid>
      <dc:creator>alejandro_e</dc:creator>
      <dc:date>2026-02-09T20:14:30Z</dc:date>
    </item>
  </channel>
</rss>