<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NXP S32M276CHABMKHSR Structure question in S32M</title>
    <link>https://community.nxp.com/t5/S32M/NXP-S32M276CHABMKHSR-Structure-question/m-p/2407046#M241</link>
    <description>&lt;P&gt;Hi&amp;nbsp;Daniel,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;When L300 is removed, I measured 4.98V on VDD_HV_A, while VDD_AE10 = 5.02V；&lt;/P&gt;&lt;P&gt;So could I say like that VDD_HV_A and VDD_AE10 are internally connected.&lt;/P&gt;&lt;P&gt;And should connect them together to make low impedance.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 20 Aug 2026 14:01:58 GMT</pubDate>
    <dc:creator>Ted_Qiao</dc:creator>
    <dc:date>2026-08-20T14:01:58Z</dc:date>
    <item>
      <title>NXP S32M276CHABMKHSR Structure question</title>
      <link>https://community.nxp.com/t5/S32M/NXP-S32M276CHABMKHSR-Structure-question/m-p/2405972#M235</link>
      <description>&lt;P&gt;Hi NXP technician,&lt;/P&gt;&lt;P&gt;This is Ted from Melecs Wuxi, nice to contact you.&lt;/P&gt;&lt;P&gt;I have one question about the structure of S32M276 IC. ( pls. refer to the attached file: Schematic- S32M276).&lt;/P&gt;&lt;P&gt;I did the design as datasheet recommendation, connect the 9pin-VDD_AE10, 12pin,25pin,37pin-VDD_HV_A together with beads. from my understanding,&amp;nbsp;9pin-VDD_AE10 P5V output voltage is generated by internal regulator, then supply the MCU-die on VDD_HV_A pin.&lt;/P&gt;&lt;P&gt;But&amp;nbsp;I removed L300, and after that, the PCBA could still working as normal.&lt;/P&gt;&lt;P&gt;So my question is that the VDD_AE10 pin and VDD_HV_A pin are internally connected together?&amp;nbsp; Otherwise, after removing L300 system still work, which does not make sense..&lt;/P&gt;</description>
      <pubDate>Tue, 18 Aug 2026 03:17:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32M/NXP-S32M276CHABMKHSR-Structure-question/m-p/2405972#M235</guid>
      <dc:creator>Ted_Qiao</dc:creator>
      <dc:date>2026-08-18T03:17:01Z</dc:date>
    </item>
    <item>
      <title>Re: NXP S32M276CHABMKHSR Structure question</title>
      <link>https://community.nxp.com/t5/S32M/NXP-S32M276CHABMKHSR-Structure-question/m-p/2406067#M236</link>
      <description>&lt;P&gt;Hi Ted,&lt;/P&gt;
&lt;P&gt;The AE die generates VDD_AE10.&lt;BR /&gt;On the AE side, VDD_AE10 is the power supply of the AE ports, all the ports are clamped to VDD_AE10.&lt;BR /&gt;On the MCU side, VDD_HV_A is the power supply of the MCU ports, all the ports are clamped to VDD_HV_A.&lt;BR /&gt;These two dies are interconnected.&lt;/P&gt;
&lt;P&gt;If the input voltage on any MCU port is higher than VDD_HV_A + Vf of the clamp, the VDD_HV_A domain is going to be powered by the injected current. And you should measure VDD_AE10 - Vf on VDD_HV_A - this can damage the device.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 18 Aug 2026 08:20:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32M/NXP-S32M276CHABMKHSR-Structure-question/m-p/2406067#M236</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2026-08-18T08:20:47Z</dc:date>
    </item>
    <item>
      <title>Re: NXP S32M276CHABMKHSR Structure question</title>
      <link>https://community.nxp.com/t5/S32M/NXP-S32M276CHABMKHSR-Structure-question/m-p/2406177#M237</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Daniel,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks for your reply.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1, So it means that the VDD_AE10 and VDD_HV_A are internally connected?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;And I could not understand the meaning of this sentence&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;[And you should measure VDD_AE10 - Vf on VDD_HV_A - this can damage the device.] &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;If you could give me some more explanation.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 18 Aug 2026 11:08:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32M/NXP-S32M276CHABMKHSR-Structure-question/m-p/2406177#M237</guid>
      <dc:creator>Ted_Qiao</dc:creator>
      <dc:date>2026-08-18T11:08:55Z</dc:date>
    </item>
    <item>
      <title>Re: NXP S32M276CHABMKHSR Structure question</title>
      <link>https://community.nxp.com/t5/S32M/NXP-S32M276CHABMKHSR-Structure-question/m-p/2406252#M239</link>
      <description>&lt;P&gt;Hi Ted,&lt;/P&gt;
&lt;P&gt;When L300 is removed, what voltage do you measure on VDD_HV_A?&lt;/P&gt;
&lt;P&gt;The MCU-side power supply domain VDD_HV_A is likely powered through the GPIOs that are shared between the MCU and the AE side, because all GPIOs are clamped to VDD_HV_A. In other words, VDD_HV_A can be powered through any pin if the voltage on that pin is greater than VDD_HV_A. You should therefore measure approximately VDD_HV_A = VDD_AE10 - Vf, not VDD_HV_A =&amp;nbsp;VDD_AE10.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you,&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 18 Aug 2026 14:56:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32M/NXP-S32M276CHABMKHSR-Structure-question/m-p/2406252#M239</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2026-08-18T14:56:10Z</dc:date>
    </item>
    <item>
      <title>Re: NXP S32M276CHABMKHSR Structure question</title>
      <link>https://community.nxp.com/t5/S32M/NXP-S32M276CHABMKHSR-Structure-question/m-p/2407046#M241</link>
      <description>&lt;P&gt;Hi&amp;nbsp;Daniel,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;When L300 is removed, I measured 4.98V on VDD_HV_A, while VDD_AE10 = 5.02V；&lt;/P&gt;&lt;P&gt;So could I say like that VDD_HV_A and VDD_AE10 are internally connected.&lt;/P&gt;&lt;P&gt;And should connect them together to make low impedance.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Aug 2026 14:01:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32M/NXP-S32M276CHABMKHSR-Structure-question/m-p/2407046#M241</guid>
      <dc:creator>Ted_Qiao</dc:creator>
      <dc:date>2026-08-20T14:01:58Z</dc:date>
    </item>
    <item>
      <title>Re: NXP S32M276CHABMKHSR Structure question</title>
      <link>https://community.nxp.com/t5/S32M/NXP-S32M276CHABMKHSR-Structure-question/m-p/2411631#M244</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256881"&gt;@Ted_Qiao&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I have checked with the design team.&amp;nbsp;In addition to the current injection path through the GPIOs shared between the two dies, there is also a connection for internal monitoring between them. However, these paths are not designed to withstand operational currents, so an external PCB connection is required.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Mon, 07 Sep 2026 07:16:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32M/NXP-S32M276CHABMKHSR-Structure-question/m-p/2411631#M244</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2026-09-07T07:16:40Z</dc:date>
    </item>
  </channel>
</rss>