<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 S32K144 S-record (S2)</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-S-record-S2/m-p/1234442#M9961</link>
    <description>&lt;P&gt;I need to generate a S-record executable file by S32DS for the S32K144 micro.&lt;/P&gt;&lt;P&gt;When I select the Motorola format in the IDE settings the result is a S1 records file but I would like to generate the S2 records, as it happens when I try to compile the example project of the unified (UDS) bootloader project by NXP.&lt;/P&gt;&lt;P&gt;Could you suggest me how is possible to make the S2 motorola format file?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance,&lt;/P&gt;&lt;P&gt;Claudio&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 22 Feb 2021 15:36:17 GMT</pubDate>
    <dc:creator>ClaudioB</dc:creator>
    <dc:date>2021-02-22T15:36:17Z</dc:date>
    <item>
      <title>S32K144 S-record (S2)</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-S-record-S2/m-p/1234442#M9961</link>
      <description>&lt;P&gt;I need to generate a S-record executable file by S32DS for the S32K144 micro.&lt;/P&gt;&lt;P&gt;When I select the Motorola format in the IDE settings the result is a S1 records file but I would like to generate the S2 records, as it happens when I try to compile the example project of the unified (UDS) bootloader project by NXP.&lt;/P&gt;&lt;P&gt;Could you suggest me how is possible to make the S2 motorola format file?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance,&lt;/P&gt;&lt;P&gt;Claudio&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Feb 2021 15:36:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-S-record-S2/m-p/1234442#M9961</guid>
      <dc:creator>ClaudioB</dc:creator>
      <dc:date>2021-02-22T15:36:17Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 S-record (S2)</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-S-record-S2/m-p/1235061#M9979</link>
      <description>&lt;P&gt;Hi, S32 Design Studio does not support S2 format. According to address ranges it automatically switches between S1 and S3 format, or you can force S3 option as shown below:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="davidtosenovjan_0-1614093669664.png" style="width: 685px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/137827i4D368CC8CA9C022B/image-dimensions/685x471?v=v2" width="685" height="471" role="button" title="davidtosenovjan_0-1614093669664.png" alt="davidtosenovjan_0-1614093669664.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;davidtosenovjan_0-1614093669664.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Or you may use some external converting tools as following for instance:&lt;/P&gt;
&lt;P&gt;&lt;A href="http://srecord.sourceforge.net/" target="_blank"&gt;http://srecord.sourceforge.net/&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Feb 2021 15:24:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-S-record-S2/m-p/1235061#M9979</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2021-02-23T15:24:06Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 S-record (S2)</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-S-record-S2/m-p/1237358#M10015</link>
      <description>&lt;P&gt;Thank you for your answer,&amp;nbsp;&lt;/P&gt;&lt;P&gt;But, I have to say you that I don't understand it, because I'm able to check that with some projects, the s32ds&amp;nbsp; generated records&amp;nbsp; results in S2 type with 3 byte long&amp;nbsp;adresses.&lt;BR /&gt;When with my previous project I obtained the S1 records format file, If I forced the ide to generate a S3 records file, I was able to see in srec file generated, the aspected rcords (S3), and as you indicate me was not possible generate the S2.&lt;BR /&gt;However in successives compiling without forcing any specific s-records format the S32DS generated &amp;nbsp;the aspected S2 records.&lt;BR /&gt;This is the reason because I answer to you just now.&lt;/P&gt;&lt;P&gt;Thank you so much for your support.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Claudio&lt;/P&gt;</description>
      <pubDate>Fri, 26 Feb 2021 16:26:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-S-record-S2/m-p/1237358#M10015</guid>
      <dc:creator>ClaudioB</dc:creator>
      <dc:date>2021-02-26T16:26:06Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 S-record (S2)</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-S-record-S2/m-p/1237362#M10016</link>
      <description>&lt;P&gt;I am apologizing but I have taken a snapshot of a option that did not work for me, by a chance. It should be there&lt;/P&gt;
&lt;P&gt;--srec-forceS3&lt;/P&gt;
&lt;P&gt;I have discussed with expert telling me S-record format switches automatically. If for used address range S1 is enough, it'll be used.&lt;/P&gt;
&lt;P&gt;Would you tell me specific case leading in S2 format? I haven't seen it with my tests, only S3.&lt;/P&gt;</description>
      <pubDate>Fri, 26 Feb 2021 16:37:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-S-record-S2/m-p/1237362#M10016</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2021-02-26T16:37:11Z</dc:date>
    </item>
  </channel>
</rss>