<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: Is OpenSDA supported for S32K2 evaluation board?</title>
    <link>https://community.nxp.com/t5/S32K/Is-OpenSDA-supported-for-S32K2-evaluation-board/m-p/1231406#M9904</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;OpenSDA should be able to connect, PEMicro and multilink should also work.&lt;/P&gt;
&lt;P&gt;Eventually you can use S32 Debug probe which is most commonly used with K2 and K3 micros.&lt;/P&gt;
&lt;P&gt;best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
    <pubDate>Tue, 16 Feb 2021 08:46:47 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2021-02-16T08:46:47Z</dc:date>
    <item>
      <title>Is OpenSDA supported for S32K2 evaluation board?</title>
      <link>https://community.nxp.com/t5/S32K/Is-OpenSDA-supported-for-S32K2-evaluation-board/m-p/1230932#M9895</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I wanted to know if OpenSDA is supported on the S32K2TV evaluation board? The schematic shows that there is a openSDA connection available to the controller but the S32 IDE does not detect the connection(pls see attached screenshot). How do you usually connect to the board? Is it through a Multilink probe or Lauterbach probe?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="S32K2_openSDA.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/137174iA8563DB286AE7AB5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="S32K2_openSDA.png" alt="S32K2_openSDA.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;S32K2_openSDA.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 15 Feb 2021 10:39:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Is-OpenSDA-supported-for-S32K2-evaluation-board/m-p/1230932#M9895</guid>
      <dc:creator>veeresh_ambe</dc:creator>
      <dc:date>2021-02-15T10:39:07Z</dc:date>
    </item>
    <item>
      <title>Re: Is OpenSDA supported for S32K2 evaluation board?</title>
      <link>https://community.nxp.com/t5/S32K/Is-OpenSDA-supported-for-S32K2-evaluation-board/m-p/1231406#M9904</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;OpenSDA should be able to connect, PEMicro and multilink should also work.&lt;/P&gt;
&lt;P&gt;Eventually you can use S32 Debug probe which is most commonly used with K2 and K3 micros.&lt;/P&gt;
&lt;P&gt;best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Tue, 16 Feb 2021 08:46:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Is-OpenSDA-supported-for-S32K2-evaluation-board/m-p/1231406#M9904</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2021-02-16T08:46:47Z</dc:date>
    </item>
  </channel>
</rss>