<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Using S32K144EVB-Q100 to program our target Board in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Using-S32K144EVB-Q100-to-program-our-target-Board/m-p/1228655#M9854</link>
    <description>&lt;P&gt;&lt;STRONG&gt;&lt;EM&gt;Hello,&lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;EM&gt;Presently we are using the S32K144EVB-Q100 for developing the firmware.Now our target board is ready.So can we use the EVB to program the S32k144 on our Target Board.We will be using the swd interface to program.What changes will be required in the evb to disconnect the existing (evb mcu) s32k144.&lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;EM&gt;Thanks and Regards &lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;EM&gt;&lt;BR /&gt;Ravi Chawda&lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 09 Feb 2021 08:56:09 GMT</pubDate>
    <dc:creator>ravichawda</dc:creator>
    <dc:date>2021-02-09T08:56:09Z</dc:date>
    <item>
      <title>Using S32K144EVB-Q100 to program our target Board</title>
      <link>https://community.nxp.com/t5/S32K/Using-S32K144EVB-Q100-to-program-our-target-Board/m-p/1228655#M9854</link>
      <description>&lt;P&gt;&lt;STRONG&gt;&lt;EM&gt;Hello,&lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;EM&gt;Presently we are using the S32K144EVB-Q100 for developing the firmware.Now our target board is ready.So can we use the EVB to program the S32k144 on our Target Board.We will be using the swd interface to program.What changes will be required in the evb to disconnect the existing (evb mcu) s32k144.&lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;EM&gt;Thanks and Regards &lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;EM&gt;&lt;BR /&gt;Ravi Chawda&lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 09 Feb 2021 08:56:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Using-S32K144EVB-Q100-to-program-our-target-Board/m-p/1228655#M9854</guid>
      <dc:creator>ravichawda</dc:creator>
      <dc:date>2021-02-09T08:56:09Z</dc:date>
    </item>
    <item>
      <title>Re: Using S32K144EVB-Q100 to program our target Board</title>
      <link>https://community.nxp.com/t5/S32K/Using-S32K144EVB-Q100-to-program-our-target-Board/m-p/1228789#M9857</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;this was already discussed here:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/Are-S32K1xx-MCUs-delivered-with-UART-Bootloader/m-p/1161357/highlight/true" target="_blank"&gt;https://community.nxp.com/t5/S32K/Are-S32K1xx-MCUs-delivered-with-UART-Bootloader/m-p/1161357/highlight/true&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;See the post from &lt;SPAN class="DateTime"&gt;&lt;SPAN class="local-date"&gt;10-01-2020&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;04:07 AM&lt;/SPAN&gt;&lt;/SPAN&gt;.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 09 Feb 2021 13:28:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Using-S32K144EVB-Q100-to-program-our-target-Board/m-p/1228789#M9857</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2021-02-09T13:28:36Z</dc:date>
    </item>
  </channel>
</rss>