<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K analog capability in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K-analog-capability/m-p/1224878#M9799</link>
    <description>&lt;P&gt;I'm trying to figure out if the S32K series has an option with the analog capability to decode the following phase reversal keyed message:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="paul_miller_0-1612283736078.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/136326iD38F95D7382ED3A3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="paul_miller_0-1612283736078.png" alt="paul_miller_0-1612283736078.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The message sweeps from 203kHz to 400kHz to 100kHz and back to 203kHz over 100us.&amp;nbsp; The difference between '1' and '0' states is 180deg.&amp;nbsp; If I double the highest frequency, I think this means that the ADC would need to sample at least once every 1.25us.&lt;/P&gt;&lt;P&gt;I need to not load down the processor with this operation.&amp;nbsp; I'll have some other analog sensing operations and a couple of digital communications buses.&amp;nbsp; Will the S32K family support this?&lt;/P&gt;</description>
    <pubDate>Tue, 02 Feb 2021 16:43:56 GMT</pubDate>
    <dc:creator>paul_miller</dc:creator>
    <dc:date>2021-02-02T16:43:56Z</dc:date>
    <item>
      <title>S32K analog capability</title>
      <link>https://community.nxp.com/t5/S32K/S32K-analog-capability/m-p/1224878#M9799</link>
      <description>&lt;P&gt;I'm trying to figure out if the S32K series has an option with the analog capability to decode the following phase reversal keyed message:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="paul_miller_0-1612283736078.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/136326iD38F95D7382ED3A3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="paul_miller_0-1612283736078.png" alt="paul_miller_0-1612283736078.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The message sweeps from 203kHz to 400kHz to 100kHz and back to 203kHz over 100us.&amp;nbsp; The difference between '1' and '0' states is 180deg.&amp;nbsp; If I double the highest frequency, I think this means that the ADC would need to sample at least once every 1.25us.&lt;/P&gt;&lt;P&gt;I need to not load down the processor with this operation.&amp;nbsp; I'll have some other analog sensing operations and a couple of digital communications buses.&amp;nbsp; Will the S32K family support this?&lt;/P&gt;</description>
      <pubDate>Tue, 02 Feb 2021 16:43:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-analog-capability/m-p/1224878#M9799</guid>
      <dc:creator>paul_miller</dc:creator>
      <dc:date>2021-02-02T16:43:56Z</dc:date>
    </item>
    <item>
      <title>Re: S32K analog capability</title>
      <link>https://community.nxp.com/t5/S32K/S32K-analog-capability/m-p/1226357#M9823</link>
      <description>&lt;P&gt;Hello Paul,&lt;/P&gt;
&lt;P&gt;The ADC conversion time can be calculated using the equation in the RM rev12.1, Section 44.5.4.5.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1612432808462.png" style="width: 646px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/136505iBC11C4B3EB9570EC/image-dimensions/646x92?v=v2" width="646" height="92" role="button" title="danielmartynek_0-1612432808462.png" alt="danielmartynek_0-1612432808462.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;At the max. fADC = 50MHz, with sample time of just 2 ADC clock cycles in the 8-bit mode, one ADC conversion takes 0.66us.&lt;/P&gt;
&lt;P&gt;But the sample time would be very short - this would required a very low source resistance so that the internal sample-and-hold capacitor could be charged to the input voltage.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;RM rev12.1, Table 27-8. Peripheral clock summary&lt;/STRONG&gt; &lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_1-1612433829186.png" style="width: 708px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/136506iA6CEDC815D46D7E8/image-dimensions/708x92?v=v2" width="708" height="92" role="button" title="danielmartynek_1-1612433829186.png" alt="danielmartynek_1-1612433829186.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_2-1612433889967.png" style="width: 716px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/136507iB5D758EB72648DE7/image-dimensions/716x34?v=v2" width="716" height="34" role="button" title="danielmartynek_2-1612433889967.png" alt="danielmartynek_2-1612433889967.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;DS rev13, Table 40. 12-bit ADC operating conditions&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_4-1612434419167.png" style="width: 713px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/136510i62EC2169222ABF11/image-dimensions/713x224?v=v2" width="713" height="224" role="button" title="danielmartynek_4-1612434419167.png" alt="danielmartynek_4-1612434419167.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Feb 2021 10:39:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-analog-capability/m-p/1226357#M9823</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-02-04T10:39:09Z</dc:date>
    </item>
  </channel>
</rss>