<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32Kのトピックproblem with S32K144EVB board</title>
    <link>https://community.nxp.com/t5/S32K/problem-with-S32K144EVB-board/m-p/1223251#M9752</link>
    <description>&lt;P&gt;Hello, a few days ago, I use two S32K144EVB boards to run the demo of CAN communication (can_pal_s32k144) and a CAN based bootloader demo. The result was ok.&lt;/P&gt;&lt;P&gt;When I try to run the same CAN communicaiton demo today, I encounter a strange problem. The LED D1 turns to red after reset. D1 is in the red square in the following picture.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="1.png" style="width: 720px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/136088i18D6A8A0B3012B96/image-size/large?v=v2&amp;amp;px=999" role="button" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I can debug the software through the opensda, the software can run in the debug environment. But when I leave the debug mode, the D1 led turns to red immediately.&lt;/P&gt;&lt;P&gt;I think that the mcu is always been reset when power of, so the program has no chance to run. I have no idea about how to deal with the problem, please help.&lt;/P&gt;</description>
    <pubDate>Fri, 29 Jan 2021 11:35:15 GMT</pubDate>
    <dc:creator>Jimny</dc:creator>
    <dc:date>2021-01-29T11:35:15Z</dc:date>
    <item>
      <title>problem with S32K144EVB board</title>
      <link>https://community.nxp.com/t5/S32K/problem-with-S32K144EVB-board/m-p/1223251#M9752</link>
      <description>&lt;P&gt;Hello, a few days ago, I use two S32K144EVB boards to run the demo of CAN communication (can_pal_s32k144) and a CAN based bootloader demo. The result was ok.&lt;/P&gt;&lt;P&gt;When I try to run the same CAN communicaiton demo today, I encounter a strange problem. The LED D1 turns to red after reset. D1 is in the red square in the following picture.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="1.png" style="width: 720px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/136088i18D6A8A0B3012B96/image-size/large?v=v2&amp;amp;px=999" role="button" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I can debug the software through the opensda, the software can run in the debug environment. But when I leave the debug mode, the D1 led turns to red immediately.&lt;/P&gt;&lt;P&gt;I think that the mcu is always been reset when power of, so the program has no chance to run. I have no idea about how to deal with the problem, please help.&lt;/P&gt;</description>
      <pubDate>Fri, 29 Jan 2021 11:35:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/problem-with-S32K144EVB-board/m-p/1223251#M9752</guid>
      <dc:creator>Jimny</dc:creator>
      <dc:date>2021-01-29T11:35:15Z</dc:date>
    </item>
  </channel>
</rss>