<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPIT maximum achievable frequency? in S32K</title>
    <link>https://community.nxp.com/t5/S32K/LPIT-maximum-achievable-frequency/m-p/1212724#M9614</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I use S32K144 and st the clock as following with using SOSC:&lt;/P&gt;&lt;P&gt;SOSC : 8MHz,&amp;nbsp; SPLL:160MHz, CORE_CLK: 80MHz,&amp;nbsp;BUS_CLK: 40MHz;&lt;/P&gt;&lt;P&gt;When I want to use LPIT with input clock = CLK_SRC_FIRC_DIV1 (which is 48MHz), There is not any problem and LPIT interrupt is as which I excepted. but in RM (page 567) "Maximum frequency governed by BUS_CLK" which is 40MHz!!!&lt;/P&gt;&lt;P&gt;48MHz is greater than 40MHz but MCU LPIT works fine !!!&lt;/P&gt;</description>
    <pubDate>Sat, 16 Jan 2021 08:44:23 GMT</pubDate>
    <dc:creator>JeorgeB</dc:creator>
    <dc:date>2021-01-16T08:44:23Z</dc:date>
    <item>
      <title>LPIT maximum achievable frequency?</title>
      <link>https://community.nxp.com/t5/S32K/LPIT-maximum-achievable-frequency/m-p/1212724#M9614</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I use S32K144 and st the clock as following with using SOSC:&lt;/P&gt;&lt;P&gt;SOSC : 8MHz,&amp;nbsp; SPLL:160MHz, CORE_CLK: 80MHz,&amp;nbsp;BUS_CLK: 40MHz;&lt;/P&gt;&lt;P&gt;When I want to use LPIT with input clock = CLK_SRC_FIRC_DIV1 (which is 48MHz), There is not any problem and LPIT interrupt is as which I excepted. but in RM (page 567) "Maximum frequency governed by BUS_CLK" which is 40MHz!!!&lt;/P&gt;&lt;P&gt;48MHz is greater than 40MHz but MCU LPIT works fine !!!&lt;/P&gt;</description>
      <pubDate>Sat, 16 Jan 2021 08:44:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPIT-maximum-achievable-frequency/m-p/1212724#M9614</guid>
      <dc:creator>JeorgeB</dc:creator>
      <dc:date>2021-01-16T08:44:23Z</dc:date>
    </item>
    <item>
      <title>Re: LPIT maximum achievable frequency?</title>
      <link>https://community.nxp.com/t5/S32K/LPIT-maximum-achievable-frequency/m-p/1220231#M9691</link>
      <description>&lt;P&gt;Please check the feedback from AE team:&lt;/P&gt;
&lt;P&gt;We need to remember that the "Bus interface clock" (BUS_CLK in this case) is the one used to feed all the logic for LPIT, in this particular example, I see that the configuration of its registers is done successfully (using the BUS_CLK), and then, the timer starts working with its functional clock (FIRCDIV2, asynchronously).&lt;/P&gt;
&lt;P&gt;That's why apparently there is no problem. Where problems could arise is when writing/reading the LPIT regs, later in the application.&lt;/P&gt;
&lt;P&gt;In a nutshell, they went out of the spec, but as they kept using only the functional clock, they didn't see any issues.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jan 2021 06:24:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPIT-maximum-achievable-frequency/m-p/1220231#M9691</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2021-01-25T06:24:53Z</dc:date>
    </item>
  </channel>
</rss>