<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: What is the power supply voltage range over which the S32K144EVB-Q100 can operate? in S32K</title>
    <link>https://community.nxp.com/t5/S32K/What-is-the-power-supply-voltage-range-over-which-the-S32K144EVB/m-p/1211186#M9591</link>
    <description>&lt;P&gt;No, I did not drop other files into MSD or Bootloader.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 13 Jan 2021 15:12:42 GMT</pubDate>
    <dc:creator>ranulf</dc:creator>
    <dc:date>2021-01-13T15:12:42Z</dc:date>
    <item>
      <title>What is the power supply voltage range over which the S32K144EVB-Q100 can operate?</title>
      <link>https://community.nxp.com/t5/S32K/What-is-the-power-supply-voltage-range-over-which-the-S32K144EVB/m-p/1207620#M9495</link>
      <description>&lt;P&gt;What is the power supply voltage range over which the S32K144EVB-Q100 can safely operate? The quick start guide says 12 V, of course, but is the range known? I can't find a datasheet for the board.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 06 Jan 2021 16:32:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/What-is-the-power-supply-voltage-range-over-which-the-S32K144EVB/m-p/1207620#M9495</guid>
      <dc:creator>ranulf</dc:creator>
      <dc:date>2021-01-06T16:32:04Z</dc:date>
    </item>
    <item>
      <title>Re: What is the power supply voltage range over which the S32K144EVB-Q100 can operate?</title>
      <link>https://community.nxp.com/t5/S32K/What-is-the-power-supply-voltage-range-over-which-the-S32K144EVB/m-p/1207624#M9496</link>
      <description>&lt;P&gt;I have a board that got 13.9 V. Now it is not recognized by the Windows 10 PC. I am wondering if the slightly high voltage could have contributed to the failure.&lt;/P&gt;</description>
      <pubDate>Wed, 06 Jan 2021 16:37:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/What-is-the-power-supply-voltage-range-over-which-the-S32K144EVB/m-p/1207624#M9496</guid>
      <dc:creator>ranulf</dc:creator>
      <dc:date>2021-01-06T16:37:45Z</dc:date>
    </item>
    <item>
      <title>Re: What is the power supply voltage range over which the S32K144EVB-Q100 can operate?</title>
      <link>https://community.nxp.com/t5/S32K/What-is-the-power-supply-voltage-range-over-which-the-S32K144EVB/m-p/1207965#M9499</link>
      <description>&lt;P&gt;Hi&amp;nbsp;ranulf,&lt;/P&gt;
&lt;P&gt;Although according to the description of &lt;A href="https://www.nxp.com/document/guide/get-started-with-the-s32k144evb:NGS-S32K144EVB" target="_self"&gt;Get Started with the S32K144EVB&lt;/A&gt; the &lt;STRONG&gt;External Power Supply&lt;/STRONG&gt; should be 5-12V. But I don't think 13.9 V will damage the power supply of the board.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="External Power Supply (5-12V).png" style="width: 843px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/134201i57F5E832A28B322E/image-size/large?v=v2&amp;amp;px=999" role="button" title="External Power Supply (5-12V).png" alt="External Power Supply (5-12V).png" /&gt;&lt;/span&gt;&lt;BR /&gt;The &lt;STRONG&gt;UJA1169TK/F&lt;/STRONG&gt; seems able to work according to the description of&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/data-sheet/UJA1169.pdf" target="_self"&gt;Mini high-speed CAN system basis chip (REV 1.0)&lt;/A&gt;. Please check the voltage of &lt;STRONG&gt;J107&lt;/STRONG&gt; Pin1(&lt;STRONG&gt;P5V_SBC&lt;/STRONG&gt;) is still OK, when using 12V external power supply(connect Pin1-2 of J107).&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="S32K144EVB-Q100 sch.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/134202iB4699D297E3D28EB/image-size/large?v=v2&amp;amp;px=999" role="button" title="S32K144EVB-Q100 sch.png" alt="S32K144EVB-Q100 sch.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;S32K144EVB can also be power through USB port(&lt;STRONG&gt;J7&lt;/STRONG&gt;). Connect pin2-3 of J107 and check if it works.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="J104.png" style="width: 990px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/134203i520270336062AC9B/image-size/large?v=v2&amp;amp;px=999" role="button" title="J104.png" alt="J104.png" /&gt;&lt;/span&gt;&lt;BR /&gt;Please make the board enter &lt;STRONG&gt;BOOTLOADER&lt;/STRONG&gt; mode:&lt;BR /&gt;1. Connect Pin 1-2 of J104 &lt;BR /&gt;2. Hold down RESET Button(&lt;STRONG&gt;SW5&lt;/STRONG&gt;)&lt;BR /&gt;3. Connect to the USB port and let OpenSDA K20 enter &lt;STRONG&gt;BOOTLOADER&lt;/STRONG&gt; mode&lt;BR /&gt;4. Release RESET Button(&lt;STRONG&gt;SW5&lt;/STRONG&gt;)&lt;/P&gt;
&lt;P&gt;Then click "&lt;STRONG&gt;SDA_INFO&lt;/STRONG&gt;" in this BOOTLOADER driver, show "&lt;STRONG&gt;Your Hardware Information&lt;/STRONG&gt;" of your board to me.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="SDA_INFO.png" style="width: 939px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/134206i993FA294BDD03F20/image-size/large?v=v2&amp;amp;px=999" role="button" title="SDA_INFO.png" alt="SDA_INFO.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;If there are issue at&amp;nbsp;&lt;SPAN&gt;&lt;STRONG&gt;Installed Application&lt;/STRONG&gt; and&amp;nbsp;&lt;STRONG&gt;Application Version&lt;/STRONG&gt;, you can drop new&amp;nbsp;application firmware:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;5. Drop application firmware into &lt;STRONG&gt;BOOTLOADER&lt;/STRONG&gt; drive&lt;BR /&gt;6. Remove and replace the USB cable.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Although the hardware is slightly different, still you can refer:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/S32K148EVB-Dead-after-OpenSDA-Update-Need-help-to-recover/m-p/1205811#M9451" target="_self"&gt;S32K148EVB Dead after OpenSDA Update. Need help to recover.&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 07 Jan 2021 03:59:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/What-is-the-power-supply-voltage-range-over-which-the-S32K144EVB/m-p/1207965#M9499</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2021-01-07T03:59:54Z</dc:date>
    </item>
    <item>
      <title>Re: What is the power supply voltage range over which the S32K144EVB-Q100 can operate?</title>
      <link>https://community.nxp.com/t5/S32K/What-is-the-power-supply-voltage-range-over-which-the-S32K144EVB/m-p/1208462#M9518</link>
      <description>&lt;P&gt;The voltage at J107 Pin1 when using a 12V external power supply is 5 V.&lt;/P&gt;&lt;P&gt;The board is not powered anymore through USB when pins 2-3 of J107 are connected even though the green diode near the Open SDA MCU chip does flash when the USB is plugged in. Also the COM port for the board no longer shows up in Windows Device Manager.&lt;/P&gt;&lt;P&gt;Below is the hardware information&lt;BR /&gt;Board Name is: EVB-S32K144&lt;BR /&gt;MicroBoot Kernel Version is: 1.08&lt;BR /&gt;Bootloader Version is: 1.13&lt;BR /&gt;Application Version is: 0.00&lt;BR /&gt;DUID is: FBE33938-24BB81A0-3755080C-DABAE678&lt;BR /&gt;EUID is: 0381A239-8AA1872E-1853EA17-00C368D6&lt;BR /&gt;TUID is: 74823938-47328196-8568DD75-9242986D&lt;BR /&gt;TOA is: 86B6E505-14311D24-B33B464C-D5EB8F01&lt;BR /&gt;TOA2 is: 86B6E505-DD682D2B-C5FAE810-46DFF349&lt;BR /&gt;SUID is: 86B6E505-5B819677-37239804-8003EC65&lt;/P&gt;&lt;P&gt;I should add that at the time of failure I was using pins J5-16 (Tx), J5-18 (Rx), and J5-12 (Gnd) for UART at 5 V. I notice that these pins are also used for LIN. Could this have somehow caused the deletion of the OpenSDA firmware?&lt;/P&gt;&lt;P&gt;Other pins were connected for BMS application as described in Table 6 on pages 7 and 8 of the document “UM11143 Battery cell controller software driver v1.1".&lt;/P&gt;&lt;P&gt;I did download the OpenSDA Firmware Apps as described in your link to "S32K148EVB Dead after OpenSDA Update. Need help to recover". There did not appear to be a perfect match for this board, but I dropped what appeared to be the closest match: "MSD-DEBUG-S32K142EVB-Q100_Pemicro_121.SDA". Is this the best choice? Should I look elsewhere for the correct driver?&lt;/P&gt;&lt;P&gt;After dragging and dropping the firmware to the drive BOOTLOADER and unplugging and plugging the USB there were a few changes:&lt;BR /&gt;1) the drive name became S32K142EVB, which isn't quite right. (According to the Quick Start Guide the drive name should be EVB-S32K144. This suggests that the download does not contain the right firmware for this board.)&lt;BR /&gt;2) The voltage accross pins 3-2 of J107 is now 5.1 V.&lt;BR /&gt;3) An OpenSDA COM port is now visible in Device Manager.&lt;/P&gt;&lt;P&gt;This exercise has demonstrated to me that the hardware is probably not damaged, even if I may not yet have the right firmware. Do you know where I can get the right firmware for the board? Do you have any ideas about how/why the original firmware was deleted?&lt;/P&gt;&lt;P&gt;(Incidentally, I have had to post this message to the thread multiple times because it keeps disappearing!)&lt;/P&gt;</description>
      <pubDate>Thu, 07 Jan 2021 18:13:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/What-is-the-power-supply-voltage-range-over-which-the-S32K144EVB/m-p/1208462#M9518</guid>
      <dc:creator>ranulf</dc:creator>
      <dc:date>2021-01-07T18:13:32Z</dc:date>
    </item>
    <item>
      <title>Re: What is the power supply voltage range over which the S32K144EVB-Q100 can operate?</title>
      <link>https://community.nxp.com/t5/S32K/What-is-the-power-supply-voltage-range-over-which-the-S32K144EVB/m-p/1208553#M9522</link>
      <description>&lt;P&gt;&lt;SPAN&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/57959"&gt;@Robin_Shen&lt;/a&gt;&amp;nbsp;Thank you for your helpful response.&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The voltage at J107 Pin1 when using a 12V external power supply is 5 V.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The board is not powered anymore through USB when pins 2-3 of J107 are connected even though the green diode near the Open SDA MCU chip does flash when the USB is plugged in. Also the COM port for the board no longer shows up in Windows Device Manager. &amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Below is the hardware information&lt;/DIV&gt;&lt;DIV&gt;Board Name is: EVB-S32K144&lt;/DIV&gt;&lt;DIV&gt;MicroBoot Kernel Version is: 1.08&lt;/DIV&gt;&lt;DIV&gt;Bootloader Version is: 1.13&lt;/DIV&gt;&lt;DIV&gt;Application Version is: 0.00&lt;/DIV&gt;&lt;DIV&gt;DUID is: FBE33938-24BB81A0-3755080C-DABAE678&lt;/DIV&gt;&lt;DIV&gt;EUID is: 0381A239-8AA1872E-1853EA17-00C368D6&lt;/DIV&gt;&lt;DIV&gt;TUID is: 74823938-47328196-8568DD75-9242986D&lt;/DIV&gt;&lt;DIV&gt;TOA is: 86B6E505-14311D24-B33B464C-D5EB8F01&lt;/DIV&gt;&lt;DIV&gt;TOA2 is: 86B6E505-DD682D2B-C5FAE810-46DFF349&lt;/DIV&gt;&lt;DIV&gt;SUID is: 86B6E505-5B819677-37239804-8003EC65&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I should add that at the time of failure I was using pins J5-16 (Tx), J5-18 (Rx), and J5-12 (Gnd) for UART at 5 V. I notice that these pins are also used for LIN. Could this have somehow caused the deletion of the OpenSDA firmware?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Other pins were connected for BMS application as described in Table 6 on pages 7 and 8 of the document “UM11143 Battery cell controller software driver v1.1".&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I did download the OpenSDA Firmware Apps as described in your link to "S32K148EVB Dead after OpenSDA Update. Need help to recover". There did not appear to be a perfect match for this board, but I dropped what appeared to be the closest match: "MSD-DEBUG-S32K142EVB-Q100_Pemicro_121.SDA". Is this the best choice? Should I look elsewhere for the correct driver?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;After dragging and dropping the firmware to the drive BOOTLOADER and unplugging and plugging the USB there were a few changes:&lt;/DIV&gt;&lt;DIV&gt;1) the drive name became S32K142EVB, which isn't quite right. (According to the Quick Start Guide the drive name should be EVB-S32K144. This suggests that the download does not contain the right firmware for this board.)&lt;/DIV&gt;&lt;DIV&gt;2) The voltage accross pins 3-2 of J107 is now 5.1 V.&lt;/DIV&gt;&lt;DIV&gt;3) An OpenSDA COM port is now visible in Device Manager.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;This exercise has demonstrated to me that the hardware is probably not damaged, even if I may not yet have the right firmware. Do you know where I can get the right firmware for the board? Do you have any ideas about how/why the original firmware was deleted?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;&lt;SPAN&gt;(Incidentally, I have had to post this message to the thread multiple times because it keeps disappearing!)&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Jan 2021 23:04:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/What-is-the-power-supply-voltage-range-over-which-the-S32K144EVB/m-p/1208553#M9522</guid>
      <dc:creator>ranulf</dc:creator>
      <dc:date>2021-01-07T23:04:16Z</dc:date>
    </item>
    <item>
      <title>Re: What is the power supply voltage range over which the S32K144EVB-Q100 can operate?</title>
      <link>https://community.nxp.com/t5/S32K/What-is-the-power-supply-voltage-range-over-which-the-S32K144EVB/m-p/1210709#M9566</link>
      <description>&lt;P&gt;Hi&amp;nbsp;ranulf,&lt;/P&gt;
&lt;P&gt;Application Version is: 0.00&lt;BR /&gt;It means there is no Application in OpenSDA. So you need to drop OpenSDA Firmware Apps into it.&lt;BR /&gt;Please try to use &lt;STRONG&gt;MSD-DEBUG-EVB-S32K144_Pemicro_v119.SDA&lt;/STRONG&gt;.&lt;/P&gt;
&lt;P&gt;Do you drop other files into MSD or BOOTLOADER driver before? It may caused the original firmware disappear.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 13 Jan 2021 02:25:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/What-is-the-power-supply-voltage-range-over-which-the-S32K144EVB/m-p/1210709#M9566</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2021-01-13T02:25:35Z</dc:date>
    </item>
    <item>
      <title>Re: What is the power supply voltage range over which the S32K144EVB-Q100 can operate?</title>
      <link>https://community.nxp.com/t5/S32K/What-is-the-power-supply-voltage-range-over-which-the-S32K144EVB/m-p/1211186#M9591</link>
      <description>&lt;P&gt;No, I did not drop other files into MSD or Bootloader.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Jan 2021 15:12:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/What-is-the-power-supply-voltage-range-over-which-the-S32K144EVB/m-p/1211186#M9591</guid>
      <dc:creator>ranulf</dc:creator>
      <dc:date>2021-01-13T15:12:42Z</dc:date>
    </item>
  </channel>
</rss>