<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K144EVB-Q100 FlexCAN Encryption Example Code</title>
    <link>https://community.nxp.com/t5/S32K/S32K144EVB-Q100-FlexCAN-Encryption-Example-Code/m-p/681040#M956</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am facing similar problem. After sending the message it is encountering a lot of errors and the bus status remains busy.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Jul 2017 23:18:15 GMT</pubDate>
    <dc:creator>saurabhkarnik</dc:creator>
    <dc:date>2017-07-24T23:18:15Z</dc:date>
    <item>
      <title>S32K144EVB-Q100 FlexCAN Encryption Example Code</title>
      <link>https://community.nxp.com/t5/S32K/S32K144EVB-Q100-FlexCAN-Encryption-Example-Code/m-p/681035#M951</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to use the flexcan_encryption example app from S32DS V1.3.&lt;/P&gt;&lt;P&gt;Compilation and flashing to S32K144EVB-Q100 board works fine. But, while testing, not able to see (using CANalyzer) the msg's in CAN bus.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the code by default CAN FD support is enabled. Tried testing by disabling CAN FD support and same results.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any register, pin or jumper configuration have to be taken care. Please confirm.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With &amp;nbsp;Regards,&lt;/P&gt;&lt;P&gt;Vasanth.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Jun 2017 02:57:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144EVB-Q100-FlexCAN-Encryption-Example-Code/m-p/681035#M951</guid>
      <dc:creator>vasanthakumarra</dc:creator>
      <dc:date>2017-06-09T02:57:28Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144EVB-Q100 FlexCAN Encryption Example Code</title>
      <link>https://community.nxp.com/t5/S32K/S32K144EVB-Q100-FlexCAN-Encryption-Example-Code/m-p/681036#M952</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Vasanth,&lt;/P&gt;&lt;P&gt;Have you supplied 12V power to the board?&lt;/P&gt;&lt;P&gt;The system basis chip cannot drive the CAN bus without 12V power.&amp;nbsp; The 12V power supply is not provided with the shipment of the board, so it must be available separately.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Jun 2017 14:36:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144EVB-Q100-FlexCAN-Encryption-Example-Code/m-p/681036#M952</guid>
      <dc:creator>allen_willson</dc:creator>
      <dc:date>2017-06-09T14:36:35Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144EVB-Q100 FlexCAN Encryption Example Code</title>
      <link>https://community.nxp.com/t5/S32K/S32K144EVB-Q100-FlexCAN-Encryption-Example-Code/m-p/681037#M953</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Allen,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply. Yes, I had connected 12V power to the board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, I tried another FlexCAN example from below path and CAN communication its working fine.&lt;/P&gt;&lt;P&gt;C:\nxp\S32DS_ARM_v1.3\eclipse\plugins\com.freescale.s32ds.arm.examples.descriptor_1.0.0.201611111129\Examples\S32K144\FlexCAN&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the above example, CAN msg data is written directly to the memory address.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But in case of&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;flexcan_encryption example app, different flexcan driver function is called.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Is there any difference? &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;With Regards,&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Vasanth.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Jun 2017 02:21:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144EVB-Q100-FlexCAN-Encryption-Example-Code/m-p/681037#M953</guid>
      <dc:creator>vasanthakumarra</dc:creator>
      <dc:date>2017-06-12T02:21:22Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144EVB-Q100 FlexCAN Encryption Example Code</title>
      <link>https://community.nxp.com/t5/S32K/S32K144EVB-Q100-FlexCAN-Encryption-Example-Code/m-p/681038#M954</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vasanth,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tested the flexcan_encryption example from S32DS V1.3 on the S32K144EVB-Q100 and it seems to be working.&lt;/P&gt;&lt;P&gt;Upon button press I see a message on the CAN bus.&lt;/P&gt;&lt;P&gt;As Allen wrote, external 12V must be connected to the board and jumper J107 set to position 1-2.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If encryption is enabled the message could not be send, when encryption is failing. The encryption uses the first non-volatile user key, which needs to be configured by running the &lt;STRONG&gt;CSEc Key Configuration&lt;/STRONG&gt; in the driver examples folder. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Jun 2017 09:24:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144EVB-Q100-FlexCAN-Encryption-Example-Code/m-p/681038#M954</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2017-06-12T09:24:10Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144EVB-Q100 FlexCAN Encryption Example Code</title>
      <link>https://community.nxp.com/t5/S32K/S32K144EVB-Q100-FlexCAN-Encryption-Example-Code/m-p/681039#M955</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Petr,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the information.&lt;/P&gt;&lt;P&gt;I tried configuring the key using the&amp;nbsp;&lt;STRONG style="color: #51626f; background-color: #ffffff; border: 0px; font-weight: bold; font-size: 14px;"&gt;CSEc Key Configuration&lt;/STRONG&gt; driver example. But, setAuthKey() and loadKey() functions are returning false.&lt;/P&gt;&lt;P&gt;So, some problem with storing the key.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For this testing I had used 12V power and jumper J107 is set to position 1-2.&lt;/P&gt;&lt;P&gt;Any thoughts on how I can proceed further?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With Regards,&lt;/P&gt;&lt;P&gt;Vasanth.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jun 2017 01:37:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144EVB-Q100-FlexCAN-Encryption-Example-Code/m-p/681039#M955</guid>
      <dc:creator>vasanthakumarra</dc:creator>
      <dc:date>2017-06-14T01:37:11Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144EVB-Q100 FlexCAN Encryption Example Code</title>
      <link>https://community.nxp.com/t5/S32K/S32K144EVB-Q100-FlexCAN-Encryption-Example-Code/m-p/681040#M956</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am facing similar problem. After sending the message it is encountering a lot of errors and the bus status remains busy.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jul 2017 23:18:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144EVB-Q100-FlexCAN-Encryption-Example-Code/m-p/681040#M956</guid>
      <dc:creator>saurabhkarnik</dc:creator>
      <dc:date>2017-07-24T23:18:15Z</dc:date>
    </item>
  </channel>
</rss>